This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Secondary boot with flash

Hi, 

 

I need to add a flash memory device to the C6472 for storing a larger boot image. I have looked at the post which discusses using an McBSP configured for SPI on the C6474 (http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/439/p/34806/121593.aspx#121593). Since there are no McBSPs on the C6472, this does not appear to be an option. I would also liked to avoid using an FPGA, if possible,  to provide an interface through the GPIO as is done in the EVM. Are there any other alternatives?

 

Thanks,

Josh King