Other Parts Discussed in Thread: OMAP-L138
Hi all,
When I test ARM interrupt DSP to implement ARM/DSP communication on OMAP-L138 platform, use CHIPSIG3 in SYSCFG.CHIPSIG.
I found a strange problem that my ISR of CHIPSIGINT3 got invoked only once though I have write a 1 to CHIPSIG_CLR.BIT[3]. And I also cleared EVTCLR.
I am using DSP/BIOS 5.41 in CCS3.3. The interrupt source is CHIPINT3 and its #EVT is 67. I have mapped EVT67 to HWI_13 using HWI_eventmap.
Here is my code in DSP using DSP/BIOS(also enable use dispatch):
void main()
{
Init_int13();
LOG_printf(&trace, "hello world!");
}
void Init_int13()
{
unsigned int *EVTMASK2 = (unsigned int*)0x01800088;
unsigned int *EVTSET2 = (unsigned int*)0x01800028;
*EVTMASK2 |= (1<<3);
*EVTSET2 |= (1<<3);
HWI_eventMap(13, SYSCFG_CHIPINT3);
HWI_dispatchPlug(ZDINTERRUPTID, (Fxn)Int13_ISR, 0, NULL);
ICR = (0x1<<13);
IER |= (0x1 << 13);
CSR |= 0x1;
}
void Int13_ISR()
{
unsigned int *EVTCLR2 = (unsigned int*) 0x01800048;
if(SYSCONFIG->CHIPSIG & (1<<3) == 1)
{
SYSCONFIG->KICKR[0] = KICK0R_UNLOCK;
SYSCONFIG->KICKR[1] = KICK1R_UNLOCK;
SYSCONFIG->CHIPSIG_CLR |= (1<<3); //disable syscfg_chipint3 intrrupt
*EVTCLR2 |= (1<<3);
// lock the system config registers.
SYSCONFIG->KICKR[0] = KICK0R_LOCK;
SYSCONFIG->KICKR[1] = KICK1R_LOCK;
}
LOG_printf(&trace, "config INT13.");
return;
}
Best wishes!
lex