This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3354: RTC not always running when enabled

Part Number: AM3354


This problem is related to https://e2e.ti.com/support/processors/f/791/p/946975/3507545#3507545 

The RTC does not always start when using the internal clock. This is becoming a quite serous issue for us.

In u-boot SPL I configure the RTC_OSC_REG to be 0x40 (internal clock)

Later, in the u-boot-prompt, I am then starting the RTC by setting RTC_CTRL_REG  = 0x01, then reading the status of RTC_STATUS_REG bit 1 to see if the RTC is running or not. I am always booting from power off when doing this test. Sometimes the RTC is started and sometimes it isn't. 

Press SPACE to abort autoboot in 0 seconds
=>         md 44e3e040 1 ; md 44e3e044 1 ; md 44e3e054 1
44e3e040: 00000000                               ....
44e3e044: 00000000                               ....
44e3e054: 00000040                               @...
=> mw 44e3e040 1 ; md 44e3e040 1 ; md 44e3e044 1 ; md 44e3e054 1
44e3e040: 00000001                               ....
44e3e044: 00000002                               .... // As you can see, the status here is running, so everything is fine
44e3e054: 00000040                               @...
=> 

Press SPACE to abort autoboot in 0 seconds
=>     md 44e3e040 1 ; md 44e3e044 1 ; md 44e3e054 1
44e3e040: 00000000                               ....
44e3e044: 00000000                               ....
44e3e054: 00000040                               @...
=> mw 44e3e040 1 ; md 44e3e040 1 ; md 44e3e044 1 ; md 44e3e054 1
44e3e040: 00000001                               ....
44e3e044: 00000000                               .... // As you can se here, the status is NOT running. 
44e3e054: 00000040                               @...
=> 

In the second case I am not able get the RTC running at all. starting/stopping the RTC have no effect.