Part Number: TDA4VM
Hello,
We have been working with PSDK RTOS 06_02_00_21 so far.
And now we are working on migrating our code base to PSDK RTOS 07_00_00_11 (and in the future to 07_01_00_11).
There is system hanging observed only when our custom node is running on MCU2_1.
When our custom node is running on MCU2_0 - no hanging is observed. But we need it to be running on MCU2_1 for performance reasons.
The same node runs on another IPU with no hanging observed in PSDK RTOS 06_02_00_21.
In PSDK RTOS 07_00_00_11 the master IPU was changed from MCU2_1 to MCU2_0.
After some debugging we found out that the reason of the hanging was a UDMA copy call from the node running on MCU2_1.
The UDMA Copy is being initialized successfully based on the logs from sourcing vision_apps_init.sh
[MCU2_1] 3.928359 s: UDMA: Init ... !!!
[MCU2_1] 3.929261 s: UDMA: Init ... Done !!!
We are using the following function for udma copying:
And the hanging occurs at: vision_apps/utils/udma/src/app_udma.c, fn: appUdmaTransfer
SemaphoreP_pend(ch_obj->transfer_done_sem, SemaphoreP_WAIT_FOREVER);
The hanging is not observed when the node is running on MCU2_0. It was not observed in PSDK RTOS 06_02_00_21 as well.
Any suggestions or recommendations would be appreciated!
Best Regards,
Todor