Part Number: J721EXCPXEVM
Hi
To get two image data separately via two CSI ports, do we have to connect two Fusion boards?
Or one Fusion board is sufficient to do it?
Thanks and Best regards,
HaTa.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: J721EXCPXEVM
Hi
To get two image data separately via two CSI ports, do we have to connect two Fusion boards?
Or one Fusion board is sufficient to do it?
Thanks and Best regards,
HaTa.
Hi Tao,
No, there are two ub960 on the same fusion board, and the output of them are connected to two difference CSI ports.
Regards,
Brijesh