Part Number: TDA4VM
Hi
I'm referring to Technical Reference Manual
https://www.tij.co.jp/jp/lit/ug/spruil1a/spruil1a.pdf
・Questions
- Is the Boot Parameter Table copied to MSRAM depending on the state of the Boot Mode Pin when the ROM Code is booted?
- There are some parameters that can't be rewritten only by setting the pin, is there any way to rewrite them manually?
- It says "cold boot", so if I want to BOOT using the manually rewritten parameters in MSRAM, do I need to use warm reset?
Thanks and Best regards,
HaTa