This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP-L138 RTC SET32COUNTER

Hello,

I'm having some trouble understanding how the SET32COUNTER bit on the Control Register of the RTC module works.

As I understand, it should replace the current value on the 32 kHz counter with whatever is present on the compensation registers. The problem is, both compensation registers together amount to a 16 bits field, and I imagine that the 32 kHz counter would be a 32 bit register.

So how does this counter set works?

Thank you,

Rafael