Part Number: TMDSICE3359
Hi,
I have a TMDSICE3359 REV1.0A.
This is very old version but I want to run it.
I plan to buy a converter for the jack and adapter connection.
I remember that the converter was enclosed with the EVM. But I lost it.
So I need the HW information of REV1.0A.
24V DC Adapter that is included EVM cannot be connected to the power jack on TMDSICE3359.
The size between the adapter and the power jack is different.
Included 24V DC Adapter has 2.1mm I.D. x 5.5mm O.D. x 9.5mm output connector.
https://www.digikey.com/en/products/detail/cui-inc/EMSA240075-P5P-SZ/2352088
latest TMDSICE3359 uses RAPC722X (switch craft), but I have information of rev 1.0A.
I can't find a schematic & BOM list of TMDSICE3359.
Can I get some documents of REV1.0A or the DC Plug converter?