After run run.sh, I got it:
[host] Enable/Disable SCD-VA GPX Event Display (Only On ON-CHIP HDMI) (YES - y / NO - n) :
[host] SCD-VA GPX Event Display DISABLED !!!
********* Entered usecase 16CH Progressive <816x> Cap/Enc/Dec/Dis
636: MCFW : CPU Revision cpuRev=8!!!
636: MCFW : CPU Revision [UNKNOWN] !!!
[c6xdsp ] 5459: Assertion @ Line: 100 in links_c6xdsp/alg_link/algLink_priv.c: status == FVID2_SOK : failed !!!
Is ling depend some other?
I SDK source code, I found that:
these link: displayLink、grpxLink、nullLink、systemLink is the same that :linkObj.getLinkInfo = NULL;
so
1 is my problem depends on displayLink ok?
2 when these link's getLinkInfo is set?