Hi,
As told in sprugx8b p1570.
SPI_D[0] I/O Can be configured as either input or output (MOSI or MISO)
SPI_D[1] I/O Can be configured as either input or output (MOSI or MISO)
How can i config SPI_D[0] as MOSI?
Is it like that ?
TI816X_MUX(TI816X_CONTROL_PADCONF_SPI_SCLK_OFFSET, OMAP_MUX_MODE0|OMAP_PULL_UP), /* SPI_SCLK */
TI816X_MUX(TI816X_CONTROL_PADCONF_SPI_D0_OFFSET, OMAP_MUX_MODE0|OMAP_PULL_UP), /* SPI_D[0] */
TI816X_MUX(TI816X_CONTROL_PADCONF_SPI_D1_OFFSET, OMAP_MUX_MODE0|OMAP_PULL_UP), /* SPI_D[1] */
Thanks!
Best Regards!