Part Number: PROCESSOR-SDK-TDAX
Is it possible to flip/mirror the source image on-the-fly along the x/y-axis to create a mirror effect on the source data?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PROCESSOR-SDK-TDAX
Is it possible to flip/mirror the source image on-the-fly along the x/y-axis to create a mirror effect on the source data?
The DISPC supports on-the-fly source image flip along the x/y-axis to create a mirror effect on the source data.
The below 3 patches could be used in order to make use of this feature.
The patches are created on top of SDK 07_03_00_07
1. TIOVX_Flip_Support.patch
In the process function of the display node, the buffer address to be assigned to Fvid queue should be as follow for respective flip options:
a. No Flip : No change in the buffer base address.
b. Vertical Flip : No change in the buffer base address.
c. Horizontal Flip : Buffer base address should point to Start of last line of the window
d. Both Vertical and horizontal flip : Buffer base address should point to Start of last line of the window
In the control function of the display node, new control command "TIVX_DISPLAY_SELECT_FLIP" is added in order to accept the flip command from the HOST.
This control command uses pointer to structure tivx_display_fliptype_t as an input argument.
Valid values for the flip type are as shown below :
0 : No Flip
1 : Horizontal Flip (Along Y-axis)
2 : Vertical Flip (Along X-axis)
3 : Horizontal + Vertical Flip
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/791/TIOVX_5F00_Flip_5F00_Support.patch
2. PDK_Flip_Support.patch
Correction in the increment value done for Horizontal flip.
The correct value to the widthInBytes is widthInBytes + pipeCfg->inFmt.pitch[0] - 1.
Added CSL_DSS_VID1_ATTRIBUTES_FLIP_VAL_NOFLIP in case of No Flip option
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/791/PDK_5F00_Flip_5F00_Support.patch
3. Vision_Apps_Flip_Support.patch
Created additional user interface for flipping the source image by the user.
User could enter 'f' and then the corresponding flip type required as shown below :
v: Vertical Flip
h: Horizontal Flip
f: Full Flip
n: No Flip
Once the fliptype is selected, the Host send the information to the display node and the source image is flipped on the display.
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/791/VisionApps_5F00_Flip_5F00_Support.patch
Please find the patches for SDK 8.2 below