This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] C665x, C667x, K2E and K2H: IPC build in RTOS Processor SDK



How to build, compile and Install IPC libraries and binaries for C665x, C667x, K2E and K2H RTOS SDK? 

  • To Build IPC in BIOS (Windows environment) following requirements should be met,

    1. Requirements:
      1. IPC directory will be installed along with RTOS Processor SDK, Download Links for RTOS SDK are
      2. Also, we can install IPC packages without installing the whole SDK, Download links of variuos versions also available.
      3. XDC tools (XDC)
      4. TI CGT for building IPC binaries for C66x devices (TI-CGT-C6000 )
    2. Procedure
      1. Goto IPC installed folder and "XDC_INSTALL_DIR", "BIOS_INSTALL_DIR", "PDK_INSTALL_DIR" and target processor needs to be specified in make file
        1. Modify the "products.mak" by adding the following lines,
        2. XDC_INSTALL_DIR ?= C:\ccs_090300\xdctools_3_60_02_34_core
          BIOS_INSTALL_DIR ?= C:\ti\bios_6_76_03_01
          PDK_INSTALL_DIR ?= C:\ti\pdk_c665x_2_0_16\packages
          ti.targets.elf.C66 ?= C:\ccs_090300\ccs\tools\compiler\ti-cgt-c6000_8.3.11
      2.  While in the same folder, open command prompt by typing "cmd" in address bar in windows explorer and then give the following commands,
        1. C:\ti\ipc_3_50_04_07>..\xdctools_3_55_02_22_core\gmake.exe -f ipc-bios.mak all
        2. IPC binaries will be Compiled and built successfully.
      3. Also attached the IPC guide for
        1. BIOS(Windows) : IPC_Install_Guide_BIOS.pdf
        2. Linux : 3051.IPC_Install_Guide_Linux.pdf
        3. QNX : IPC_Install_Guide_QNX.pdf

    Thanks,

    Rajarajan U