Other Parts Discussed in Thread: AM1707, OMAP-L138, AM1808
Hi,
I am trying to load the ramdisk.gz(from the DaVinci-PSP-SDK-03.20.00.08 package) to my customized AM1707 board which is pin to pin compatible with OMAPL137
case1: ramdisk
--------------------------
The package contains two filesystem images viz. ramdisk-base.gz(3.1MB) and ramdisk.gz(12MB) , we have loaded ramdisk-base.gz successfully with the following u-boot environment variables set:
I have used ymodem to load the filesystem and uImage to the board , since there was some problem with the ethernet hardware.
setenv bootcmd 'nand read.e 0xc1180000 0x400000 0x400000; nboot.e 0xc0700000 0 0x200000; bootm'
setenv bootargs mem=32M console=ttyS2,115200n8 root=/dev/ram0 rw initrd=0xc1180000,4M ip=off
After the above steps i successfully booted the kernel.
But , when i used the other the complete ramdisk.gz (12MB) then i saw that kernel does not come up. It is giving the following error
oading from NAND 512MiB 3,3V 8-bit, offset 0x200000
Image Name: Linux-2.6.33-rc4
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1989996 Bytes = 1.9 MB
Load Address: c0008000
Entry Point: c0008000
## Booting kernel from Legacy Image at c0700000 ...
Image Name: Linux-2.6.33-rc4
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1989996 Bytes = 1.9 MB
Load Address: c0008000
Entry Point: c0008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Linux version 2.6.33-rc4 (x0029463@psplinux051) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #1 PREEMPT Tue Nov 9 18:0
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
CPU: VIVT data cache, VIVT instruction cache
Machine: DaVinci DA830/OMAP-L137/AM17xx EVM
Memory policy: ECC disabled, Data cache writethrough
DaVinci da830/omap-l137 rev2.0 variant 0x9
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 8128
Kernel command line: mem=32M console=ttyS2,115200n8 root=/dev/ram0 rw initrd=0xc1180000,4M ip=off
PID hash table entries: 128 (order: -3, 512 bytes)
Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)
Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)
Memory: 32MB = 32MB total
Memory: 24148KB available (3764K code, 296K data, 140K init, 0K highmem)
SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Hierarchical RCU implementation.
NR_IRQS:245
Console: colour dummy device 80x30
Calibrating delay loop... 227.73 BogoMIPS (lpj=1138688)
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
DaVinci: 128 gpio irqs
NET: Registered protocol family 16
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
pcf857x: probe of 1-003f failed with error -121
Switching to clocksource timer0_0
musb_hdrc: version 6.0, cppi4.1-dma, host, debug=0
Waiting for USB PHY clock good...
musb_hdrc: USB Host mode controller at fee00000 using DMA, IRQ 58
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 1024 (order: 1, 8192 bytes)
TCP bind hash table entries: 1024 (order: 0, 4096 bytes)
TCP: Hash tables configured (established 1024 bind 1024)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
rootfs image is not initramfs (no cpio magic); looks like an initrd
Freeing initrd memory: 4096K
JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.
msgmni has been set to 55
io scheduler noop registered (default)
Serial: 8250/16550 driver, 3 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO 0x1c42000 (irq = 25) is a 16550A
serial8250.0: ttyS1 at MMIO 0x1d0c000 (irq = 53) is a 16550A
serial8250.0: ttyS2 at MMIO 0x1d0d000 (irq = 61) is a 16550A
console [ttyS2] enabled
brd: module loaded
at24 1-0050: 32768 byte 24c256 EEPROM (writable)
spi_davinci spi_davinci.0: DaVinci SPI driver in EDMA mode
Using RX channel = 14 , TX channel = 15 and event queue = 1
m25p80 spi0.0: non-JEDEC variant of w25x32
m25p80 spi0.0: w25x32 (4096 Kbytes)
Creating 3 MTD partitions on "m25p80":
0x000000000000-0x000000040000 : "U-Boot"
0x000000040000-0x000000044000 : "U-Boot Environment"
0x000000044000-0x000000400000 : "Linux"
spi_davinci spi_davinci.0: Controller at 0xfec41000
console [netcon0] enabled
netconsole: network logging started
ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
ohci ohci.0: DA8xx OHCI
ohci ohci.0: new USB bus registered, assigned bus number 2
ohci ohci.0: irq 59, io mem 0x01e25000
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
tsc2004: probe of 1-0049 failed with error -121
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
omap_rtc: RTC power up reset detected
i2c /dev entries driver
Linux video capture interface: v2.00
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v0.1.0)
watchdog watchdog: heartbeat 60 sec
davinci_mmc davinci_mmc.0: Using DMA, 4-bit mode
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
Advanced Linux Sound Architecture Driver Version 1.0.21.
usbcore: registered new interface driver snd-usb-audio
No device for DAI tlv320aic3x
asoc: tlv320aic3x <-> davinci-i2s mapping ok
ALSA device list:
#0: DA830/OMAP-L137 EVM (tlv320aic3x)
TCP cubic registered
NET: Registered protocol family 17
Clocks: disable unused aemif
Clocks: disable unused emac
davinci_emac_probe: using random MAC addr: fe:10:18:90:a6:6c
emac-mii: probed
omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
RAMDISK: gzip image found at block 0
RAMDISK: EOF while reading compressed data
uncompression error
EXT2-fs (ram0): warning: mounting unchecked fs, running e2fsck is recommended
VFS: Mounted root (ext2 filesystem) on device 1:0.
Freeing init memory: 140K
EXT2-fs (ram0): error: ext2_lookup: deleted inode referenced: 4001
Warning: unable to open an initial console.
EXT2-fs (ram0): error: ext2_lookup: deleted inode referenced: 4009
EXT2-fs (ram0): error: ext2_lookup: deleted inode referenced: 4005
Kernel panic - not syncing: Attempted to kill init!
Backtrace:
[<c002f718>] (dump_backtrace+0x0/0x114) from [<c02f32f4>] (dump_stack+0x18/0x1c)
r7:c1c20000 r6:c1c20000 r5:000c72bc r4:c0403ab8
[<c02f32dc>] (dump_stack+0x0/0x1c) from [<c02f335c>] (panic+0x64/0x13c)
[<c02f32f8>] (panic+0x0/0x13c) from [<c00427dc>] (do_exit+0x74/0x6b4)
r3:c03e1160 r2:00000000 r1:c1c23f60 r0:c0382dc0
[<c0042768>] (do_exit+0x0/0x6b4) from [<c0042ee4>] (do_group_exit+0xc8/0xfc)
[<c0042e1c>] (do_group_exit+0x0/0xfc) from [<c0042f30>] (sys_exit_group+0x18/0x24)
r5:000c72bc r4:000c72e0
[<c0042f18>] (sys_exit_group+0x0/0x24) from [<c002bf20>] (ret_fast_syscall+0x0/0x28)
Please let us know whether our environment variable setting is wrong. It would be great if you can send us the correct u-boot bootargs and bootcmd settings.
case2 : using JFFS2
-----------------------------
Incase of using jffs2 iam getting the following error
setenv bootargs mem=32M console=ttyS2,115200n8 root=/dev/mtdblock4 rw rootfstype=jffs2 ip=off
error is as follows ( i have not copied the complete boot up log ,only the error is copied at the tail end)
............................
ALSA device list:
#0: DA830/OMAP-L137 EVM (tlv320aic3x)
TCP cubic registered
NET: Registered protocol family 17
Clocks: disable unused emac
davinci_emac_probe: using random MAC addr: 0e:8b:69:db:50:cb
emac-mii: probed
omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
Root-NFS: No NFS server available, giving up.
VFS: Unable to mount root fs via NFS, trying floppy.
List of all partitions:
No filesystem could mount root, tried: jffs2
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)
Please suggest the solution in case of ramdisk or jffs2. We are looking to flash either using jffs2 or ramdisk
thanks
lokesh