This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] 66AK2E05: How to flash the u-boot into SPI of K2E ?? using PROCESSOR-SDK-LINUX-K2E

Part Number: 66AK2E05

HI,

How to flash the u-boot into SPI of K2E ?? using  PROCESSOR-SDK-LINUX-K2E

Regards

Shankari G

  • Pre-requisite 

    1. Linux-PC with Ubuntu 18.04 LTS
    2. Download " PROCESSOR-SDK-LINUX-K2E — Linux Processor SDK for K2E " from https://www.ti.com/tool/PROCESSOR-SDK-K2E
    3. Rebuild the u-boot by following this FAQ : https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1106109/faq-66ak2e05-how-to-build-u-boot-for-k2e-from-the-package-processor-sdk-linux-k2e

    Steps:

    1. copy u-boot from the built image folder to the tftp boot folder.
    ====================================================


    shankari@shankari-Latitude-E7470:~/ti-processor-sdk-linux-k2e-evm-06.03.00.106/board-support/u-boot-2019.01+gitAUTOINC+333c3e72d3-g333c3e72d3$ cp -rf u-boot-spi.gph /tftpboot/u-boot-spi_shank.gph

    2. host/server network configuration - Set the ip address manually.
    ======================================================


    shankari@shankari-Latitude-E7470:~/ti-processor-sdk-linux-k2e-evm-06.03.00.106/board-support/linux-4.19.94+gitAUTOINC+be5389fd85-gbe5389fd85$ ifconfig

    enp0s31f6: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 1500
            ether d4:81:d7:d1:60:e8  txqueuelen 1000  (Ethernet)
            RX packets 0  bytes 0 (0.0 B)
            RX errors 0  dropped 0  overruns 0  frame 0
            TX packets 136  bytes 25658 (25.6 KB)
            TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
            device interrupt 16  memory 0xe1200000-e1220000  

    lo: flags=73<UP,LOOPBACK,RUNNING>  mtu 65536
            inet 127.0.0.1  netmask 255.0.0.0
            inet6 ::1  prefixlen 128  scopeid 0x10<host>
            loop  txqueuelen 1000  (Local Loopback)
            RX packets 4450  bytes 303900 (303.9 KB)
            RX errors 0  dropped 0  overruns 0  frame 0
            TX packets 4450  bytes 303900 (303.9 KB)
            TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

    wlp1s0: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 1500
            inet 192.168.43.191  netmask 255.255.255.0  broadcast 192.168.43.255
            inet6 2401:4900:25ee:4e4:f042:bcd8:59e2:22ef  prefixlen 64  scopeid 0x0<global>
            inet6 2401:4900:25ee:4e4:d77:bf2e:aded:87af  prefixlen 64  scopeid 0x0<global>
            inet6 fe80::491f:2f81:870:f42a  prefixlen 64  scopeid 0x20<link>
            ether 14:ab:c5:a1:2a:70  txqueuelen 1000  (Ethernet)
            RX packets 633979  bytes 838345136 (838.3 MB)
            RX errors 0  dropped 0  overruns 0  frame 0
            TX packets 191510  bytes 23601148 (23.6 MB)
            TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

    ==================================================
    No Ip address is set above, so pls set manually like below.

    ==================================================


    sudo ifconfig enp0s31f6 10.100.1.10 up

    ifconfig

    3. On device - terminal, please set the environment variables such as serverip and EVM's ipaddress like below.
    ==========================================================================================

    K2E EVM # setenv ethact K2F_EMAC0   --- down port
    K2E EVM # setenv ethact K2E_EMAC1   --- top port
    K2E EVM # setenv eth1addr 01:02:03:04:05:06
    K2E EVM # setenv eth2addr 01:02:03:04:05:07
    K2E EVM # setenv ipaddr 10.100.1.11
    K2E EVM # setenv serverip 10.100.1.10
    K2E EVM # saveenv

    K2E EVM # ping 10.100.1.10
    Using K2E_EMAC1 device
    host 10.100.1.10 is alive

    4. Issue tftpboot command

    ======================

    K2E EVM # tftpboot 0x88000000 u-boot-spi_shank.gph

    Using K2E_EMAC1 device


    ---
    Please get the size of the u-boot and change the offset accordingly.

    For example, the size of the u-boot image size is 0xa1216 and for spi flashing, the size used approximately is  0x100000 ( adding some buffer memory and rounded off the value. These adding buffer and rounding off is not necessary for SPI-flash. You can use the size, 0Xa1216, directly.

    May be for NAND with ECC, it might be meaning ful.

    ---

    5 Flashing uboot into SPI:
    ===================

    K2E EVM # sf probe
    SF: Detected N25Q128A with page size 64 KiB, total 16 MiB

    (Offset depends on u-boot image size )


    K2E EVM # sf erase 0 0x100000


    K2E EVM # sf write 0x88000000 0 0x100000

    ===================

    Please have a look at the snapshot for each flashing steps.

    -----------------------------------

    DIP SWITCH setting

    SW1 : 0 0 1 0

    Press powerON reset button

    The newly built u-boot will get booted from the SPI flash

    Please verify the Date and timestamp of the u-boot built with the output messages from the device-terminal.

    For example, I built the u-boot on 14 May 2022 , and here it shows the same date, 14 May 2022

    ---------------------------------------

    Regards

    Shankari G