This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] TMS320C6678: How to utilize the clock ticks to measure the time taken for the code execution?

Part Number: TMS320C6678
Other Parts Discussed in Thread: MATHLIB

Hi,

How to utilize the clock ticks to measure the time taken for the code execution?

  • How to utilize the clock ticks to measure the time taken for the code execution?

    Type 1: FOR PDK / SDK examples, which encloses the CSL library.

    Type 2: For other Mathlib package which doesnot enclose the CSL library.

    ---

    For cycle time, the following methods shall be used.

    ================

    This will make use of the clock ticks/cycles of DSP core running at  1000  MHz and it will be precise...

    =================

    Type 1:  FOR PDK / SDK examples, which encloses the CSL library.

    Code snippet: 

    //Start-Declaration  for time ticks

    #include "C:\ti\pdk_keystone2_3_01_04_07\packages\ti\csl\csl_tsc.h"

    //<ti/csl/csl_tsc.h> // check the path where the csl_tsc.h is located. Accordingly include the path of the file.

    extern uint32_t utilReadTime32();

    //End-Declaration  for time ticks

    ......

    /*Throughput calculation initialization */


    unsigned int StartTime = 0;
    unsigned int EndTime = 0;
    unsigned int Total_cycle_ticks = 0;

    /*Throughput calculation initialization Ends */

    .......

    //Usage 

    /* Enable the time stamp counter. */
    CSL_tscEnable();

    StartTime = utilReadTime32();

    // Please insert your code here 

    sauConnDmPktTest(tf, pat,
    100, /* Number of packets per connection */
    512, /* initial payload length */
    0, /* payload llength increment step */
    SAU_PAYLOAD_INC8 /* payload pattern */
    );


    EndTime = utilReadTime32();

    Total_cycle_ticks = EndTime-StartTime;


     System_printf("StartTime = %d \n", StartTime);
     System_printf("EndTime = %d \n", EndTime);

     System_printf("Total_cycle_ticks = %d \n", Total_cycle_ticks);


    // System_printf(" sauConnDmPktTest 2048 PacketSize, 100 packets -Total_cycle_ticks = %d \n", Total_cycle_ticks);

    ------------------

    Time tick calculation , you can use according to the number of Total_cycle_ticks, you get......

    Total no of CPU cycles =    cycles 

    DSP core frequency = 1000 MHz

     

    Time = 1 / Freq ( General formula )

              = 1 / 1000 MHz ( DSP core frequency )

              = 0.001 us ( Micro seconds) 

     

    1000000000 cycles = 1 sec

    =>32149501  cycles =  0.032 sec

    -----------------------

    Type 2: For other Mathlib package which doesnot enclose the CSL library.

    Pre-requisite : 

    Download and install "PROCESSOR-SDK-RTOS-C667x  06_03_00_106"
    from https://software-dl.ti.com/processor-sdk-rtos/esd/C667x/latest/index_FDS.html

    ( Please install the SDK in the recommended path: C:\ti\)

    This will include the CSL library.

    --

     utilize the "TSCH" to calculate the cycles taken for the function, "atan2sp_v"

    Steps:

    In the file, atan2sp_d.c, do the following.

    Step 1:

    1. extern void  CSL_tscEnable(void); // This function is part of CSL library. We have to include  library, "ti.csl.ae66" located in the C:\ti\pdk_c667x_2_0_15\packages\ti\csl\lib\c6678\c66\release\ti.csl.ae66 in the project configuration. ( Look at the snapshot below )

    Step 2:

    2. Declare these variables.

    /*Throughput calculation initialization */

    unsigned int StartTime = 0;
    unsigned int EndTime = 0;
    unsigned int Total_cycle_ticks = 0;

    /*Throughput calculation initialization Ends */

    Step 3:

    3. Define the utilReadTime32() function.

    /*****************************************************************************
    * Function: Utility function a cycle clock
    ****************************************************************************/
    extern cregister volatile unsigned int TSCL;

    uint32_t utilReadTime32()
    {
    uint32_t timeVal;
    timeVal = TSCL;
    return timeVal;
    }

    Step 4:

    /* Enable the time stamp counter. */
    CSL_tscEnable();

    StartTime = utilReadTime32();
    atan2sp_v (a_sc, b_sc, output[MTH_FCN_VEC], NUM_SC_INPUTS*NUM_SC_INPUTS);
    EndTime = utilReadTime32();

    Total_cycle_ticks = EndTime-StartTime;
    printf("StartTime = %d \n", StartTime);
    printf("EndTime = %d \n", EndTime);

    printf("Total_cycle_ticks = %d \n", Total_cycle_ticks);

    ---

    The modified source file is available here: 

    /* ======================================================================== *
     * MATHLIB -- TI Floating-Point Math Function Library                       *
     *                                                                          *
     *                                                                          *
     * Copyright (C) 2011 Texas Instruments Incorporated - http://www.ti.com/   *
     *                                                                          *
     *                                                                          *
     *  Redistribution and use in source and binary forms, with or without      *
     *  modification, are permitted provided that the following conditions      *
     *  are met:                                                                *
     *                                                                          *
     *    Redistributions of source code must retain the above copyright        *
     *    notice, this list of conditions and the following disclaimer.         *
     *                                                                          *
     *    Redistributions in binary form must reproduce the above copyright     *
     *    notice, this list of conditions and the following disclaimer in the   *
     *    documentation and/or other materials provided with the                *
     *    distribution.                                                         *
     *                                                                          *
     *    Neither the name of Texas Instruments Incorporated nor the names of   *
     *    its contributors may be used to endorse or promote products derived   *
     *    from this software without specific prior written permission.         *
     *                                                                          *
     *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS     *
     *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT       *
     *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR   *
     *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT    *
     *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,   *
     *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT        *
     *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,   *
     *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY   *
     *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT     *
     *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE   *
     *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.    *
     * ======================================================================== */
    
    /* ======================================================================= */
    /* atan2sp_d.h - arctangent two argument driver file                       */
    /* ======================================================================= */
    //Shankari-Start-Declaration  for time ticks
    //#include "C:\ti\pdk_c667x_2_0_16\packages\ti\csl\csl_tsc.h"
    //#include <ti/csl/csl_tsc.h>
    
    //extern uint32_t utilReadTime32();
    //Shankari-End-Declaration  for time ticks
    //Shankari declare the CSL_tscEnable as extern.
    extern void  CSL_tscEnable(void);
    
    #include <float.h>
    #include <stdio.h>
    #include <math.h>
    #include <stdlib.h>
    
    #include <ti/mathlib/src/common/common.h>
    #include <ti/mathlib/src/common/drvsp.h>
    #include "atan2sp.h"
    
    
    /* ======================================================================== */
    /*  Defines for driver test functionality                                   */
    /* ======================================================================== */
    /*Throughput calculation initialization */
    
    unsigned int StartTime = 0;
    unsigned int EndTime = 0;
    unsigned int Total_cycle_ticks = 0;
    
    /*Throughput calculation initialization Ends */
    
    /* Range for random inputs:  RAND_OFFSET to (RAND_RANGE + RAND_OFFSET) */
    #define RAND_RANGE   (2*MTH_TWO_PI)
    #define RAND_OFFSET  ( -MTH_TWO_PI)
    
    /*  Number of input arguments */
    #define NUM_INPUTS      (201)
    #define NUM_SC_INPUTS     (6)
    #define NUM_EXT_INPUTS  (237)
    
    /* Floating Point Tolerances */
    #define RET_VAL_TOL    (1e-6)
    
    /* Number of random test values */
    #define BUF_SIZE        (128)
    
    /* Function name */
    #define KERNEL_NAME  "atan2SP"
    
    /* Equality comparison requirements */
    #define KERNEL_REQ   (MTH_REQ_PERCENT)
    
    
    /* ======================================================================== */
    /*  Pre-defined input test data                                             */
    /* ======================================================================== */
    
    float a [NUM_INPUTS] = {
    /*   0 -  09 */  2.3135381,  1.8968619, -0.0756768,  0.8868028, -0.9800547,  0.1826697, -1.1155889, -1.0483080,  1.6465753, -0.8641856,
    /*  10 -  19 */ -0.8528155, -1.9450655, -2.6390254,  0.5221994,  2.8218998, -0.9806798, -3.1345328, -1.9067114, -2.3209479,  1.0272207,
    /*  20 -  29 */  2.8233285,  2.6390254,  1.1275215,  1.3495004, -2.9128084, -1.9651832, -2.5642326,  1.8925702, -2.3064093, -2.1316203,
    /*  30 -  39 */  0.4856401,  2.7499643,  1.9174446,  1.3146485, -2.7798670,  2.2517497, -1.0791098, -0.4656905, -1.9318173, -3.0600822,
    /*  40 -  49 */  1.4257409,  0.8000701, -0.9783753,  0.4934743,  1.3673927, -1.0034392,  0.6332442, -0.3479142,  1.5669944, -1.1302520,
    /*  50 -  59 */  1.6678470, -1.8060988,  3.0330084, -2.9716971, -0.9224464, -1.7681531, -1.2403497,  0.9910658,  0.7251339,  0.0664521,
    /*  60 -  69 */ -1.1956786, -2.4353275,  0.0850895,  2.2100750, -1.0904034, -3.0326055,  1.3948207,  1.3624830, -0.6940544,  1.3543253,
    /*  70 -  79 */  0.8774785, -1.1167824, -1.5397275, -1.4583951, -0.7318605,  0.4957987, -0.5997590, -0.2675051,  1.8631171, -2.2671664,
    /*  80 -  89 */ -2.9832040,  1.7920738, -0.5029850, -0.9580196, -2.9132679, -0.2031369,  0.2392143, -1.2708957, -2.7262275, -0.3890131,
    /*  90 -  99 */ -2.3026158,  1.7395388, -0.1722220, -0.8664596,  2.6893643, -1.2955357, -1.1141723,  0.6524964, -1.0036292, -2.5341911,
    /* 100 - 109 */ -0.6030755, -1.4845922,  0.1847009, -2.2969809, -1.7284012, -2.1670837, -0.9162604, -2.6918627, -3.0926890,  1.9026916,
    /* 110 - 119 */ -0.6157909, -1.2167198,  1.3122679, -0.2426267,  2.9885612,  2.7933659,  3.0079707, -2.5318231, -2.4902929,  1.9892559,
    /* 120 - 129 */ -1.8243082, -0.6330179,  0.1249213, -0.2402831, -0.0144180,  1.7226800,  1.2449822, -2.1712261,  1.0182503, -0.9841044,
    /* 130 - 139 */  1.8955267,  2.3830600, -1.5845531,  2.8392730,  1.5114688, -1.1034743,  0.0325057, -2.1286954, -2.3589811,  2.7031802,
    /* 140 - 149 */ -0.5401727, -1.5467144, -1.2573473,  2.0498470,  1.0994474, -1.6878354, -1.2113809,  2.3451656,  1.1922679,  1.9623993,
    /* 150 - 159 */  2.6861392,  0.9585329,  0.6380016, -0.4698215,  0.9541665, -0.2773711, -1.5496726, -1.6967815,  1.1994481, -1.2693016,
    /* 160 - 169 */ -1.7465209, -2.4450130,  2.9895873,  2.6623165,  1.8586202,  0.9722465, -2.2202118,  1.7101600,  3.0139285, -2.0721991,
    /* 170 - 179 */  0.5109130, -2.9975483, -0.0452963,  1.1814785, -0.8643483,  0.4049361,  1.8757297,  2.9287528, -1.3302178, -3.1057060,
    /* 180 - 189 */ -2.8633637, -0.1973840,  2.4147408,  1.1097204, -2.3930683, -0.7517271, -0.6176767,  0.7760660,  0.7684358,  0.6968723,
    /* 190 - 199 */  1.7993756,  0.6814629,  2.3639156,  1.7913911,  1.4757554, -2.4254864,  2.6482566, -1.6377824,  0.8112791, -0.9589719,
    /* 200 - 200 */  0.0636593,
    };
    
    float b [NUM_INPUTS] = {
    /*   0 -  09 */ -91.2572958,  18.7408531, -53.8650442, -75.7569229,  96.3077229,  -7.6091001, -19.2073345,  90.0992421,   8.8307813,  58.0715861,
    /*  10 -  19 */ -55.1536422,  82.1953898,  90.7922245,  70.3973330,  54.3926883,  27.9326546, -70.8640362,  28.7746900,  67.9949544,  -4.3990179,  
    /*  20 -  29 */  56.3853689,  72.7330394,  89.7958760,   0.6506345, -53.2568907,  90.5001414, -34.3886068,   0.1867002,  18.4165466, -89.5764153,  
    /*  30 -  39 */  86.0586351,  96.1277471,  33.6452472, -93.5818388, -13.4470613, -65.5907704, -99.7548511,  -4.3503695, -56.5984360, -97.3693208,  
    /*  40 -  49 */  66.9302629,  39.2945708, -19.9401670, -65.2324650, -72.0181957,  40.9931386,  62.4405059, -93.5376590,  20.1598249, -49.2629567,  
    /*  50 -  59 */  97.3422339,  38.1619053,  24.9950952,  57.8565606, -59.7228016,  94.3208155, -33.4966502,   1.9489241, -13.1378145, -17.3492702,  
    /*  60 -  69 */  15.8208954, -40.3999316, -21.6943411, -46.7005935,  83.4348239,  56.1003863,  -0.9574840,   3.5718092,  26.1776647, -42.3677828,  
    /*  70 -  79 */  75.9682995,  71.6556690,  43.3485769,  74.3978270, -17.6547310,  40.5521602,  79.0387887, -37.0366985,  32.3184751, -64.2953153,  
    /*  80 -  89 */  21.3656540, -79.2134105,  87.1901856, -72.6390439, -99.0990864, -10.6543498, -51.6327866, -68.6458331,  93.0084248, -45.0833611,  
    /*  90 -  99 */ -37.1702853,   5.1907654, -83.6970233, -52.2043266,  21.5931263, -51.1775924,  32.6228238,  40.7333065, -41.1037088, -92.1953541,  
    /* 100 - 109 */  47.8323105,  51.2813626, -46.9896947, -27.5270931, -87.4029587, -59.7726969, -74.5733577, -25.9424445, -78.4035322,  12.3785878,  
    /* 110 - 119 */ -58.3340343,  89.3806460, -89.5980000, -85.7810516,  12.0531909,  40.0593417,  61.7391895,  40.9334400,  87.7929490,  88.5997007,  
    /* 120 - 129 */ -99.2242204, -73.7385827,  67.2410088,  43.0963350,  93.5867665,  51.0842296,  -8.7863589,  55.6547355,  54.9392907,  37.9593670,  
    /* 130 - 139 */  41.4129360,  21.6191053, -58.7140204,  53.4582739, -50.1859543, -21.1997344,  51.5337994,  10.5222224, -14.6191417, -89.4206358,  
    /* 140 - 149 */  28.6006195, -37.8060334, -35.7869307, -55.6486036,  61.7771647, -92.8920502,  47.2177382, -50.7940962,  82.0212409, -12.0875024,  
    /* 150 - 159 */ -64.5874273, -60.2094873, -38.0300459,  89.7133750,  76.1698976,  73.2225305, -76.2539171,  42.4176305,  60.8972830,  51.4205129,  
    /* 160 - 169 */ -71.9763577,  19.9461477,  22.6601886, -80.4704549,  80.2687399, -60.5444334,  40.8969899,  66.7207540,  31.5421414,  60.5660213,  
    /* 170 - 179 */ -63.2807533,  26.1853248, -24.6500728, -10.7415857,  76.0305761,  73.5657775,  49.2212160,  73.1837210, -32.8017910,  30.0932223,  
    /* 180 - 189 */ -65.3040785,   4.7972407,  64.1718504,  57.8754685,  55.7897783,  20.5711835, -35.8692133,  67.7430589, -18.7016050,  98.6509677,  
    /* 190 - 199 */   6.7179056, -90.9222510,  24.8186046, -36.4573513,  77.1555061, -23.1775585,  40.8544334,  82.2189711,   2.3360194,  11.5269520,  
    /* 200 - 200 */  31.0396471,  
    };
    
    /*****************************************************************************
     * Function: Utility function a cycle clock
     ****************************************************************************/
    //shankari
    extern cregister volatile unsigned int TSCL;
    
    uint32_t utilReadTime32()
    {
        uint32_t timeVal;
        timeVal = TSCL;
        return timeVal;
    }
    
    /* ======================================================================== */
    /*  Main test driver                                                        */
    /* ======================================================================== */
    
    void main()
    {
      int i, j, k;  
    
        
      /* ======================================================================== */
      /*  INITIALIZATION                                                          */
      /* ======================================================================== */
    
      /* Initialize the driver */
      driver_init (KERNEL_NAME);
    
    
      /* ======================================================================== */
      /*  PREDEFINED TEST DATA                                                    */
      /* ======================================================================== */
    
      /* Obtain results using predefined test vectors */
      for (i = 0; i < NUM_INPUTS ; i++) {
        output[MTH_FCN_RTS][i] = atan2f (a[i],b[i]);
      }
      for (i = 0; i < NUM_INPUTS ; i++) {
        output[MTH_FCN_ASM][i] = atan2sp (a[i],b[i]);
      }
      for (i = 0; i < NUM_INPUTS; i++) {
        output[MTH_FCN_CI][i] = atan2sp_c (a[i],b[i]);
      }
      for (i = 0; i < NUM_INPUTS ; i++) {
        output[MTH_FCN_INL][i] = atan2sp_i (a[i],b[i]);
      }
      atan2sp_v (a, b, output[MTH_FCN_VEC], NUM_INPUTS);
    
      /* Check results and display */
      allequal (NUM_INPUTS, RET_VAL_TOL, KERNEL_REQ);
      print_test_results (MTH_TST_PREDEF);
    
      /* ======================================================================== */
      /*  SPECIAL CASE and EXTENDED RANGE TEST DATA                               */
      /* ======================================================================== */
    
      /* Obtain results using special case test vectors */
      a_sc[0] = b_sc[0] = 0;
      a_sc[1] = b_sc[1] = _itof(0x80000000);
      a_sc[2] = b_sc[2] = _itof(0x7F800000);
      a_sc[3] = b_sc[3] = _itof(0xFF800000);
      a_sc[4] = b_sc[4] = 1;
      a_sc[5] = b_sc[5] = -1;
      i = NUM_SC_INPUTS;
      for (j = 1; j < NUM_SC_INPUTS ; j++) {
        for (k = 0; k < NUM_SC_INPUTS ; k++) {
          a_sc[i] = a_sc[k];
          b_sc[i] = b_sc[(j+k)%NUM_SC_INPUTS];
          i++;
        }
      }
      i = 0;
      for (j = 0; j < NUM_SC_INPUTS ; j++) {
        for (k = 0; k < NUM_SC_INPUTS ; k++) {
          output[MTH_FCN_RTS][i] = atan2 (a_sc[i],b_sc[i]);
          output[MTH_FCN_ASM][i] = (b_sc[i] < 0) ? atan2(a_sc[i],b_sc[i]) : atan2sp(a_sc[i],b_sc[i]); // ignore Asm result when b is negative
          output[MTH_FCN_CI] [i] = atan2sp_c (a_sc[i],b_sc[i]);
          output[MTH_FCN_INL][i] = atan2sp_i (a_sc[i],b_sc[i]);
          i++;
        }
      }
      /* Enable the time stamp counter. */
      CSL_tscEnable();
    
      StartTime = utilReadTime32();
      atan2sp_v (a_sc, b_sc, output[MTH_FCN_VEC], NUM_SC_INPUTS*NUM_SC_INPUTS);
      EndTime = utilReadTime32();
    
      Total_cycle_ticks = EndTime-StartTime;
      printf("StartTime = %d \n", StartTime);
      printf("EndTime = %d \n", EndTime);
    
      printf("Total_cycle_ticks = %d \n", Total_cycle_ticks);
    
      /* Check results and display */
      allequal (NUM_SC_INPUTS*NUM_SC_INPUTS, RET_VAL_TOL, KERNEL_REQ);
      print_test_results (MTH_TST_SPECIAL);
    
      /* Obtain results using extended range test vectors */
      a_ext[0] = FLT_MIN;
      b_ext[0] = 1.;
      for (i = 0; i < NUM_EXT_INPUTS ; i++) {
        output[MTH_FCN_RTS][i] = atan2 (a_ext[i],b_ext[i]);
        output[MTH_FCN_ASM][i] = atan2sp (a_ext[i],b_ext[i]);
        output[MTH_FCN_CI] [i] = atan2sp_c (a_ext[i],b_ext[i]);
        output[MTH_FCN_INL][i] = atan2sp_i (a_ext[i],b_ext[i]);
        a_ext[i+1] = a_ext[i] * 2.1;
        b_ext[i+1] = b_ext[i] *(-1.);
      }
      atan2sp_v (a_ext, b_ext, output[MTH_FCN_VEC], NUM_EXT_INPUTS);
    
      /* Check results and display */
      allequal (NUM_EXT_INPUTS, RET_VAL_TOL, KERNEL_REQ);
      print_test_results (MTH_TST_EXTENDED);
    
      /* ======================================================================== */
      /*  RANDOM TEST DATA & PROFILING                                            */
      /* ======================================================================== */
        
      // Time the fastRTS inline function
      profile_init (MTH_FCN_INL);
      for (i = 0; i < BUF_SIZE; i++) {
        /* Fill input random data vectors */
        input[0][i] = gimme_random (RAND_RANGE, RAND_OFFSET);
        input[1][i] = gimme_random (RAND_RANGE, RAND_OFFSET);
        
        /* Run the inline routine */
        profile_start ();
        output[MTH_FCN_INL][i] = atan2sp_i (input[0][i],input[1][i]);
        profile_update (MTH_FCN_INL);
      }
      profile_avg (MTH_FCN_INL, BUF_SIZE);
      
      // Time the RTS function 
      profile_init (MTH_FCN_RTS);
      for (i = 0; i < BUF_SIZE; i++) {
        output[MTH_FCN_RTS][i] = atan2f (input[0][i],input[1][i]);
      }
      profile_update (MTH_FCN_RTS);
      profile_avg    (MTH_FCN_RTS, BUF_SIZE);
    
      // Time the fastRTS ASM function
      profile_init (MTH_FCN_ASM);
      for (i = 0; i < BUF_SIZE; i++) {
        output[MTH_FCN_ASM][i] = atan2sp (input[0][i],input[1][i]);
      }
      profile_update (MTH_FCN_ASM);
      profile_avg    (MTH_FCN_ASM, BUF_SIZE);
    
      // Time the fastRTS C intrinsic function
      profile_init (MTH_FCN_CI);
      for (i = 0; i < BUF_SIZE; i++) {
        output[MTH_FCN_CI][i] = atan2sp_c (input[0][i],input[1][i]);
      }
      profile_update (MTH_FCN_CI);
      profile_avg    (MTH_FCN_CI, BUF_SIZE);
    
      // Time the fastRTS vector function
      profile_init (MTH_FCN_VEC);
      atan2sp_v (input[0], input[1], output[MTH_FCN_VEC], BUF_SIZE);
      profile_update (MTH_FCN_VEC);
      profile_avg    (MTH_FCN_VEC, BUF_SIZE);
    
      /* Display Random Test Vector Results */
      allequal (BUF_SIZE, RET_VAL_TOL, KERNEL_REQ);
      print_test_results (MTH_TST_RANDOM);
      print_hline ();
      
      /* ======================================================================== */
      /*  CYCLE AND MEMORY REQUIREMENTS                                           */
      /* ======================================================================== */
    
      /* Display profiling results */
      print_profile_results (KERNEL_NAME);
    
      /* Display memory requirements */
      print_memory_results (KERNEL_NAME);
    }
    
    /* ======================================================================== */
    /*  End of file: atan2sp_d.c                                                */
    /* ======================================================================== */
    
    
    

    Output console messages :

    [C66xx_0]

    --------------------------------------------------------------------------------
    Verification Results: atan2SP
    --------------------------------------------------------------------------------
    Pre-defined Data: Passed
    StartTime = 7
    EndTime = 864
    Total_cycle_ticks = 857
    Special Case Data: Failed (ASM,C,INL,VEC)
    Extended Range Data: Passed
    Random Data (seed = 30578): Passed
    --------------------------------------------------------------------------------

    --------------------------------------------------------------------------------
    Cycle Profile: atan2SP
    --------------------------------------------------------------------------------
    RTS: 363 cycles
    ASM: 126 cycles
    C: 126 cycles
    Inline: 472 cycles
    Vector: 21 cycles
    --------------------------------------------------------------------------------

    --------------------------------------------------------------------------------
    Memory Profile: atan2SP
    --------------------------------------------------------------------------------
    ASM: 0 bytes
    C: 896 bytes
    Vector: 2688 bytes
    --------------------------------------------------------------------------------

    Time tick calculation , you can use according to the number of Total_cycle_ticks, you get......

    ------------------

    Step 5:

    Total no of CPU cycles =    cycles 

    DSP core frequency = 1000 MHz

     

    Time = 1 / Freq ( General formula )

              = 1 / 1000 MHz ( DSP core frequency )

              = 0.001 us ( Micro seconds) 

     

    1000000000 cycles = 1 sec

    =>32149501  cycles =  0.032 sec

    -----------------> here we receive Total_cycle_ticks = 857 ===> ( (1/1000000000) * 857 = 0.000000857 seconds )

    ---------------------------

    snapshot to include the CSL library in the build configuration:

    Regards

    Shankari G