Part Number: TDA4VM
Can we start running an OpenVX application automatically at Linux Boot
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VM
Can we start running an OpenVX application automatically at Linux Boot
In order to start an OpenVX application automatically during Linux boot, you could call the application in a service.
Please follow the below steps to achieve this
Step 1: Boot the EVM and login as 'root'
Step 2: Create a shell script in which you call the executable for your application along with its dependencies
(A sample shell script (appl.sh) is as shown below which loads the TIDL demo)
/cfs-file/__key/communityserver-discussions-components-files/1132/1856.appl.sh
Step 3: Save this shell script in /etc/init.d/
Step 4: Create a Systemd Unit File in /lib/systemd/system/ as shown below
sudo vi /lib/systemd/system/application.service
Step 5: Add the following contents and save the file
[Unit] Description=My Shell Script
[Service] ExecStart=/etc/init.d/appl.sh
[Install] WantedBy=multi-user.target
Step 6: Enable the new service as shown below
sudo systemctl daemon-reload
sudo systemctl enable application.service
sudo systemctl start application.service
Step 7: Verify the script is up and running with the below command
sudo systemctl status application.service
==============================
The output should look like below
==============================
* application.service - My Shell Script
Loaded: loaded (/lib/systemd/system/application.service; enabled; vendor preset: disabled)
Active: active (running) since Tue 2022-08-30 11:43:32 UTC; 11min ago
Main PID: 697 (appl.sh)
Tasks: 9 (limit: 16491)
Memory: 45.4M
CGroup: /system.slice/application.service
|-697 /bin/sh /etc/init.d/appl.sh
|-698 /opt/vision_apps/vx_app_arm_remote_log.out
`-746 /opt/vision_apps/vx_app_tidl.out --cfg /opt/vision_apps/app_oc.cfg
Aug 30 11:43:33 j721s2-evm appl.sh[698]: [C7x_1 ] 702.612181 s: APP: Run ... Done !!!
Aug 30 11:43:33 j721s2-evm appl.sh[698]: [C7x_1 ] 702.613379 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] C7X_1[s] C7X_2[P]
Aug 30 11:43:33 j721s2-evm appl.sh[698]: [C7x_1 ] 702.625081 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[P] C7X_1[s] C7X_2[P]
Aug 30 11:43:33 j721s2-evm appl.sh[698]: [C7x_1 ] 702.666312 s: IPC: Echo status: mpu1_0[x] mcu2_0[P] mcu2_1[P] C7X_1[s] C7X_2[P]
Aug 30 11:43:33 j721s2-evm appl.sh[698]: [C7x_2 ] 693.963430 s: CIO: Init ... Done !!!
Aug 30 11:43:33 j721s2-evm appl.sh[698]: [C7x_2 ] 693.963445 s: ### CPU Frequency = 1000000000 Hz
Aug 30 11:43:33 j721s2-evm appl.sh[698]: [C7x_2 ] 693.963456 s: APP: Init ... !!!
Aug 30 11:43:33 j721s2-evm appl.sh[698]: [C7x_2 ] 693.963464 s: SCICLIENT: Init ... !!!
Aug 30 11:43:33 j721s2-evm appl.sh[698]: [C7x_2 ] 693.963584 s: SCICLIENT: DMSC FW version [8.4.1--v08.04.01 (Jolly Jellyfi]
Aug 30 11:43:33 j721s2-evm appl.sh[698]: [C7x_2 ] 693.963599 s: SCICLIENT: DMSC FW revision 0x8
==============================
Step 8: Reboot the EVM and your OpenVX application automatically runs during Linux boot
Regards,
Nikhil