Other Parts Discussed in Thread: AM3874
4403.questions-GPMC_WAIT2.xlsxHi,
I asked GPMC_WAIT signal of AM3874 before. But I have more question from our customer.
Q1) I was advised that there is no specific timing between GPMC_WAIT deassersion and assertion again in before question. Is this meaning that next GPMC_WAIT signal can assert as soon as the previous GPMC_WAIT is recoginzed? Of course it assumes WAITMONITERINGTIME is kept.
Q2) According to the FIG.11-8 of TRM, WAIT signal only needs to satisfy WAITMONITERINGTIME for D0. D1, D2 and D3 doesn't need to satisfy it, do it?
Q3) I was advised WAIT signal toggle in WAIT inactive period is not effect, but it is not recommended. According to the additional information, customer would like to use one WAIT pin for multiple CS(Customer would like to use both Asynchronous I/F and Synchronous I/F each CS(Chip Select) with one WAIT pin). Can TI guarantee the GPMC of AM3874 with this use?
Q4) According to the data sheet(Fig 8-21 to Fig. 8-26), the assertion of GPMC_WAIT signal is doen when GPMC_ADV_ALE signal is low. Is there any timing requirement between GPMC_WAIT and GPMC_ADV_ALE?
Q5) Multiple(Burst) and Singl access is configured each CS(chip select) on GPMC register . If Burst (multiple access if synchronous) is set, it is occurred only burst cycle, single cycle never occurred. The burst length must be set in GPMC register. Which does this length represent variable length or fixed length?
I attached one excel file for Q1,Q2 and Q4. Please see it.
Best regards,
Michi