Other Parts Discussed in Thread: OMAP-L138
Hi,
I'd like to know, compared to L2RAM on DSP, what the speed of L3 shared memory.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OMAP-L138
Hi,
I'd like to know, compared to L2RAM on DSP, what the speed of L3 shared memory.
Thanks
Hello,
You'll find pasted below some brute measurement of OMAP-L138 DSP RAM throughput for 32-bit access that may be useful (personal data, not TI validated, no guaranty).
Jakez
| OMAP-L138 RAM 32-bit data access performance for DSP core (CPU rev. 2.0) |
||||||||
| Measures done by averaging the execution time of 1000 calls to pipelined loops | ||||||||
| operating sequential accesses to a buffer of 8K 32-bit words (32 KB) | ||||||||
| Notes: | ||||||||
| Write test : one write per buffer element, theorical min. 1 CPU cycle / element | ||||||||
| Read test : one read per buffer element, theorical min. 1 CPU cycle / element | ||||||||
| RMW test : one read & one write per buffer element, theorical min. 1 CPU cycle / element | ||||||||
| DDR2 SDRAM : 16-bit data bus, CAS latency=3, 8 banks, 2 KB pages, 4ms refresh | ||||||||
| DDR2 max throughput (bursts) : 3/10 32-bit word per CPU cycle = f(DDRCLK) / f(CPU) | ||||||||
| f(CPU) = 450 MHz, f(DDRCLK)=135 MHz (270 MHz/2) | ||||||||
| L1P cache active, ARM core & peripherals inactive, no interrupt | ||||||||
| When configured as caches, L1D is full cache (32 KB), L2 cache is 64 KB | ||||||||
| Data caches are emptied before each loop when used | ||||||||
| Test loops functions prolog/epilog execution time included | ||||||||
| Program is located in DDR2 SDRAM | ||||||||
| Measurements through DSP Time Stamp Counter (TSC) | ||||||||
| Performance unit : average CPU cycles / word; DDR2_CLK rel : average DDR_CLK cycle / word | ||||||||
| Native RAM performance (32-bit) | ||||||||
| L1D & L2 caches inactive - MARn registers are 0 (disabling cache on L3 & DDR2 domains) | ||||||||
| Test type \ RAM | L1D | L2 | L3 | DDR2 | DDR2 (CLK rel) | |||
| Read | 1.01 | 7.76 | 33.89 | 72.35 | 21.71 | |||
| Write | 1.01 | 1.01 | 18.01 | 18.56 | 5.57 | |||
| RMW | 1.01 | 11.38 | 54.25 | 108.49 | 32.55 | |||
| Cached RAM performance (32-bit) | ||||||||
| L1D & L2 caches active - MARn registers are 1 (enabling cache on L3 & DDR2 domains) | ||||||||
| Test type \ RAM | L2 | L3 | DDR2 | DDR2 (CLK rel) | ||||
| Read | 1.77 | 3.89 | 6.67 | 2.00 | ||||
| Write | 1.14 | 8.88 | 11.63 | 3.49 | ||||
| RMW | 1.87 | 3.94 | 6.68 | 2.00 | ||||
| L1 cache only performance (32-bit) | ||||||||
| L1D cache active only - MARn registers are 1 | ||||||||
| Test type \ RAM | L2 | L3 | DDR2 | DDR2 (CLK rel) | ||||
| Read | 1.84 | 4.72 | 8.76 | 2.63 | ||||
| Write | 1.18 | 18.15 | 18.68 | 5.60 | ||||
| RMW | 1.98 | 4.85 | 8.90 | 2.67 | ||||
| L2 cache only performance (32-bit) | ||||||||
| L2 cache active only - MARn registers are 1 | ||||||||
| Measure type \ RAM | L1D | L2 | L3 | DDR2 | DDR2 (CLK rel) | |||
| Read | 1.15 | 7.90 | 12.46 | 15.20 | 4.56 | |||
| Write | 1.13 | 1.13 | 8.88 | 11.62 | 3.49 | |||
| RMW | 1.17 | 11.54 | 18.23 | 21.02 | 6.31 | |||
| Disabled caching RAM performance (near native performance) | ||||||||
| L1D & L2 caches active but MARn registers are 0 | ||||||||
| Test type \ RAM | L2 | L3 | DDR2 | DDR2 (CLK rel) | ||||
| Read | 1.84 | 34.07 | 72.55 | 21.77 | ||||
| Write | 1.17 | 18.14 | 18.69 | 5.61 | ||||
| RMW | 1.98 | 54.44 | 108.68 | 32.60 | ||||
| The funny one (should be native performance for L3 & DDR2) | ||||||||
| L1D & L2 caches inactive but MARn registers are 1 | ||||||||
| Test type \ RAM | L1D | L2 | L3 | DDR2 | DDR2 (CLK rel) | |||
| Read | 1.01 | 7.76 | 56.01 | 120.56 | 36.17 | |||
| Write | 1.01 | 1.01 | 18.01 | 18.56 | 5.57 | |||
| RMW | 1.01 | 11.38 | 76.00 | 154.99 | 46.50 | |||