Other Parts Discussed in Thread: TVP5147M1, DM3730
Hi all,
when we start a camera to preview program(which modified from saMmapLoopback.c),
Normally,it is ok to show preview image to LCD,
but,sometimes,we start a camera to preview program,we have an occasion to occur "CCDC won't become idle!" issue
such that we cann't see any preview image @ LCD,
and once this message happened,we always see this messages,and cann't see preview image even when we turn off and turn on the
program again
the following is detail description:
Environment:
Hardware: (1) DM3730 associated with TVP5147M1
(2) connnection lines between the 2 are
CAM_D0 ~ CAM_D9
CAM_PCLK/CAM_HS/CAM_VS/CAM_WEN
I2C interface (SCL/SDA)
INTREQ (currently this interrupt function be disable by tvp514x driver)
PWDN
RESETB
(3) external CCD sensor connected to TVP5147M1 CVBSin 2B channel
Software: under Android 2.3.4
and use Camera 2 vout loopback program as image preview program
which refer to and modified from saMmapLoopback.c mentioned from
Webside:UserGuideOmap35xCaptureDriver PSP 04.02.00.07,
http://processors.wiki.ti.com/index.php/UserGuideOmap35xCaptureDriver_PSP_04.02.00.07
Other Info:(1)Camera sensor format is NTSC (720x480)
(2)we have connection CVBSin channel @ TVP5147M1 2B channel
(3)the protocol between tvp5147M1 and ISPCCDC is BT656
(4)as I know,INTREQ between DM3730 and TVP5147M1 is not used now
(5)under Media Controller Framework @kernelV2.6.37,our link is tvp514x<->ISPCCDC<->Memory
(6) pixel clock is 27Mhz
Issue Description:
@our platform (DM3730 + TVP5147M1) and under Android/Linux evironment,
when we execute a camera capture 2 preview program which modified from saMmapLoopback.c ,
normally,we can see Image captured and show Image to our LCD panel,
sometimes and have an opportunity,
we cann't see preview image @ LCD when we start the camera capture 2 preview program,
by the way,the terminal show "CCDC won't become idle!" message,
and once this message happenS,we always see this messages,
and cann't see preview image even when we turn off and turn on the
camera to preview program again
the following is related CCDC configuration Registers dump:
omap3isp omap3isp: -------------CCDC Register dump-------------
omap3isp omap3isp: ###CCDC PCR=0x00000000
omap3isp omap3isp: ###CCDC SYN_MODE=0x00032f84
omap3isp omap3isp: ###CCDC HD_VD_WID=0x00000000
omap3isp omap3isp: ###CCDC PIX_LINES=0x00000000
omap3isp omap3isp: ###CCDC HORZ_INFO=0x0000059f
omap3isp omap3isp: ###CCDC VERT_START=0x00000000
omap3isp omap3isp: ###CCDC VERT_LINES=0x000000ef
omap3isp omap3isp: ###CCDC CULLING=0xffff00ff
omap3isp omap3isp: ###CCDC HSIZE_OFF=0x000005a0
omap3isp omap3isp: ###CCDC SDOFST=0x00000249
omap3isp omap3isp: ###CCDC SDR_ADDR=0x00000000
omap3isp omap3isp: ###CCDC CLAMP=0x00000010
omap3isp omap3isp: ###CCDC DCSUB=0x00000040
omap3isp omap3isp: ###CCDC COLPTN=0x00000000
omap3isp omap3isp: ###CCDC BLKCMP=0x00000000
omap3isp omap3isp: ###CCDC FPC=0x00000000
omap3isp omap3isp: ###CCDC FPC_ADDR=0x00000000
omap3isp omap3isp: ###CCDC VDINT=0x00ee0000
omap3isp omap3isp: ###CCDC ALAW=0x00000000
omap3isp omap3isp: ###CCDC REC656IF=0x00000003
omap3isp omap3isp: ###CCDC CFG=0x00008800
omap3isp omap3isp: ###CCDC FMTCFG=0x00006000
omap3isp omap3isp: ###CCDC FMT_HORZ=0x000002d0
omap3isp omap3isp: ###CCDC FMT_VERT=0x000001e0
omap3isp omap3isp: ###CCDC PRGEVEN0=0x00000000
omap3isp omap3isp: ###CCDC PRGEVEN1=0x00000000
omap3isp omap3isp: ###CCDC PRGODD0=0x00000000
omap3isp omap3isp: ###CCDC PRGODD1=0x00000000
omap3isp omap3isp: ###CCDC VP_OUT=0x03be2d00
omap3isp omap3isp: ###CCDC LSC_CONFIG=0x00006600
omap3isp omap3isp: ###CCDC LSC_INITIAL=0x00000000
omap3isp omap3isp: ###CCDC LSC_TABLE_BASE=0x00000000
omap3isp omap3isp: ###CCDC LSC_TABLE_OFFSET=0x00000000
omap3isp omap3isp: --------------------------------------------
could you have any suggetion to avoid/skip this issue ?
thanks a lot ~