Hi,
I would like to find a replacement SPI NOR flash for the C6678.
The NOR flash used in the C6678EVM is the old Numonyx part. I am having troubles getting lower quantities of these flashes.
I understand that there are various post already discussing about SPI NOR flash and booting from it. However, I am unable to find any post that has a clear answer on which NOR Flash is suitable for use with the C6678.
My main concern is that if I were to use an incompatible SPI NOR Flash, I will not be able to flash in my program into the NOR flash using JTAG.
Hence, I would appreciate if my following doubts can be answered:
- Is there a difference between the various types of NOR flash that can be used with the C6678 for booting and for flashing in programs?
- If there is, is there a specific document that documents which type of NOR flash is suitable to be used with C6678 such that I can not only boot from it, but also use the JTAG and an emulator to burn in my programs.
- Are there any other recommended SPI NOR flashes?