Other Parts Discussed in Thread: SYSBIOS
Hello,
Where is the documentation on the CSL for the C6670, using sysBios 6.33? In the folder ...\bios_6_33_04_39\docs I can find the Bios_User_Guide.pdf which just has passing references to the CSL. I looked there because at this link: http://processors.wiki.ti.com/index.php/Chip_support_library#Chip_Support_Library_for_C6670
I found this text: "The Chip Support Library for the C6670 device is delivered with the SYS/BIOS MultiCore SDK 2.0."
I can't find any other pointers to CSL docs. Any help would be appreciated.
The reason I'm looking for this is to find how to implement a timer without using SysBios in order to be able to create a very small IBL executable which will perform some simple platform testing as well as do the intermediate boot loading functionality.
Thanks,
Geraldine