Other Parts Discussed in Thread: ADS8471, OMAP-L138, ADS5560
I would like to know whether there is the ADC which can connect directly to uPP.
Here is a way to connect ADS8471 to OMAP-L138 via uPP.
http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/t/144344.aspx
A BUSY pin of ADS8471 is tied to a CHx_CLK pin of OMAP-L138. I guess that it does not meet the setup time.
Is not there the ADC which can connect directly to uPP?
Best regards,
Daisuke