Other Parts Discussed in Thread: OMAP-L137
Hello,
i try to enable the onboard soundcodec on an omap l137-evm.
I compiled the kernel (2.6.29-rc8-davinci1-06020-ge28a1e2-dirty) with ALSA for SoC audio support.
--- ALSA for SoC audio support
<*> SoC Audio for the TI DAVINCI chip
<*> SoC Audio support for DA830/OMAP-L137 EVM
< > Build all ASoC CODEC drivers
At kernelstartup is the following output:
[...]
i2c /dev entries driver
Advanced Linux Sound Architecture Driver Version 1.0.18a.
No device for DAI tlv320aic3x
No device for DAI davinci-i2s
No device for DAI davinci-dit
AIC3X Audio Codec 0.2
asoc: tlv320aic3x <-> davinci-i2s mapping ok
ALSA device list:
#0: DA830 EVM (tlv320aic3x)
TCP cubic registered
[...]
In the proc fs is the soundcard available:
#cat /proc/asound/card0/pcm0p/info
card: 0
device: 0
subdevice: 0
stream: PLAYBACK
id: AIC3X tlv320aic3x-0
name:
subname: subdevice #0
class: 0
subclass: 0
subdevices_count: 1
subdevices_avail: 1
The alsa utils don´t recognize the sound device!
#aplay -l
aplay: device_list:223: no soundcards found...
Any ideas how to get this working?
Whats todo for sound-specific content in the /dev folder?
Thank you very much.