We know the 720P H264 encoding is supported from 4.02 DVSDK, however, we want to know whether only standard resolutions (VGA, D1, 720P) are supported and 800x600 resolution is not supported. When we use the demo application or our-self application written with DMAI to encode 800x600 resolution video, it always reports "failed to create h264enc". Can you help to confirm this?
BTW, we also want add some OSD data in the encoded video, however, we found the blend function isn't supported for DM3725. Is there any way to implement this? Thanks!