Hi,everyone,
I use srio interface between FPGA and DSP 6678, After running for a period of time, the SPx_ERR_DET become 0x100004 from 0x100000,which means thre is a SRIO delineation error . At this moment, if i use the function 'Srio_sockSend' to send a doorbell to fpga, it used about 3000ms, and return 0(no error code or response timeout). And then the communication is ok between 6678 and fpga, but after a period of time,may be some minutes or one hour, the run time of the function 'Srio_sockSend' is about 3000ms again, and so on....The SPx_ERR_DET is always 0x100004.
1、Does anybody know that how the SRIO Delineation Error generate?
2、 how to recover after this error?