This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)



hello ,

I used the EVM board dm365 with linux-2.6.18_pro500 and  arm_v5t_le- compiler  and now i have the DM355IPNC-VCA1 and i want to use the same version of linux and compiler , so i followed the procedure to build kernel for EVM board dm355 and i tried to boot the uImage with tftp and file systeme.

My question it's possible to use the same version of linux and the same compiler , if yes how i can resolve my problem because i have Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0) error.

Thank you !

output of my log boot :

DM355 IPNC # setenv bootargs console=ttyS1,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nfsroot=$(nfshost):$(rootpath), nolock mem=80M v4l2_c
DM355 IPNC # setenv bootcmd 'tftpboot 0x80700000 uImage; bootm 0x80700000'
DM355 IPNC # boot
Found DM9000 ID:90000a46 at address 4000000 !
DM9000 work in 16 bus width
[eth_init]MAC:0:11:22:33:44:55:
TFTP from server 192.168.1.66; our IP address is 192.168.1.119
Filename 'uImage'.
Load address: 0x80700000
Loading: T #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         #######
done
Bytes transferred = 2028592 (1ef430 hex)
## Booting image at 80700000 ...
   Image Name:   Linux-2.6.18_pro500-davinci_evm-
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2028528 Bytes =  1.9 MB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
OK

Starting kernel ...

Linux version 2.6.18_pro500-davinci_evm-arm_v5t_le (version gcc 4.2.0 (MontaVista 4.2.0-16.0.32.0801914 2008-08-30)) #0
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
Machine: DaVinci DM355 EVM
Memory policy: ECC disabled, Data cache writeback
DaVinci DM0350 variant 0x0
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Built 1 zonelists.  Total pages: 20480
Kernel command line: console=ttyS1,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nfsroot=192.168.1.66:/home/me/workdir/filesys, nolock mem=c
PID hash table entries: 512 (order: 9, 2048 bytes)
Clock event device timer0_0 configured with caps set: 07
Console: colour dummy device 80x30
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 80MB = 80MB total
Memory: 76672KB available (3481K code, 735K data, 196K init)
Security Framework v1.0.0 initialized
Capability LSM initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
NET: Registered protocol family 16
DaVinci: 104 gpio irqs
MUX: initialized SD1_CLK
MUX: initialized SD1_CMD
MUX: initialized SD1_DATA3
MUX: initialized SD1_DATA2
MUX: initialized SD1_DATA1
MUX: initialized SD1_DATA0
DM355 IPIPE intialized in Single Shot mode
ch0 default output "COMPOSITE", mode "NTSC"
VPBE Encoder Initialized
LogicPD encoder initialized
Avnetlcd encoder initialized
MUX: initialized I2C_SDA
MUX: initialized I2C_SCL
SCSI subsystem initialized
usbcore: registered new driver usbfs
usbcore: registered new driver hub
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 4096 bind 2048)
TCP reno registered
VFS: Disk quotas dquot_6.5.1
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
squashfs: version 3.1 (2006/08/19) Phillip Lougher
JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.
yaffs Jan 25 2010 11:23:13 Installing.
SGI XFS with no debug enabled
Initializing Cryptographic API
io scheduler noop registered
io scheduler anticipatory registered (default)
LTT : ltt-facilities init
LTT : ltt-facility-core init in kernel
davincifb davincifb.0: dm_osd0_fb: Initial window configuration is invalid.
davincifb davincifb.0: dm_osd0_fb: 720x576x16@0,0 with framebuffer size 2025KB
davincifb davincifb.0: dm_vid0_fb: 0x0x16@0,0 with framebuffer size 675KB
davincifb davincifb.0: dm_osd1_fb: 720x480x4@0,0 with framebuffer size 1350KB
davincifb davincifb.0: dm_vid1_fb: Initial window configuration is invalid.
davincifb davincifb.0: dm_vid1_fb: 720x576x16@0,0 with framebuffer size 2500KB
DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec
imp serializer initialized
davinci_previewer initialized
davinci_resizer initialized
Serial: 8250/16550 driver $Revision: 1.90 $ 3 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO map 0x1c20000 mem 0xfbc20000 (irq = 40) is a 16550A
serial8250.0: ttyS1 at MMIO map 0x1c20400 mem 0xfbc20400 (irq = 41) is a 16550A
serial8250.0: ttyS2 at MMIO map 0x1e06000 mem 0xfbe06000 (irq = 14) is a 16550A
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
dm9000 Ethernet Driver
dm9000: read wrong id 0x2b2a2928
dm9000: read wrong id 0x2b2a2928
dm9000: wrong id: 0x2b2a2928
dm9000: not found (0).
netconsole: not configured, aborting
Linux video capture interface: v2.00
vpfe_init
MUX: initialized VIN_CAM_WEN
MUX: initialized VIN_CINL_EN
starting ccdc_reset...<7>
End of ccdc_reset...<5>vpfe_probe
vpfe ccdc capture vpfe ccdc capture.1: vpif_register_decoder: decoder = MT9T001
vpfe ccdc capture vpfe ccdc capture.1: vpif_register_decoder: decoder = MT9P031
TVP514X : nummber of channels = 1
vpfe ccdc capture vpfe ccdc capture.1: vpif_register_decoder: decoder = TVP514X
Trying to register davinci display video device.
layer=c09fb800,layer->video_dev=c09fb960
Trying to register davinci display video device.
layer=c09fb600,layer->video_dev=c09fb760
davinci_init:DaVinci V4L2 Display Driver V1.0 loaded
af major#: 252, minor# 0
aew major#: 251, minor# 0
i2c /dev entries driver
nand_davinci nand_davinci.0: Using 4-bit hardware ECC
NAND device: Manufacturer ID: 0xec, Chip ID: 0x75 (Samsung NAND 32MiB 3,3V 8-bit)
2 NAND chips detected
Bad block table not found for chip 0
Bad block table not found for chip 1
Bad block table not found for chip 0
Bad block table not found for chip 1
Scanning device for bad blocks
Scanning device for bad blocks
Creating 5 MTD partitions on "nand_davinci.0":
0x00000000-0x003c0000 : "bootloader"
0x003c0000-0x00400000 : "params"
0x00400000-0x00800000 : "kernel"
0x00800000-0x20800000 : "filesystem1"
mtd: partition "filesystem1" extends beyond the end of device "nand_davinci.0" -- size truncated to 0x3800000
0x20800000-0x04000000 : "filesystem2"
mtd: partition "filesystem2" is out of reach -- disabled
nand_davinci nand_davinci.0: hardware revision: 2.3
dm_spi.0: davinci SPI Controller driver at 0xc5866000 (irq = 42) use_dma=0
Initializing USB Mass Storage driver...
usbcore: registered new driver usb-storage
USB Mass Storage support registered.
usbcore: registered new driver usbhid
drivers/usb/input/hid-core.c: v2.6:USB HID core driver
musb_hdrc: version 6.0, cppi-dma, host, debug=0
musb_hdrc musb_hdrc: No DMA interrupt line
musb_hdrc: USB Host mode controller at c586e000 using DMA, IRQ 12
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
usb usb1: configuration #1 chosen from 1 choice
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mice: PS/2 mouse device common for all mice
davinci-mmc davinci-mmc.0: Supporting 4-bit mode
davinci-mmc davinci-mmc.0: Using DMA mode
davinci-mmc davinci-mmc.1: Supporting 4-bit mode
davinci-mmc davinci-mmc.1: Using DMA mode
Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC).
ASoC version 0.13.1
AIC3X Audio Codec 0.2
ALSA device list:
  No soundcards found.
IPv4 over IPv4 tunneling driver
TCP bic registered
NET: Registered protocol family 1
NET: Registered protocol family 17
Time: timer0_1 clocksource has been installed.
Clock event device timer0_0 configured with caps set: 08
Switched to high resolution mode on CPU 0
IP-Config: No network devices available.
Looking up port of RPC 100003/2 on 192.168.1.66
portmap: RPC call returned error 101
Root-NFS: Unable to get nfsd port number from server, using default
Looking up port of RPC 100005/1 on 192.168.1.66
portmap: RPC call returned error 101
Root-NFS: Unable to get mountd port number from server, using default
mount: RPC call returned error 101
Root-NFS: Server returned error -101 while mounting /home/me/workdir/filesys
VFS: Unable to mount root fs via NFS, trying floppy.
VFS: Cannot open root device "nfs" or unknown-block(2,0)
Please append a correct "root=" boot option
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)

My Uboot environement :

DM355 IPNC # print env
## Error: "env" not defined
DM355 IPNC #printenv
Unknown command printenv' - try 'help'
DM355 IPNC # printenv
bootdelay=3
baudrate=115200
fileaddr=82000000
bootm=0x80700000
nboot=0x80700000 0 0x200000
bbootcmd=nand read 0x82000000 0x500000 0xa00000;nboot 0x80700000 0 0x200000;bootm 0x80700000
initrd=0x82000000,10M1stdin=serial
bootcmd=nand read 0x82000000 0x500000 0xa00000;nboot 0x80700000 0 0x200000;bootm 0x80700000
bootargs=mem=80M console=ttyS1,115200n8 root=/dev/ram0 rw initrd=0x82000000,10M ip=dhcp eth=00:11:45:11:03:55 v4l2_video_capture=:device=Mc
nfshost=192.168.1.66
bootfile=uImage
ipaddr=192.168.1.119
serverip=192.168.1.66
rootpath=/home/me/workdir/filesys
stdin=serial
stdout=serial
stderr=serial
ver=U-Boot 1.2.0 (Aug 12 2008 - 00:04:55) IPNC-U-1.0.2

Environment size: 797/16380 bytes

 

  • rblode said:
    IP-Config: No network devices available.
    Looking up port of RPC 100003/2 on 192.168.1.66
    portmap: RPC call returned error 101
    Root-NFS: Unable to get nfsd port number from server, using default
    Looking up port of RPC 100005/1 on 192.168.1.66
    portmap: RPC call returned error 101
    Root-NFS: Unable to get mountd port number from server, using default
    mount: RPC call returned error 101
    Root-NFS: Server returned error -101 while mounting /home/me/workdir/filesys
    VFS: Unable to mount root fs via NFS, trying floppy.
    VFS: Cannot open root device "nfs" or unknown-block(2,0)
    Please append a correct "root=" boot option
    Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)

    This is a bit unusual, it sounds like your kernel is not configured to use the network interface on the EVM somehow, you mention that you are working with the IPNC software, my suspicion is that the kernel for the IPNC reference design uses a different Ethernet driver than the EVM, and that this is preventing you from booting the same kernel properly on the EVM. Note that I do not have the IPNC reference design so I am not all that familiar with how it differs from the EVM, but the errors you have indicate the network is not coming up for some reason, and I would blame the kernel specifically since the same hardware is working earlier from U-Boot.

    To try to fix this you may want to try booting a pre built kernel that is included with the DVSDK, or try building the kernel again with the DVSDK getting started guide instructions.

    EDIT: I think I misunderstood your question and got things reversed, reading your first few words I was under the impression you were working with the EVM trying to run IPNC software, but it seems you are doing the reverse by using the IPNC kit and running EVM software. It should be possible to use the same tools to build for the IPNC, however you probably need to change some kernel build options to include whatever hardware support is needed for the IPNC, in this case it looks like the network driver is broken/missing.

  • Hi,

    Yes it looks strange that you have this at booting the kernel :

     

    dm9000 Ethernet Driver
    dm9000: read wrong id 0x2b2a2928
    dm9000: read wrong id 0x2b2a2928
    dm9000: wrong id: 0x2b2a2928
    dm9000: not found (0).

    1-it looks like your ethernet link is down.

    try to locate this message on a working configuration. If it is the same message the error is elsewhere (in such situation the drive loading messages would be weird).

    but it is strange because your uboot used tftp through the DM9000 ethernet device. so my 2nd suggestion

     

    2- my other suggestion is that if you read before your kernel panic, you notice that the transaction is closed because your platform ask your server to open the nfsd port and could not get the port (rpc).

    First ensure that your server PC has the right IP address, sometimes it changes at reboot if you use dhcp.

    Second, try to type the commands below when connecting in a console being "root" (as user you will not be able to type them)

    /sbin/service iptables stop (it will stop the firewall)

    /sbin/service nfs restart  (it will restart the nfs service)

    3- Of course the kernel that you have may be not configured for NFS, in this case you will have to recompile it with the right options and reflash it, and restart. but this is another story. Try the first 2 points before.

    Cheers

     

     

     

     

     

  •  

    Just a precision:

    The commands are to be typed on the server Linux PC, in a new terminal window (not the serial console). I was not clear.

    And connect as root on this terminal.

     

  • Bernie Thompson said:
    EDIT: I think I misunderstood your question and got things reversed, reading your first few words I was under the impression you were working with the EVM trying to run IPNC software, but it seems you are doing the reverse by using the IPNC kit and running EVM software. It should be possible to use the same tools to build for the IPNC, however you probably need to change some kernel build options to include whatever hardware support is needed for the IPNC, in this case it looks like the network driver is broken/missing.

    Thank you for the reply

    Yes i'm working with the EVM DM365 and now i try to use the same environement for the IPNCDM355-VCA1 , the question which build options i must change it ?.


  • Thank you for the reply

    reda38 said:

    Yes it looks strange that you have this at booting the kernel :

     

    dm9000 Ethernet Driver
    dm9000: read wrong id 0x2b2a2928
    dm9000: read wrong id 0x2b2a2928
    dm9000: wrong id: 0x2b2a2928
    dm9000: not found (0).

    Yes i see this but i select dm9000 Ethernet Driver when i builded the kernel , i followed the getting start with the default value of configuratio

    reda38 said:

    1-it looks like your ethernet link is down.

    try to locate this message on a working configuration. If it is the same message the error is elsewhere (in such situation the drive loading messages would be weird).

    but it is strange because your uboot used tftp through the DM9000 ethernet device. so my 2nd suggestion

     

    I agree with you because on Uboot I can ping without problem which show that the driver works well and even ftp it works also

    reda38 said:

    2- my other suggestion is that if you read before your kernel panic, you notice that the transaction is closed because your platform ask your server to open the nfsd port and could not get the port (rpc).

    First ensure that your server PC has the right IP address, sometimes it changes at reboot if you use dhcp.

    Second, try to type the commands below when connecting in a console being "root" (as user you will not be able to type them)

    /sbin/service iptables stop (it will stop the firewall)

    Yes I thought about that but I have no problem with the DM365 EVM card, although I get to mount the filesys no problem with the same host platforme

    reda38 said:
    3- Of course the kernel that you have may be not configured for NFS, in this case you will have to recompile it with the right options and reflash it, and restart. but this is another story. Try the first 2 points before.

    I used the default configuration following the getting start guide

  • rblode said:
    Yes i'm working with the EVM DM365 and now i try to use the same environement for the IPNCDM355-VCA1 , the question which build options i must change it ?.

    Unfortunately I do not have an IPNC kit so I have not really worked with it much and could not say what options would have to be changed. Though the build tools can probably be the same you may have to do some additional patch work to get the kernel that came with the EVM to run on the IPNC kit, I am not sure that it would include all the code needed for the IPNC in the kernel (primarily drivers for any hardware differences, in this case the Ethernet). In other words, I am not sure what Appro had to modify in the kernel to get the IPNC to work, whatever they had to do,  you would have to do as well.

    What kernel version are you running on the IPNC? If it is a close enough version to the one you were running on the EVM than I would probably just try to stick with it and port the rest of your higher level software stack instead. If the kernel versions are different than porting around the driver code is a possibility to make the EVM kernel run on the IPNC kit however that could prove to be a lot of work.

  • rblode said:

    I agree with you because on Uboot I can ping without problem which show that the driver works well and even ftp it works also

    Please note that u-boot does basic hardware initialization to make sure Kernel and File-system can be found and loaded properly.  However, once u-boot serves its purposes, its initialization of hardware is overriden by the hardware initialization done by the kernel.  Hence the fact that you can ping in u-boot simply implies your hardware appears to be functioning ok, but does not guarantee the kernel will not override the hardware settings when it tries to load its inthernet driver, perhaps causing ethernet hardware to stop working (especially if driver assumes dm900 ethernet part and a different part is found on IPNC); I believe this is the point Bernie has been describing, there are likely differences between IPNC hardware vs EVM hardware and the kernel you use must account for those differences. 

  • Bernie Thompson said:
    What kernel version are you running on the IPNC? If it is a close enough version to the one you were running on the EVM than I would probably just try to stick with it and port the rest of your higher level software stack instead. If the kernel versions are different than porting around the driver code is a possibility to make the EVM kernel run on the IPNC kit however that could prove to be a lot of work.

    the default version of IPNC is Linux kernel version: 2.6.10_mvl401 , i tried to run my sample code directly in this version but i have  "segmentation falut" error

    if it's not possible to use my environement of dm365  you know where i cn find the toolchaine for this version of kernel.

     

    Thank you

  • thank you Juan for this informations , now i see the the difference

  • Hello

    There is still a strange point in your question. Let me explain :

    You said this :

    "[...] EVM board dm365 with linux-2.6.18_pro500 and  arm_v5t_le- compiler  and now i have the DM355IPNC-VCA1 [...]"


    I think the main source of your problem comes from the different target you have :

    EVM365 is base on DM365, this chip includes an Ethernet MAC.

    DM355IPNC-VCA1 is based on DM355, this chip does not include an Ethernet MAC but instead uses the Davicom DM9000 Ethernet MAC+PHY

    The thing that happens is that if you put the kernel forecast for DM355 on a platform for DM365 you will get problems. There are probably other peripherals which will cause problems.

    So when loading your DM355 kernel configured to use DM9000 on the EVM365, there will be the message you got.

    What you need in my opinion is either you get EVM355, or you get DM365IPNC-VCA1 which i do not know if it exists.

     

    Just my 2 cents contribution.


  • reda38 said:
    "[...] EVM board dm365 with linux-2.6.18_pro500 and  arm_v5t_le- compiler  and now i have the DM355IPNC-VCA1 [...]"

    I used EVM board dm365 in the first and now i try to use DM355IPNC-VCA1

    reda38 said:
    The thing that happens is that if you put the kernel forecast for DM355 on a platform for DM365 you will get problems. There are probably other peripherals which will cause problems.

    i put the kernel forecast for EVM-DM355 on a platform DM355IPNC-VCA1

  • This is a great catch by reda38.  All DM365 DVSDKs have been based on MV Pro 5 thus far; whereas, DM355 DVSDKs have been based on MV Pro 4 (dvsdk 1.30) or MV Pro 5 (dvsdk 2.0).  Aside from this, there are fundametal differences in the parts, hence using a DM365 kernel on DM355 will likely reduce further any chance of your IPNC system working.

    Did you know there is a DM365-based IPNC available

    http://www.appropho.com/NewWeb/Product_DM365IMX035_Product.php

    If you decide to stick with DM355 IPNC, then perhaps a closer match would be the DVSDK 1.3 for DM355 available at

    http://software-dl.ti.com/dsps/dsps_registered_sw/sdo_sb/targetcontent/dvsdk/mv_dvsdk/index.html

    The kernel included in this DVSDK is at least based on the same tool chain (MV Pro 4) and developed for the same platform (DM355); though this does not guarantee it will work, you would still need to accoung for any hardware differences between the DM355 EVM and the DM355 IPNC.  That said, is there a good reason you do not want to use the kernel provided with the DM355-IPNC?

     

     

  • Juan Gonzales said:

    http://www.appropho.com/NewWeb/Product_DM365IMX035_Product.php

    If you decide to stick with DM355 IPNC, then perhaps a closer match would be the DVSDK 1.3 for DM355 available at

    http://software-dl.ti.com/dsps/dsps_registered_sw/sdo_sb/targetcontent/dvsdk/mv_dvsdk/index.html

    Thank you Juan for the link

    Juan Gonzales said:
    The kernel included in this DVSDK is at least based on the same tool chain (MV Pro 4) and developed for the same platform (DM355); though this does not guarantee it will work, you would still need to accoung for any hardware differences between the DM355 EVM and the DM355 IPNC.  That said, is there a good reason you do not want to use the kernel provided with the DM355-IPNC?

    I want to use the kernel Pro 5 because i  can use my program that i do with the evm-dm365

     

  • well, from you previous comments above, it appears DM355 IPNC software you are using is based on MV Pro 4.0; therefore, if you move to an MV Pro 5 kernel, you would need to update more than just the kernel, you would also need to upgarde the file system.  In this case, I would contact the third party that you bough DM355 IPNC from and see if they have a newer MV Pro 5 -based Linux stack.

    Worst case, scenerio you can try porting DVSDK 2.0 to IPNC enviroment but this will likely result in challenges such as the one you are running into.  Hence it may be worth your time to figure out if Appro or whoever you bought the IPNC from has already done this.

  • hi bernie

    well my kernel is working for bootm command but

    whenever i m going for tftp boot the following things are coming

    BOOTP broadcast 1                                                                                                                                                                                                                                           
    DHCP client bound to address 192.168.72.135                                                                                                                                                                                                                 
    TFTP from server 192.168.72.136; our IP address is 192.168.72.135                                                                                                                                                                                           
    Filename 'uImage'.                                                                                                                                                                                                                                          
    Load address: 0x80700000                                                                                                                                                                                                                                    
    Loading: T T T T T T T T T T T T T T T T T T T T                                                                                                                                                                                                            
    Retry count exceeded; starting again                                                                                                                                                                                                                        
    BOOTP broadcast 1                                                                                                                                                                                                                                           
    DHCP client bound to address 192.168.72.135                                                                                                                                                                                                                 
    TFTP from server 192.168.72.136; our IP address is 192.168.72.135                                                                                                                                                                                           
    Filename 'uImage'.                                                                                                                                                                                                                                          
    Load address: 0x80700000                                                                                                                                                                                                                                    
    Loading: T T...........
    continue like that

    well tftp is set same as given in GSG and it is set to

    i m not able to short out the problem

    thanks

    vs

  • vigneshwaran sekar said:
    TFTP from server 192.168.72.136; our IP address is 192.168.72.135                                                                                                                                                                                           
    Filename 'uImage'.                                                                                                                                                                                                                                          
    Load address: 0x80700000                                                                                                                                                                                                                                    
    Loading: T T T T T T T T T T T T T T T T T T T T                                                                                                                                                                                                            
    Retry count exceeded; starting again   

    The Ts you see indicate timeout events, as in U-Boot sent a request to the TFTP server and did not hear back, this sort of issue is mentioned in many other threads on the forums as well. This could be caused by a few different things, such as the TFTP server not running, having the wrong server address, or having a firewall on the server preventing the TFTP server from operating. I would probably start by ensuring you can ping the server properly.