This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

can 6678 boot from i2c eeprom + nand flash?



dear sir:

  i'm developing a system based on c6678. In order to simplify the design, the nor flash on the evm board from 

advantech is removed. Now I doubt if the system can boot just by i2c eeprom and nand flash?

  I read some article in this forum which point out that the codes in i2c eeprom do some initialization, then the dsp

can access the nand and boot flow jumps to the nand code, then boot can be completed, can it really work?

  If I want to run the linux, is this architecture OK?

thanks!