This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

kernel hangs

Hi All,

            I'm using a custom board based on AM33x EVM. The processor is DRA608 J5(similar to AM335x). I did

make tisdk_am335x-evm_defconfig and make, generated images. I flashed the images onto NOR using uboot.

when it boots I get print, "starting kernel ... " from "uboot". There afterwards it hangs. What should i do? what can be the reason?

Regards,

Gangadhar

  • prints

    U-Boot# loadx 0x80200000                                                                                                  
    ## Ready for binary (xmodem) download to 0x80200000 at 115200 bps...                                                      
    CxyzModem - CRC mode, 32171(SOH)/0(STX)/0(CAN) packets, 3 retries                                                      
    ## Total Size      = 0x003ed460 = 4117600 Bytes                                                                           
    U-Boot# loadx 0x80F80000                                                                                                  
    ## Ready for binary (xmodem) download to 0x80F80000 at 115200 bps...                                                      
    CxyzModem - CRC mode, 264(SOH)/0(STX)/0(CAN) packets, 5 retries                                                      
    ## Total Size      = 0x000081d3 = 33235 Bytes                                                                             
    U-Boot# bootz 0x80200000 - 0x80F80000                                                                                     
    Kernel image @ 0x80200000 [ 0x000000 - 0x3ed460 ]                                                                         
    ## Flattened Device Tree blob at 80f80000                                                                                 
       Booting using the fdt blob at 0x80f80000                                                                               
       Loading Device Tree to 8f32a000, end 8f3351d2 ... OK                                                                   
                                                                                                                              
    Starting kernel ...     

    I've modified my dts/dtb file for my board.

    Regards,

    Gangadhar

  • Hi Gangadhar,

    I will contact the factory team about support for the processor you are using.

  • thankyou Biser. I tried with two sets of dts file.

    1. 1st dts; retaining only uarts from am335x-evm.dts , adding nor flash to it. I've attached this one.

    2. 2nd dts: completely changed with pin mux for my custom board. I've attached this dts as well as the pin mux file.


    Please see it.

    Regards,

    Gangadhar

    /*
     * Copyright (C) 2012 Texas Instruments Incorporated - http://www.ti.com/
     *
     * This program is free software; you can redistribute it and/or modify
     * it under the terms of the GNU General Public License version 2 as
     * published by the Free Software Foundation.
     */
    /dts-v1/;
    
    #include "am33xx.dtsi"
    
    / {
    	model = "TI AM335x EVM";
    	compatible = "ti,am335x-evm", "ti,am33xx";
    
    	cpus {
    		cpu@0 {
    			cpu0-supply = <&vdd1_reg>;
    		};
    	};
    
    	memory {
    		device_type = "memory";
    		reg = <0x80000000 0x10000000>; /* 256 MB */
    	};
    	
    	vdd1_reg: fixedregulator-dvp1_1v26_sw {
    		/* VDD_MPU voltage */
    		compatible = "regulator-fixed";
    		regulator-name = "vdd_mpu";
    		regulator-min-microvolt = <1260000>;
    		regulator-max-microvolt = <1260000>;
    		regulator-boot-on;
    		regulator-always-on;
    	};
    
    	am33xx_pinmux: pinmux@44e10800 {
    		pinctrl-names = "default";
    		pinctrl-0 = <&clkout2_pin>;
    
    
    		uart0_pins: pinmux_uart0_pins {
    			pinctrl-single,pins = <
    				0x170 (PIN_INPUT_PULLUP | MUX_MODE0)	/* uart0_rxd.uart0_rxd */
    				0x174 (PIN_OUTPUT_PULLDOWN | MUX_MODE0)	/* uart0_txd.uart0_txd */
    			>;
    		};
    
    		uart1_pins_default: pinmux_uart1_pins_default {
    			pinctrl-single,pins = <
    				0x178 (PIN_INPUT | MUX_MODE0)			/* uart1_ctsn.uart1_ctsn */
    				0x17C (PIN_OUTPUT_PULLDOWN | MUX_MODE0)	/* uart1_rtsn.uart1_rtsn */
    				0x180 (PIN_INPUT_PULLUP | MUX_MODE0)	/* uart1_rxd.uart1_rxd */
    				0x184 (PIN_OUTPUT_PULLDOWN | MUX_MODE0) 	/* uart1_txd.uart1_txd */
    			>;
    		};
    
    		uart1_pins_sleep: pinmux_uart1_pins_sleep {
    			pinctrl-single,pins = <
    				0x178 (PIN_INPUT_PULLDOWN | MUX_MODE7)
    				0x17C (PIN_INPUT_PULLDOWN | MUX_MODE7)
    				0x180 (PIN_INPUT_PULLDOWN | MUX_MODE7)
    				0x184 (PIN_INPUT_PULLDOWN | MUX_MODE7)
    			>;
    		};
    
    		clkout2_pin: pinmux_clkout2_pin {
    			pinctrl-single,pins = <
    				0x1b4 (PIN_OUTPUT_PULLDOWN | MUX_MODE3)	/* xdma_event_intr1.clkout2 */
    			>;
    		};
    
    		norflash_pins: norflash_pins {
    			pinctrl-single,pins = <
    
    				/*Data lines*/
    				0x0 (INPUT_EN | MUX_MODE0)	/* gpmc_ad0.gpmc_ad0 */
    				0x4 (INPUT_EN | MUX_MODE0)	/* gpmc_ad1.gpmc_ad1 */
    				0x8 (INPUT_EN | MUX_MODE0)	/* gpmc_ad2.gpmc_ad2 */
    				0xc (INPUT_EN | MUX_MODE0)	/* gpmc_ad3.gpmc_ad3 */
    				0x10 (INPUT_EN | MUX_MODE0)	/* gpmc_ad4.gpmc_ad4 */
    				0x14 (INPUT_EN | MUX_MODE0)	/* gpmc_ad5.gpmc_ad5 */
    				0x18 (INPUT_EN | MUX_MODE0)	/* gpmc_ad6.gpmc_ad6 */
    				0x1c (INPUT_EN | MUX_MODE0)	/* gpmc_ad7.gpmc_ad7 */
    				0x20 (INPUT_EN | MUX_MODE0)	/* gpmc_ad8.gpmc_ad8 */
    				0x24 (INPUT_EN | MUX_MODE0)	/* gpmc_ad9.gpmc_ad9 */
    				0x28 (INPUT_EN | MUX_MODE0)	/* gpmc_ad10.gpmc_ad10 */
    				0x2c (INPUT_EN | MUX_MODE0)	/* gpmc_ad11.gpmc_ad11 */
    				0x30 (INPUT_EN | MUX_MODE0)	/* gpmc_ad12.gpmc_ad12 */
    				0x34 (INPUT_EN | MUX_MODE0)	/* gpmc_ad13.gpmc_ad13 */
    				0x38 (INPUT_EN | MUX_MODE0)	/* gpmc_ad14.gpmc_ad14 */
    				0x3c (INPUT_EN | MUX_MODE0)	/* gpmc_ad15.gpmc_ad15 */
    
    				/*Addr lines*/
    				0xA0 (PIN_INPUT | MUX_MODE7)    /* lcd_data0.gpio2[6]*/
    				0xA4 (PIN_INPUT | MUX_MODE1)    /* lcd_data1.gpmc_a1_mux1*/
    				0xA8 (PIN_INPUT | MUX_MODE1)    /* lcd_data2.gpmc_a2_mux1*/
    				0xAC (PIN_INPUT | MUX_MODE1)    /* lcd_data3.gpmc_a3_mux1*/
    				0xB0 (PIN_INPUT | MUX_MODE1)    /* lcd_data4.gpmc_a4_mux1*/
    				0xB4 (PIN_INPUT | MUX_MODE1)    /* lcd_data5.gpmc_a5_mux1*/
    				0xB8 (PIN_INPUT | MUX_MODE1)    /* lcd_data6.gpmc_a6_mux1*/
    				0xBC (PIN_INPUT | MUX_MODE1)    /* lcd_data7.gpmc_a7_mux1*/
    				0xe0 (PIN_INPUT | MUX_MODE1)    /* lcd_vsync.gpmc_a8_mux1*/
    				0xe4 (PIN_INPUT | MUX_MODE1)    /* lcd_hsync.gpmc_a9_mux1*/
    				0xe8 (PIN_INPUT | MUX_MODE1)    /* lcd_pclk.gpmc_a10_mux1*/
    				0xec (PIN_INPUT | MUX_MODE1)    /* lcd_ac_bias_en.gpmc_a11_mux1*/
                                    0xC0 (PULL_DISABLE | MUX_MODE1) /* lcd_data8.gpmc_a12*/
                                    0xC4 (PULL_DISABLE | MUX_MODE1) /* lcd_data9.gpmc_a13*/
                                    0xC8 (PULL_DISABLE | MUX_MODE1) /* lcd_data10.gpmc_a14*/
                                    0xCC (PULL_DISABLE | MUX_MODE1) /* lcd_data11.gpmc_a15*/
                                    0xD0 (PULL_DISABLE | MUX_MODE1) /* lcd_data12.gpmc_a16_mux1*/
                                    0xD4 (PULL_DISABLE | MUX_MODE1) /* lcd_data13.gpmc_a17_mux1*/
                                    0xD8 (PULL_DISABLE | MUX_MODE1) /* lcd_data14.gpmc_a18_mux1*/
                                    0xDC (PULL_DISABLE | MUX_MODE1) /* lcd_data15.gpmc_a19_mux1*/
    				0xF0 (PIN_OUTPUT_PULLUP | MUX_MODE1) /*mmc0_dat3.gpmc_a20_mux1*/
    				0xF4 (PIN_OUTPUT_PULLUP | MUX_MODE1) /*mmc0_dat2.gpmc_a21_mux1*/
    				0xF8 (PIN_OUTPUT_PULLUP | MUX_MODE1) /*mmc0_dat1.gpmc_a22_mux1*/
    				0xFC (PIN_OUTPUT_PULLUP | MUX_MODE1) /*mmc0_dat0.gpmc_a23_mux1*/
    				0x100 (PIN_OUTPUT_PULLUP | MUX_MODE1) /*mmc0_clk.gpmc_a24_mux1*/
    
    				/*Control lines*/
    				0x70 (PIN_INPUT_PULLUP | MUX_MODE0)	/* gpmc_wait0.gpmc_wait0 */
    				0x7c (PIN_INPUT_PULLUP | MUX_MODE0)	/* gpmc_csn0.gpmc_csn0  */
    				0x94 (PIN_OUTPUT_PULLUP | MUX_MODE0)	/* gpmc_oen_ren.gpmc_oen_ren */
    				0x98 (PIN_INPUT_PULLUP | MUX_MODE0)	/* gpmc_wen.gpmc_wen */
    			>;
    		};
    
    
    	};
    
    	ocp {
    		uart0: serial@44e09000 {
    			pinctrl-names = "default";
    			pinctrl-0 = <&uart0_pins>;
    
    			status = "okay";
    		};
    
    		uart1: serial@48022000 {
    			pinctrl-names = "default", "sleep";
    			pinctrl-0 = <&uart1_pins_default>;
    			pinctrl-1 = <&uart1_pins_sleep>;
    
    			status = "okay";
    		};
    
    
    		gpmc: gpmc@50000000 {
    				status = "okay";
    				pinctrl-names = "default";
    				pinctrl-0 = <&norflash_pins>;
    				ranges = <0 0 0x08000000 0x02000000>;	/* CS0: NOR */
    
    				nor@0,0 {
    				compatible = "cfi-flash";
    				linux,mtd-name= "amd,s29gl256s";
    				#address-cells = <1>;
    				#size-cells = <1>;
    				reg = <0 0 0x02000000>;
    				bank-width = <2>;
    
    				gpmc,mux-add-data;
    				gpmc,cs-on-ns = <0>;
    				gpmc,cs-rd-off-ns = <186>;
    				gpmc,cs-wr-off-ns = <186>;
    				gpmc,adv-on-ns = <12>;
    				gpmc,adv-rd-off-ns = <48>;
    				gpmc,adv-wr-off-ns = <48>;
    				gpmc,oe-on-ns = <54>;
    				gpmc,oe-off-ns = <168>;
    				gpmc,we-on-ns = <54>;
    				gpmc,we-off-ns = <168>;
    				gpmc,rd-cycle-ns = <186>;
    				gpmc,wr-cycle-ns = <186>;
    				gpmc,access-ns = <114>;
    				gpmc,page-burst-access-ns = <6>;
    				gpmc,bus-turnaround-ns = <12>;
    				gpmc,cycle2cycle-delay-ns = <18>;
    				gpmc,wr-data-mux-bus-ns = <90>;
    				gpmc,wr-access-ns = <186>;
    				gpmc,cycle2cycle-samecsen;
    				gpmc,cycle2cycle-diffcsen;
    
    				partition@0 {
    					label = "uboot";
    					reg = <0 0x80000>;
    				};
    				partition@0x80000 {
    					label = "1st-copy-uboot-env";
    					reg = <0x80000 0x40000>;
    				};
    				partition@0xA0000 {
    					label = "2nd-copy-uboot-env";
    					reg = <0xA0000 0x40000>;
    				};
    				partition@0xC0000 {
    					label = "linux-kernel";
    					reg = <0xC0000 0x400000>;
    				};
    				partition@0x4C0000 {
    					label = "userland";
    					reg = <0x4C0000 0x1B40000>;
    				};
    			};
    		};
    
    
    
    	};
    
    };
    
    
    /*
     * Copyright (C) 2012 Texas Instruments Incorporated - http://www.ti.com/
     *
     * This program is free software; you can redistribute it and/or modify
     * it under the terms of the GNU General Public License version 2 as
     * published by the Free Software Foundation.
     */
    /dts-v1/;
    
    #include "am33xx.dtsi"
    
    / {
    	model = "DVP1 DRA608 J5 Echo";
    	compatible = "ti,am335x-evm", "ti,am33xx";
    
    	cpus {
    		cpu@0 {
    			cpu0-supply = <&vdd1_reg>;
    		};
    	};
    
    	memory {
    		device_type = "memory";
    		reg = <0x80000000 0x10000000>; /* 256 MB */
    	};
    		
    	vdd1_reg: fixedregulator-dvp1_1v26_sw {
    		/* VDD_MPU voltage */
    		compatible = "regulator-fixed";
    		regulator-name = "vdd_mpu";
    		regulator-min-microvolt = <1260000>;
    		regulator-max-microvolt = <1260000>;
    		regulator-boot-on;
    		regulator-always-on;
    	};
    		
    	vdd2_reg: fixedregulator-dvp1_1v1_sw {
    		/* VDD_CORE voltage */
    		compatible = "regulator-fixed";
    		regulator-name = "vdd_core";
    		regulator-min-microvolt = <1100000>;
    		regulator-max-microvolt = <1100000>;
    		regulator-boot-on;
    		regulator-always-on;
    	};
    		
    	dvp1_3v3_sw: fixedregulator-dvp1_3v3_sw {
    		compatible = "regulator-fixed";
    		regulator-name = "dvp1_3v3_sw";
    		regulator-min-microvolt = <3300000>;
    		regulator-max-microvolt = <3300000>;
    	};
    
    	am33xx_pinmux: pinmux@44e10800 {
    
    		i2c0_pins: pinmux_i2c0_pins {
    			pinctrl-single,pins = <
    				0x188 (PIN_INPUT | MUX_MODE0)	/* i2c0_sda.i2c0_sda */
    				0x18c (PIN_INPUT | MUX_MODE0)	/* i2c0_scl.i2c0_scl */
    			>;
    		};
    
    		i2c2_pins: pinmux_i2c2_pins {
    			pinctrl-single,pins = <
    				0x170 (PIN_INPUT | MUX_MODE3)	/* uart0_rxd.i2c2_sda */
    				0x174 (PIN_INPUT | MUX_MODE3)	/* uart0_txd.i2c2_scl */
    			>;
    		};
    
    		spi0_pins: pinmux_spi0_pins {
    			pinctrl-single,pins = <
    			0x150 (PIN_INPUT |  MUX_MODE0) /* spi0_sclk.spi0_sclk */
    			0x154 (PIN_INPUT |  MUX_MODE0) /* spi0_d0.spi0_d0 */
    			0x158 (PIN_INPUT |  MUX_MODE7) /* spi0_d1.gpio0[4] */
    			0x15C (PIN_INPUT |  MUX_MODE0) /* spi0_cs0.spi0_cs0 */
    			0x160 (PIN_INPUT |  MUX_MODE7) /* spi0_cs1.gpio0[6] */
    			>;
    		};
    
    		dcan0_pins: pinmux_dcan0_pins{
    			pinctrl-single,pins = <
    				0x178 (PULL_DISABLE | MUX_MODE2)  /*uart1_ctsn.dcan0_tx_mux2 */
    	        		0x17C (PIN_INPUT | MUX_MODE2)	  /*uart1_rtsn.dcan0_rx_mux2 */
    			>;
    		};
    
    		uart0_pins: pinmux_uart0_pins {
    		/*Not used*/
    			pinctrl-single,pins = <
    				0x168 (PIN_INPUT | MUX_MODE7)   /*uart0_ctsn.gpio1[8] */
    				0x16c (PIN_INPUT | MUX_MODE7)   /*uart0_rtsn.gpio1[9] */
    			>;
    		};
    
    		uart1_pins: pinmux_uart1_pins {
    			pinctrl-single,pins = <
    				0x180 (PIN_INPUT | MUX_MODE0)	 /* uart1_rxd.uart1_rxd */
    				0x184 (PULL_DISABLE | MUX_MODE0) /* uart1_txd.uart1_txd */
    			>;
    		};
    
    		uart2_pins: pinmux_uart2_pins {
    			pinctrl-single,pins = <
    				0x12C (INPUT_EN | MUX_MODE1)   /*mii1_txclk.uart2_rxd */
    				0x130 (INPUT_EN | MUX_MODE1)   /*mii1_rxclk.uart2_txd */
    			>;
    		};
    
    		uart5_pins: pinmux_uart5_pins {
    			pinctrl-single,pins = <
    				0x10C (INPUT_EN | MUX_MODE5)  /* mii1_crs.uart5_ctsn */
    	        		0x110 (PIN_OUTPUT_PULLDOWN | MUX_MODE5)	  /* mii1_rxerr.uart5_rtsn */
    				0x148 (PIN_OUTPUT_PULLUP | MUX_MODE2)	  /* mdio_data.uart5_rxd_mux3 */
    				0x14C (PIN_OUTPUT_PULLUP | MUX_MODE2)  /* mdio_clk.uart5_txd_mux3 */
    			>;
    		};
    
    		usb0_pins: pinmux_usb0_pins {
    			pinctrl-single,pins = <
    				0x21C (PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* usb0_drvvbus.usb0_drvvbus */
    			>;
    		};
    
    		norflash_pins: norflash_pins {
    			pinctrl-single,pins = <
    
    				/*Data lines*/
    				0x0 (INPUT_EN | MUX_MODE0)	/* gpmc_ad0.gpmc_ad0 */
    				0x4 (INPUT_EN | MUX_MODE0)	/* gpmc_ad1.gpmc_ad1 */
    				0x8 (INPUT_EN | MUX_MODE0)	/* gpmc_ad2.gpmc_ad2 */
    				0xc (INPUT_EN | MUX_MODE0)	/* gpmc_ad3.gpmc_ad3 */
    				0x10 (INPUT_EN | MUX_MODE0)	/* gpmc_ad4.gpmc_ad4 */
    				0x14 (INPUT_EN | MUX_MODE0)	/* gpmc_ad5.gpmc_ad5 */
    				0x18 (INPUT_EN | MUX_MODE0)	/* gpmc_ad6.gpmc_ad6 */
    				0x1c (INPUT_EN | MUX_MODE0)	/* gpmc_ad7.gpmc_ad7 */
    				0x20 (INPUT_EN | MUX_MODE0)	/* gpmc_ad8.gpmc_ad8 */
    				0x24 (INPUT_EN | MUX_MODE0)	/* gpmc_ad9.gpmc_ad9 */
    				0x28 (INPUT_EN | MUX_MODE0)	/* gpmc_ad10.gpmc_ad10 */
    				0x2c (INPUT_EN | MUX_MODE0)	/* gpmc_ad11.gpmc_ad11 */
    				0x30 (INPUT_EN | MUX_MODE0)	/* gpmc_ad12.gpmc_ad12 */
    				0x34 (INPUT_EN | MUX_MODE0)	/* gpmc_ad13.gpmc_ad13 */
    				0x38 (INPUT_EN | MUX_MODE0)	/* gpmc_ad14.gpmc_ad14 */
    				0x3c (INPUT_EN | MUX_MODE0)	/* gpmc_ad15.gpmc_ad15 */
    
    				/*Addr lines*/
    				0xA0 (PIN_INPUT | MUX_MODE7)    /* lcd_data0.gpio2[6]*/
    				0xA4 (PIN_INPUT | MUX_MODE1)    /* lcd_data1.gpmc_a1_mux1*/
    				0xA8 (PIN_INPUT | MUX_MODE1)    /* lcd_data2.gpmc_a2_mux1*/
    				0xAC (PIN_INPUT | MUX_MODE1)    /* lcd_data3.gpmc_a3_mux1*/
    				0xB0 (PIN_INPUT | MUX_MODE1)    /* lcd_data4.gpmc_a4_mux1*/
    				0xB4 (PIN_INPUT | MUX_MODE1)    /* lcd_data5.gpmc_a5_mux1*/
    				0xB8 (PIN_INPUT | MUX_MODE1)    /* lcd_data6.gpmc_a6_mux1*/
    				0xBC (PIN_INPUT | MUX_MODE1)    /* lcd_data7.gpmc_a7_mux1*/
    				0xe0 (PIN_INPUT | MUX_MODE1)    /* lcd_vsync.gpmc_a8_mux1*/
    				0xe4 (PIN_INPUT | MUX_MODE1)    /* lcd_hsync.gpmc_a9_mux1*/
    				0xe8 (PIN_INPUT | MUX_MODE1)    /* lcd_pclk.gpmc_a10_mux1*/
    				0xec (PIN_INPUT | MUX_MODE1)    /* lcd_ac_bias_en.gpmc_a11_mux1*/
                                    0xC0 (PULL_DISABLE | MUX_MODE1) /* lcd_data8.gpmc_a12*/
                                    0xC4 (PULL_DISABLE | MUX_MODE1) /* lcd_data9.gpmc_a13*/
                                    0xC8 (PULL_DISABLE | MUX_MODE1) /* lcd_data10.gpmc_a14*/
                                    0xCC (PULL_DISABLE | MUX_MODE1) /* lcd_data11.gpmc_a15*/
                                    0xD0 (PULL_DISABLE | MUX_MODE1) /* lcd_data12.gpmc_a16_mux1*/
                                    0xD4 (PULL_DISABLE | MUX_MODE1) /* lcd_data13.gpmc_a17_mux1*/
                                    0xD8 (PULL_DISABLE | MUX_MODE1) /* lcd_data14.gpmc_a18_mux1*/
                                    0xDC (PULL_DISABLE | MUX_MODE1) /* lcd_data15.gpmc_a19_mux1*/
    				0xF0 (PIN_OUTPUT_PULLUP | MUX_MODE1) /*mmc0_dat3.gpmc_a20_mux1*/
    				0xF4 (PIN_OUTPUT_PULLUP | MUX_MODE1) /*mmc0_dat2.gpmc_a21_mux1*/
    				0xF8 (PIN_OUTPUT_PULLUP | MUX_MODE1) /*mmc0_dat1.gpmc_a22_mux1*/
    				0xFC (PIN_OUTPUT_PULLUP | MUX_MODE1) /*mmc0_dat0.gpmc_a23_mux1*/
    				0x100 (PIN_OUTPUT_PULLUP | MUX_MODE1) /*mmc0_clk.gpmc_a24_mux1*/
    
    				/*Control lines*/
    				0x70 (PIN_INPUT_PULLUP | MUX_MODE0)	/* gpmc_wait0.gpmc_wait0 */
    				0x7c (PIN_INPUT_PULLUP | MUX_MODE0)	/* gpmc_csn0.gpmc_csn0  */
    				0x94 (PIN_OUTPUT_PULLUP | MUX_MODE0)	/* gpmc_oen_ren.gpmc_oen_ren */
    				0x98 (PIN_INPUT_PULLUP | MUX_MODE0)	/* gpmc_wen.gpmc_wen */
    			>;
    		};
    
    
    		mmc2_pins: pinmux_mmc2_pins {
    			pinctrl-single,pins = <
    				0x44 (INPUT_EN | MUX_MODE3)			/* gpmc_a1.mmc2_dat0_mux0 */
    				0x48 (INPUT_EN | MUX_MODE3)			/* gpmc_a2.mmc2_dat1_mux0 */
    				0x4C (INPUT_EN | MUX_MODE3)			/* gpmc_a3.mmc2_dat2_mux0 */
    				0x78 (PIN_INPUT_PULLUP | MUX_MODE3) 		/* gpmc_ben1.mmc2_dat3_mux0*/
    				0x58 (INPUT_EN | MUX_MODE3)			/* gpmc_a6.mmc2_dat4_mux0 */
    				0x5C (INPUT_EN | MUX_MODE3)     		/* gpmc_a7.mmc2_dat5_mux0 */
    				0x60 (INPUT_EN | MUX_MODE3)     		/* gpmc_a8.mmc2_dat6_mux0 */
    				0x64 (INPUT_EN | MUX_MODE3)     		/* gpmc_a9.mmc2_dat7_mux0 */
    				0x88 (PIN_INPUT_PULLUP | MUX_MODE3) 		/* gpmc_csn3.mmc2_cmd_mux0 */
    				0x8C (INPUT_EN | MUX_MODE3)			/* gpmc_clk.mmc2_clk_mux0 */
    				0x74 (PIN_INPUT_PULLUP | MUX_MODE7)             /* gpmc_wpn.gpio0[31]*/
    			>;
    		};
    	};
    
    	ocp {
    		uart1: serial@48022000 {
    			pinctrl-names = "default";
    			pinctrl-0 = <&uart1_pins>;
    
    			status = "okay";
    		};
    		
    		uart2: serial@48024000 {
    			pinctrl-names = "default";
    			pinctrl-0 = <&uart2_pins>;
    
    			status = "okay";
    		};
    		
    		uart5: serial@481aa000 {
    			pinctrl-names = "default";
    			pinctrl-0 = <&uart5_pins>;
    
    			status = "okay";
    		};
    
    
    		i2c0: i2c@44e0b000 {
    			pinctrl-names = "default";
    			pinctrl-0 = <&i2c0_pins>;
    
    			status = "okay";
    			clock-frequency = <400000>;
    
    			ipod: ipod@10 {
    				reg = <0x10>;
    			};
    
    		};
    
    		musb: usb@47400000 {
    			status = "okay";
    
    			control@44e10000 {
    				status = "okay";
    			};
    
    			usb-phy@47401300 {
    				status = "okay";
    			};
    
    			usb@47401000 {
    				status = "okay";
    				pinctrl-names = "default";
    				pinctrl-0 = <&usb0_pins>;
    			};
    
    			dma-controller@07402000  {
    				status = "okay";
    			};
    		};
    
    		i2c2: i2c@4819c000 {
    			pinctrl-names = "default";
    			pinctrl-0 = <&i2c2_pins>;
    
    			status = "okay";
    			clock-frequency = <400000>;
    
    			audio: audio@C5 {
    				reg = <0xC5>;
    			};
    
    			hero: hero@C6 {
    				reg = <0xC6>;
    			};
    		};
    
    		spi0: spi@48030000 {
    		/*4-line Display*/
    			pinctrl-names = "default";
    			pinctrl-0 = <&spi0_pins>;
    			clock-frequency = <400000>;
    			status = "okay";
    		};
    
    		dcan0: d_can@481cc000 {
    			pinctrl-names = "default";
    			pinctrl-0 = <&dcan0_pins>;
    			status = "okay";
    		};
    		
    
    		elm: elm@48080000 {
    			status = "okay";
    		};
    
    
    		gpmc: gpmc@50000000 {
    				status = "okay";
    				pinctrl-names = "default";
    				pinctrl-0 = <&norflash_pins>;
    				ranges = <0 0 0x08000000 0x02000000>;	/* CS0: NOR */
    
    				nor@0,0 {
    				compatible = "cfi-flash";
    				linux,mtd-name= "amd,s29gl256s";
    				#address-cells = <1>;
    				#size-cells = <1>;
    				reg = <0 0 0x02000000>;
    				bank-width = <2>;
    
    				gpmc,mux-add-data;
    				gpmc,cs-on-ns = <0>;
    				gpmc,cs-rd-off-ns = <186>;
    				gpmc,cs-wr-off-ns = <186>;
    				gpmc,adv-on-ns = <12>;
    				gpmc,adv-rd-off-ns = <48>;
    				gpmc,adv-wr-off-ns = <48>;
    				gpmc,oe-on-ns = <54>;
    				gpmc,oe-off-ns = <168>;
    				gpmc,we-on-ns = <54>;
    				gpmc,we-off-ns = <168>;
    				gpmc,rd-cycle-ns = <186>;
    				gpmc,wr-cycle-ns = <186>;
    				gpmc,access-ns = <114>;
    				gpmc,page-burst-access-ns = <6>;
    				gpmc,bus-turnaround-ns = <12>;
    				gpmc,cycle2cycle-delay-ns = <18>;
    				gpmc,wr-data-mux-bus-ns = <90>;
    				gpmc,wr-access-ns = <186>;
    				gpmc,cycle2cycle-samecsen;
    				gpmc,cycle2cycle-diffcsen;
    
    				partition@0 {
    					label = "uboot";
    					reg = <0 0x80000>;
    				};
    				partition@0x80000 {
    					label = "1st-copy-uboot-env";
    					reg = <0x80000 0x40000>;
    				};
    				partition@0xA0000 {
    					label = "2nd-copy-uboot-env";
    					reg = <0xA0000 0x40000>;
    				};
    				partition@0xC0000 {
    					label = "linux-kernel";
    					reg = <0xC0000 0x400000>;
    				};
    				partition@0x4C0000 {
    					label = "userland";
    					reg = <0x4C0000 0x1B40000>;
    				};
    			};
    		};
    
    		mmc2: mmc@481d8000 {
    			status = "okay";
    			pinctrl-names = "default";
    			pinctrl-0 = <&mmc2_pins>;
    			vmmc-supply = <&dvp1_3v3_sw>;
    			bus-width = <8>;
    			ti,non-removable;
    			cap-mmc-dual-data-rate;
    		};
    
    	};
    
    };
    
    
    
    &edma {
    	ti,edma-xbar-event-map = <1 12
    				  2 13>;
    };
    
    #ifndef _MUX_H_
    #define _MUX_H_
    
    /*
     * MODE0 - Mux Mode 0
     * MODE1 - Mux Mode 1
     * MODE2 - Mux Mode 2
     * MODE3 - Mux Mode 3
     * MODE4 - Mux Mode 4
     * MODE5 - Mux Mode 5
     * MODE6 - Mux Mode 6
     * MODE7 - Mux Mode 7
     * IDIS - Receiver disabled
     * IEN - Receiver enabled
     * PD - Internal pull-down
     * PU - Internal pull-up
     * OFF - Internal pull disabled
     */
    
    #define MODE0 0
    #define MODE1 1
    #define MODE2 2
    #define MODE3 3
    #define MODE4 4
    #define MODE5 5
    #define MODE6 6
    #define MODE7 7
    #define IDIS (0 << 5)
    #define IEN (1 << 5)
    #define PD (0 << 3)
    #define PU (2 << 3)
    #define OFF (1 << 3)
    
    /*
     * To get the physical address the offset has
     * to be added to AM335X_CTRL_BASE
     */
    
    #define CONTROL_PADCONF_GPMC_AD0                  0x0800
    #define CONTROL_PADCONF_GPMC_AD1                  0x0804
    #define CONTROL_PADCONF_GPMC_AD2                  0x0808
    #define CONTROL_PADCONF_GPMC_AD3                  0x080C
    #define CONTROL_PADCONF_GPMC_AD4                  0x0810
    #define CONTROL_PADCONF_GPMC_AD5                  0x0814
    #define CONTROL_PADCONF_GPMC_AD6                  0x0818
    #define CONTROL_PADCONF_GPMC_AD7                  0x081C
    #define CONTROL_PADCONF_GPMC_AD8                  0x0820
    #define CONTROL_PADCONF_GPMC_AD9                  0x0824
    #define CONTROL_PADCONF_GPMC_AD10                 0x0828
    #define CONTROL_PADCONF_GPMC_AD11                 0x082C
    #define CONTROL_PADCONF_GPMC_AD12                 0x0830
    #define CONTROL_PADCONF_GPMC_AD13                 0x0834
    #define CONTROL_PADCONF_GPMC_AD14                 0x0838
    #define CONTROL_PADCONF_GPMC_AD15                 0x083C
    #define CONTROL_PADCONF_GPMC_A0                   0x0840
    #define CONTROL_PADCONF_GPMC_A1                   0x0844
    #define CONTROL_PADCONF_GPMC_A2                   0x0848
    #define CONTROL_PADCONF_GPMC_A3                   0x084C
    #define CONTROL_PADCONF_GPMC_A4                   0x0850
    #define CONTROL_PADCONF_GPMC_A5                   0x0854
    #define CONTROL_PADCONF_GPMC_A6                   0x0858
    #define CONTROL_PADCONF_GPMC_A7                   0x085C
    #define CONTROL_PADCONF_GPMC_A8                   0x0860
    #define CONTROL_PADCONF_GPMC_A9                   0x0864
    #define CONTROL_PADCONF_GPMC_A10                  0x0868
    #define CONTROL_PADCONF_GPMC_A11                  0x086C
    #define CONTROL_PADCONF_GPMC_WAIT0                0x0870
    #define CONTROL_PADCONF_GPMC_WPN                  0x0874
    #define CONTROL_PADCONF_GPMC_BEN1                 0x0878
    #define CONTROL_PADCONF_GPMC_CSN0                 0x087C
    #define CONTROL_PADCONF_GPMC_CSN1                 0x0880
    #define CONTROL_PADCONF_GPMC_CSN2                 0x0884
    #define CONTROL_PADCONF_GPMC_CSN3                 0x0888
    #define CONTROL_PADCONF_GPMC_CLK                  0x088C
    #define CONTROL_PADCONF_GPMC_ADVN_ALE             0x0890
    #define CONTROL_PADCONF_GPMC_OEN_REN              0x0894
    #define CONTROL_PADCONF_GPMC_WEN                  0x0898
    #define CONTROL_PADCONF_GPMC_BEN0_CLE             0x089C
    #define CONTROL_PADCONF_LCD_DATA0                 0x08A0
    #define CONTROL_PADCONF_LCD_DATA1                 0x08A4
    #define CONTROL_PADCONF_LCD_DATA2                 0x08A8
    #define CONTROL_PADCONF_LCD_DATA3                 0x08AC
    #define CONTROL_PADCONF_LCD_DATA4                 0x08B0
    #define CONTROL_PADCONF_LCD_DATA5                 0x08B4
    #define CONTROL_PADCONF_LCD_DATA6                 0x08B8
    #define CONTROL_PADCONF_LCD_DATA7                 0x08BC
    #define CONTROL_PADCONF_LCD_DATA8                 0x08C0
    #define CONTROL_PADCONF_LCD_DATA9                 0x08C4
    #define CONTROL_PADCONF_LCD_DATA10                0x08C8
    #define CONTROL_PADCONF_LCD_DATA11                0x08CC
    #define CONTROL_PADCONF_LCD_DATA12                0x08D0
    #define CONTROL_PADCONF_LCD_DATA13                0x08D4
    #define CONTROL_PADCONF_LCD_DATA14                0x08D8
    #define CONTROL_PADCONF_LCD_DATA15                0x08DC
    #define CONTROL_PADCONF_LCD_VSYNC                 0x08E0
    #define CONTROL_PADCONF_LCD_HSYNC                 0x08E4
    #define CONTROL_PADCONF_LCD_PCLK                  0x08E8
    #define CONTROL_PADCONF_LCD_AC_BIAS_EN            0x08EC
    #define CONTROL_PADCONF_MMC0_DAT3                 0x08F0
    #define CONTROL_PADCONF_MMC0_DAT2                 0x08F4
    #define CONTROL_PADCONF_MMC0_DAT1                 0x08F8
    #define CONTROL_PADCONF_MMC0_DAT0                 0x08FC
    #define CONTROL_PADCONF_MMC0_CLK                  0x0900
    #define CONTROL_PADCONF_MMC0_CMD                  0x0904
    #define CONTROL_PADCONF_MII1_COL                  0x0908
    #define CONTROL_PADCONF_MII1_CRS                  0x090C
    #define CONTROL_PADCONF_MII1_RX_ER                0x0910
    #define CONTROL_PADCONF_MII1_TX_EN                0x0914
    #define CONTROL_PADCONF_MII1_RX_DV                0x0918
    #define CONTROL_PADCONF_MII1_TXD3                 0x091C
    #define CONTROL_PADCONF_MII1_TXD2                 0x0920
    #define CONTROL_PADCONF_MII1_TXD1                 0x0924
    #define CONTROL_PADCONF_MII1_TXD0                 0x0928
    #define CONTROL_PADCONF_MII1_TX_CLK               0x092C
    #define CONTROL_PADCONF_MII1_RX_CLK               0x0930
    #define CONTROL_PADCONF_MII1_RXD3                 0x0934
    #define CONTROL_PADCONF_MII1_RXD2                 0x0938
    #define CONTROL_PADCONF_MII1_RXD1                 0x093C
    #define CONTROL_PADCONF_MII1_RXD0                 0x0940
    #define CONTROL_PADCONF_RMII1_REF_CLK             0x0944
    #define CONTROL_PADCONF_MDIO                      0x0948
    #define CONTROL_PADCONF_MDC                       0x094C
    #define CONTROL_PADCONF_SPI0_SCLK                 0x0950
    #define CONTROL_PADCONF_SPI0_D0                   0x0954
    #define CONTROL_PADCONF_SPI0_D1                   0x0958
    #define CONTROL_PADCONF_SPI0_CS0                  0x095C
    #define CONTROL_PADCONF_SPI0_CS1                  0x0960
    #define CONTROL_PADCONF_ECAP0_IN_PWM0_OUT         0x0964
    #define CONTROL_PADCONF_UART0_CTSN                0x0968
    #define CONTROL_PADCONF_UART0_RTSN                0x096C
    #define CONTROL_PADCONF_UART0_RXD                 0x0970
    #define CONTROL_PADCONF_UART0_TXD                 0x0974
    #define CONTROL_PADCONF_UART1_CTSN                0x0978
    #define CONTROL_PADCONF_UART1_RTSN                0x097C
    #define CONTROL_PADCONF_UART1_RXD                 0x0980
    #define CONTROL_PADCONF_UART1_TXD                 0x0984
    #define CONTROL_PADCONF_I2C0_SDA                  0x0988
    #define CONTROL_PADCONF_I2C0_SCL                  0x098C
    #define CONTROL_PADCONF_MCASP0_ACLKX              0x0990
    #define CONTROL_PADCONF_MCASP0_FSX                0x0994
    #define CONTROL_PADCONF_MCASP0_AXR0               0x0998
    #define CONTROL_PADCONF_MCASP0_AHCLKR             0x099C
    #define CONTROL_PADCONF_MCASP0_ACLKR              0x09A0
    #define CONTROL_PADCONF_MCASP0_FSR                0x09A4
    #define CONTROL_PADCONF_MCASP0_AXR1               0x09A8
    #define CONTROL_PADCONF_MCASP0_AHCLKX             0x09AC
    #define CONTROL_PADCONF_XDMA_EVENT_INTR0          0x09B0
    #define CONTROL_PADCONF_XDMA_EVENT_INTR1          0x09B4
    #define CONTROL_PADCONF_WARMRSTN                  0x09B8
    #define CONTROL_PADCONF_EXTINTN                   0x09C0
    #define CONTROL_PADCONF_TMS                       0x09D0
    #define CONTROL_PADCONF_TDI                       0x09D4
    #define CONTROL_PADCONF_TDO                       0x09D8
    #define CONTROL_PADCONF_TCK                       0x09DC
    #define CONTROL_PADCONF_TRSTN                     0x09E0
    #define CONTROL_PADCONF_EMU0                      0x09E4
    #define CONTROL_PADCONF_EMU1                      0x09E8
    #define CONTROL_PADCONF_RTC_PWRONRSTN             0x09F8
    #define CONTROL_PADCONF_PMIC_POWER_EN             0x09FC
    #define CONTROL_PADCONF_EXT_WAKEUP                0x0A00
    #define CONTROL_PADCONF_RTC_KALDO_ENN             0x0A04
    #define CONTROL_PADCONF_USB0_DRVVBUS              0x0A1C
    #define CONTROL_PADCONF_USB1_DRVVBUS              0x0A34
    
    #define MUX_VAL(OFFSET,VALUE)\
        writel((VALUE), AM335X_CTRL_BASE + (OFFSET));
    
    #endif
    
    #ifndef _PINMUX_H_
    #define _PINMUX_H_
    
    /*
     * MODE0 - Mux Mode 0
     * MODE1 - Mux Mode 1
     * MODE2 - Mux Mode 2
     * MODE3 - Mux Mode 3
     * MODE4 - Mux Mode 4
     * MODE5 - Mux Mode 5
     * MODE6 - Mux Mode 6
     * MODE7 - Mux Mode 7
     * IDIS - Receiver disabled
     * IEN - Receiver enabled
     * PD - Internal pull-down
     * PU - Internal pull-up
     * OFF - Internal pull disabled
     */
    
    #define MUX_EVM() \
    
    /* Design Status: NO ERRORS */
    
    MUX_VAL(CONTROL_PADCONF_GPMC_AD0, (IEN | PD | MODE0 )) /* gpmc_ad0 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_AD1, (IEN | PD | MODE0 )) /* gpmc_ad1 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_AD2, (IEN | PD | MODE0 )) /* gpmc_ad2 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_AD3, (IEN | PD | MODE0 )) /* gpmc_ad3 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_AD4, (IEN | PD | MODE0 )) /* gpmc_ad4 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_AD5, (IEN | PD | MODE0 )) /* gpmc_ad5 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_AD6, (IEN | PD | MODE0 )) /* gpmc_ad6 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_AD7, (IEN | PD | MODE0 )) /* gpmc_ad7 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_AD8, (IEN | PD | MODE0 )) /* gpmc_ad8 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_AD9, (IEN | PD | MODE0 )) /* gpmc_ad9 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_AD10, (IEN | PD | MODE0 )) /* gpmc_ad10 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_AD11, (IEN | PD | MODE0 )) /* gpmc_ad11 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_AD12, (IEN | PD | MODE0 )) /* gpmc_ad12 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_AD13, (IEN | PD | MODE0 )) /* gpmc_ad13 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_AD14, (IEN | PD | MODE0 )) /* gpmc_ad14 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_AD15, (IEN | PD | MODE0 )) /* gpmc_ad15 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_A0, (IEN | PD | MODE7 )) /* gpio1[16] */\
    MUX_VAL(CONTROL_PADCONF_GPMC_A1, (IEN | PD | MODE3 )) /* mmc2_dat0_mux0 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_A2, (IEN | PD | MODE3 )) /* mmc2_dat1_mux0 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_A3, (IEN | PD | MODE3 )) /* mmc2_dat2_mux0 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_A4, (IEN | PD | MODE7 )) /* gpio1[20] */\
    MUX_VAL(CONTROL_PADCONF_GPMC_A5, (IEN | PD | MODE7 )) /* gpio1[21] */\
    MUX_VAL(CONTROL_PADCONF_GPMC_A6, (IEN | PD | MODE3 )) /* mmc2_dat4_mux0 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_A7, (IEN | PD | MODE3 )) /* mmc2_dat5_mux0 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_A8, (IEN | PD | MODE3 )) /* mmc2_dat6_mux0 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_A9, (IEN | PD | MODE3 )) /* mmc2_dat7_mux0/rmii2_crs_dv_mux2 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_A10, (IEN | PD | MODE7 )) /* gpio1[26] */\
    MUX_VAL(CONTROL_PADCONF_GPMC_A11, (IEN | PD | MODE7 )) /* gpio1[27] */\
    MUX_VAL(CONTROL_PADCONF_GPMC_WAIT0, (IEN | PU | MODE0 )) /* gpmc_wait0 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_WPN, (IEN | PU | MODE7 )) /* gpio0[31] */\
    MUX_VAL(CONTROL_PADCONF_GPMC_BEN1, (IEN | PU | MODE3 )) /* mmc2_dat3_mux0 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_CSN0, (IEN | PU | MODE0 )) /* gpmc_csn0 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_CSN1, (IEN | PU | MODE7 )) /* gpio1[30] */\
    MUX_VAL(CONTROL_PADCONF_GPMC_CSN2, (IEN | PU | MODE7 )) /* gpio1[31] */\
    MUX_VAL(CONTROL_PADCONF_GPMC_CSN3, (IEN | PU | MODE3 )) /* mmc2_cmd_mux0 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_CLK, (IEN | PD | MODE3 )) /* mmc2_clk_mux0 */\
    MUX_VAL(CONTROL_PADCONF_GPMC_ADVN_ALE, (IEN | PU | MODE7 )) /* gpio2[2] */\
    MUX_VAL(CONTROL_PADCONF_GPMC_OEN_REN, (IDIS | PU | MODE0 )) /* gpmc_oen_ren */\
    MUX_VAL(CONTROL_PADCONF_GPMC_WEN, (IEN | PU | MODE0 )) /* gpmc_wen */\
    MUX_VAL(CONTROL_PADCONF_GPMC_BEN0_CLE, (IEN | PU | MODE2 )) /* timer5_mux3 */\
    MUX_VAL(CONTROL_PADCONF_LCD_DATA0, (IEN | OFF | MODE7 )) /* gpio2[6] */\
    MUX_VAL(CONTROL_PADCONF_LCD_DATA1, (IEN | OFF | MODE1 )) /* gpmc_a1_mux1 */\
    MUX_VAL(CONTROL_PADCONF_LCD_DATA2, (IEN | OFF | MODE1 )) /* gpmc_a2_mux1 */\
    MUX_VAL(CONTROL_PADCONF_LCD_DATA3, (IEN | OFF | MODE1 )) /* gpmc_a3_mux1 */\
    MUX_VAL(CONTROL_PADCONF_LCD_DATA4, (IEN | OFF | MODE1 )) /* gpmc_a4_mux1 */\
    MUX_VAL(CONTROL_PADCONF_LCD_DATA5, (IEN | OFF | MODE1 )) /* gpmc_a5_mux1 */\
    MUX_VAL(CONTROL_PADCONF_LCD_DATA6, (IEN | OFF | MODE1 )) /* gpmc_a6_mux1 */\
    MUX_VAL(CONTROL_PADCONF_LCD_DATA7, (IEN | OFF | MODE1 )) /* gpmc_a7_mux1 */\
    MUX_VAL(CONTROL_PADCONF_LCD_DATA8, (IDIS | OFF | MODE1 )) /* gpmc_a12 */\
    MUX_VAL(CONTROL_PADCONF_LCD_DATA9, (IDIS | OFF | MODE1 )) /* gpmc_a13 */\
    MUX_VAL(CONTROL_PADCONF_LCD_DATA10, (IDIS | OFF | MODE1 )) /* gpmc_a14 */\
    MUX_VAL(CONTROL_PADCONF_LCD_DATA11, (IDIS | OFF | MODE1 )) /* gpmc_a15 */\
    MUX_VAL(CONTROL_PADCONF_LCD_DATA12, (IDIS | OFF | MODE1 )) /* gpmc_a16_mux1 */\
    MUX_VAL(CONTROL_PADCONF_LCD_DATA13, (IDIS | OFF | MODE1 )) /* gpmc_a17_mux1 */\
    MUX_VAL(CONTROL_PADCONF_LCD_DATA14, (IDIS | OFF | MODE1 )) /* gpmc_a18_mux1 */\
    MUX_VAL(CONTROL_PADCONF_LCD_DATA15, (IDIS | OFF | MODE1 )) /* gpmc_a19_mux1 */\
    MUX_VAL(CONTROL_PADCONF_LCD_VSYNC, (IEN | OFF | MODE1 )) /* gpmc_a8_mux1 */\
    MUX_VAL(CONTROL_PADCONF_LCD_HSYNC, (IEN | OFF | MODE1 )) /* gpmc_a9_mux1 */\
    MUX_VAL(CONTROL_PADCONF_LCD_PCLK, (IEN | OFF | MODE1 )) /* gpmc_a10_mux1 */\
    MUX_VAL(CONTROL_PADCONF_LCD_AC_BIAS_EN, (IEN | OFF | MODE1 )) /* gpmc_a11_mux1 */\
    MUX_VAL(CONTROL_PADCONF_MMC0_DAT3, (IDIS | PU | MODE1 )) /* gpmc_a20_mux1 */\
    MUX_VAL(CONTROL_PADCONF_MMC0_DAT2, (IDIS | PU | MODE1 )) /* gpmc_a21_mux1 */\
    MUX_VAL(CONTROL_PADCONF_MMC0_DAT1, (IDIS | PU | MODE1 )) /* gpmc_a22_mux1 */\
    MUX_VAL(CONTROL_PADCONF_MMC0_DAT0, (IDIS | PU | MODE1 )) /* gpmc_a23_mux1 */\
    MUX_VAL(CONTROL_PADCONF_MMC0_CLK, (IDIS | PU | MODE1 )) /* gpmc_a24_mux1 */\
    MUX_VAL(CONTROL_PADCONF_MMC0_CMD, (IEN | PU | MODE7 )) /* gpio2[31] */\
    MUX_VAL(CONTROL_PADCONF_MII1_COL, (IEN | PD | MODE4 )) /* mcasp1_axr2_mux1 */\
    MUX_VAL(CONTROL_PADCONF_MII1_CRS, (IEN | PD | MODE5 )) /* uart5_ctsn_mux2 */\
    MUX_VAL(CONTROL_PADCONF_MII1_RX_ER, (IDIS | PD | MODE5 )) /* uart5_rtsn_mux2 */\
    MUX_VAL(CONTROL_PADCONF_MII1_TX_EN, (IEN | PD | MODE7 )) /* gpio3[3] */\
    MUX_VAL(CONTROL_PADCONF_MII1_RX_DV, (IEN | PD | MODE4 )) /* mcasp1_aclkx_mux0 */\
    MUX_VAL(CONTROL_PADCONF_MII1_TXD3, (IEN | PD | MODE4 )) /* mcasp1_fsx_mux0 */\
    MUX_VAL(CONTROL_PADCONF_MII1_TXD2, (IEN | PD | MODE4 )) /* mcasp1_axr0_mux0 */\
    MUX_VAL(CONTROL_PADCONF_MII1_TXD1, (IEN | PD | MODE7 )) /* gpio0[21] */\
    MUX_VAL(CONTROL_PADCONF_MII1_TXD0, (IEN | PD | MODE7 )) /* gpio0[28] */\
    MUX_VAL(CONTROL_PADCONF_MII1_TX_CLK, (IEN | PD | MODE1 )) /* uart2_rxd_mux0 */\
    MUX_VAL(CONTROL_PADCONF_MII1_RX_CLK, (IEN | PD | MODE1 )) /* uart2_txd_mux0 */\
    MUX_VAL(CONTROL_PADCONF_MII1_RXD3, (IEN | PD | MODE7 )) /* gpio2[18] */\
    MUX_VAL(CONTROL_PADCONF_MII1_RXD2, (IEN | PD | MODE7 )) /* gpio2[19] */\
    MUX_VAL(CONTROL_PADCONF_MII1_RXD1, (IEN | PD | MODE7 )) /* gpio2[20] */\
    MUX_VAL(CONTROL_PADCONF_MII1_RXD0, (IEN | PD | MODE7 )) /* gpio2[21] */\
    MUX_VAL(CONTROL_PADCONF_RMII1_REF_CLK, (IEN | PD | MODE7 )) /* gpio0[29] */\
    MUX_VAL(CONTROL_PADCONF_MDIO, (IDIS | PU | MODE2 )) /* uart5_rxd_mux3 */\
    MUX_VAL(CONTROL_PADCONF_MDC, (IDIS | PU | MODE2 )) /* uart5_txd_mux3 */\
    MUX_VAL(CONTROL_PADCONF_SPI0_SCLK, (IEN | OFF | MODE0 )) /* spi0_sclk */\
    MUX_VAL(CONTROL_PADCONF_SPI0_D0, (IEN | OFF | MODE0 )) /* spi0_d0 */\
    MUX_VAL(CONTROL_PADCONF_SPI0_D1, (IEN | OFF | MODE7 )) /* gpio0[4] */\
    MUX_VAL(CONTROL_PADCONF_SPI0_CS0, (IEN | OFF | MODE0 )) /* spi0_cs0 */\
    MUX_VAL(CONTROL_PADCONF_SPI0_CS1, (IEN | OFF | MODE7 )) /* gpio0[6] */\
    MUX_VAL(CONTROL_PADCONF_ECAP0_IN_PWM0_OUT, (IEN | OFF | MODE7 )) /* gpio0[7] */\
    MUX_VAL(CONTROL_PADCONF_UART0_CTSN, (IEN | OFF | MODE7 )) /* gpio1[8] */\
    MUX_VAL(CONTROL_PADCONF_UART0_RTSN, (IEN | OFF | MODE7 )) /* gpio1[9] */\
    MUX_VAL(CONTROL_PADCONF_UART0_RXD, (IEN | OFF | MODE3 )) /* I2C2_SDA_mux1 */\
    MUX_VAL(CONTROL_PADCONF_UART0_TXD, (IEN | OFF | MODE3 )) /* I2C2_SCL_mux1 */\
    MUX_VAL(CONTROL_PADCONF_UART1_CTSN, (IDIS | OFF | MODE2 )) /* dcan0_tx_mux2 */\
    MUX_VAL(CONTROL_PADCONF_UART1_RTSN, (IEN | OFF | MODE2 )) /* dcan0_rx_mux2 */\
    MUX_VAL(CONTROL_PADCONF_UART1_RXD, (IEN | OFF | MODE0 )) /* uart1_rxd */\
    MUX_VAL(CONTROL_PADCONF_UART1_TXD, (IDIS | OFF | MODE0 )) /* uart1_txd */\
    MUX_VAL(CONTROL_PADCONF_I2C0_SDA, (IEN | OFF | MODE0 )) /* I2C0_SDA */\
    MUX_VAL(CONTROL_PADCONF_I2C0_SCL, (IEN | OFF | MODE0 )) /* I2C0_SCL */\
    MUX_VAL(CONTROL_PADCONF_MCASP0_ACLKX, (IEN | PD | MODE0 )) /* mcasp0_aclkx_mux0 */\
    MUX_VAL(CONTROL_PADCONF_MCASP0_FSX, (IEN | PD | MODE0 )) /* mcasp0_fsx_mux0 */\
    MUX_VAL(CONTROL_PADCONF_MCASP0_AXR0, (IEN | PD | MODE0 )) /* mcasp0_axr0_mux0 */\
    MUX_VAL(CONTROL_PADCONF_MCASP0_AHCLKR, (IEN | PD | MODE7 )) /* gpio3[17] */\
    MUX_VAL(CONTROL_PADCONF_MCASP0_ACLKR, (IEN | PD | MODE2 )) /* mcasp0_axr2_mux1 */\
    MUX_VAL(CONTROL_PADCONF_MCASP0_FSR, (IEN | PD | MODE2 )) /* mcasp0_axr3_mux1 */\
    MUX_VAL(CONTROL_PADCONF_MCASP0_AXR1, (IEN | PD | MODE0 )) /* mcasp0_axr1_mux0 */\
    MUX_VAL(CONTROL_PADCONF_MCASP0_AHCLKX, (IEN | PD | MODE7 )) /* gpio3[21] */\
    MUX_VAL(CONTROL_PADCONF_XDMA_EVENT_INTR0, (IEN | OFF | MODE2 )) /* timer4_mux1 */\
    MUX_VAL(CONTROL_PADCONF_XDMA_EVENT_INTR1, (IEN | OFF | MODE4 )) /* timer7_mux1 */\
    MUX_VAL(CONTROL_PADCONF_WARMRSTN, (IEN | OFF | MODE0 )) /* nRESETIN_OUT */\
    MUX_VAL(CONTROL_PADCONF_EXTINTN, (IEN | OFF | MODE0 )) /* nNMI */\
    MUX_VAL(CONTROL_PADCONF_TMS, (IEN | PU | MODE0 )) /* TMS */\
    MUX_VAL(CONTROL_PADCONF_TDI, (IEN | PU | MODE0 )) /* TDI */\
    MUX_VAL(CONTROL_PADCONF_TDO, (IDIS | PU | MODE0 )) /* TDO */\
    MUX_VAL(CONTROL_PADCONF_TCK, (IEN | PU | MODE0 )) /* TCK */\
    MUX_VAL(CONTROL_PADCONF_TRSTN, (IEN | PD | MODE0 )) /* nTRST */\
    MUX_VAL(CONTROL_PADCONF_EMU0, (IEN | PU | MODE7 )) /* gpio3[7] */\
    MUX_VAL(CONTROL_PADCONF_EMU1, (IEN | PU | MODE7 )) /* gpio3[8] */\
    MUX_VAL(CONTROL_PADCONF_RTC_PWRONRSTN, (IEN | OFF | MODE0 )) /* RTC_porz */\
    MUX_VAL(CONTROL_PADCONF_PMIC_POWER_EN, (IDIS | PU | MODE0 )) /* PMIC_POWER_EN */\
    MUX_VAL(CONTROL_PADCONF_EXT_WAKEUP, (IEN | PD | MODE0 )) /* EXT_WAKEUP */\
    MUX_VAL(CONTROL_PADCONF_RTC_KALDO_ENN, (IEN | OFF | MODE0 )) /* ENZ_KALDO_1P8V */\
    MUX_VAL(CONTROL_PADCONF_USB0_DRVVBUS, (IDIS | PD | MODE0 )) /* USB0_DRVVBUS */\
    MUX_VAL(CONTROL_PADCONF_USB1_DRVVBUS, (IEN | PD | MODE7 )) /* gpio3[13] */\
    
    #endif
    

  • Hi,

    The answer from the factory team is that DRA608 J5 is not supported by the Sitara team. Please contact your TI FAE for support.

  • Hi All,

    1. If I use SDK6.0 generate uImage, run as bootm uImage on my custom board, kernel boots and I get prints.

    2. If I use SDK7.0 generate uImage/zImage and run as bootm uImage - dtb or bootz zImage - dtb on my custom board , kernel does not boot and no prints. But the same images  perfectly work on AM335x EVM.

    What am I missing? To generate kernel I just  used make tisdk_am335x-evm_defconfig and make / make uImage.

    In my previous posts I've also attached the dts file that I'm using.

    Regards,

    Gangadhar

  • Hi All,

    With SDK 7.0, linux - 3.12, custom board, I used early_print() to get prints. No prints from printk(), Also kernel hangs

    after calling do_initcall_level() twice. Sequence: start_kernel -> rest_init() -> kernel_init() -> kernel_init_freeable() -> do_basic_setup() -> do_initcalls  -> do_initcall_level()

    The same image gives prints(printk()) on EVM.

    1. I checked bootargs using early_print(), it's correct:  console=ttyO0,115200n8 root=/dev/ram0 rw ramdisk_size=65536 initrd=0x81000000,64M rootfstype=ext2

    2. I checked my uart0 pin mux in dts file, it matches that in uboot.

    3. I also tried removing uart0 pin mux in dts as it'll be initiallized in uboot, but the issue remains the same.

    What am I missing?

    Regards,

    Gangadhar

  • Problem solved. I'm able to get kernel running on my custom board. I made kernel to take bootargs defined from kernel at make menuconfig --> boot option and passed earlyprintk as one of the parameters. Got prints and found that it crashes while enabling system cache, i bypassed this temporarily. Kernel came up completely.

    Regards,

    Gangadhar