This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Alignment exception using Syslink Memory_alloc

Guru 10685 points

I have a buffer that is allocated as follows using the Syslink API:

heap = (IHeap_Handle)SharedRegion_getHeap(2);

buf = Memory_alloc(heap, length, 128, NULL);

If I then try to use

memcpy(buf+1, soneDataArray, 4);

to copy some data into that memory, I get this:

Unhandled fault: alignment exception (0x801)

I don't get any errors if I access buf 4-byte aligned:

memcpy(buf, someDataArray, 4);

so my question is, how can I access my buf without having to write 4-byte aligned data? i.e. like a normal buffer created with "malloc".

Thanks,

Ralph

  • What is your silicon revision ? Are you using neon optimized memcpy

  • Thanks for your prompt reply Badri.


    We are using PG2.0 silicon.

    We are using the 2009-q1 Code Sourcery compiler. I'm not sure if it's optimised or not. Do you know, as this compiler is the standard one TI recommends for the DM8168.

    Thanks,

    Ralph

  • By neon_memcpy I mean if you have overridden the default libc implementation of memcpy with a neon optimized version

    This is done in DVRRDk as explained in this post  http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/t/271221.aspx

    There is a silicon advisory 1.1.38 on using Neon instructions on strongly ordered memory. If you are using PG2.0 this is not applicable.

    If you haven't done anything like this you can ignore neon.The tool chain will not use neon memcpy by default.

    Cortex A8 supports unaligned memory access . http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0344k/Beihgifg.html

    However unaligned access to strongly ordered memory is not supported (http://community.arm.com/thread/3631)

    I am not sure what is the property of sharedRegion 2 in ezSDK. You can put printk in

    \syslink_2_xx_xx_xx\packages\ti\syslink\utils\hlos\knl\osal\Linux\OsalDriver.c

    OsalDrv_mmap() function to print vm_page_prot passed to remap_pfn_range. The function will be called several times so first check if physAddr is SR2 start address and then put the printk

    Also refer following links which appear relevant to the issue you are facing

    http://blog.galemin.com/tag/alignment/

    http://lists.infradead.org/pipermail/linux-arm-kernel/2009-October/002772.html

  • Thanks for the links. I put printk into the module and get this when the module loads:

    >>>>>SharedRegion_isCacheEnabled(2)=0
    >>>>>regionId == 2, remap_pfn_range(0xd53a4478, 0x406e3000, 0x000b3d00, 197132288, 0x183)

    Then when I run my program to allocate memory from the shared region, I get this:

    >>>>>SharedRegion_isCacheEnabled(2)=0
    >>>>>regionId == 2, remap_pfn_range(0xd57f2210, 0x4a400000, 0x000b3d00, 197132288, 0x383)

    And the remap_pfn_range function is of this format:

    remap_pfn_range (vma, vma->vm_start, vma->vm_pgoff, vma->vm_end - vma->vm_start, vma->vm_page_prot)

    So the cache is not enabled for any of the regions. Are you saying that I need to enable the cache in order to access Shared region 2 non-aligned? So do I access it cached and then do a flush?

    Thanks,

    Ralph

  • The MT for vm_page_prot should be bufferable even if it is non cached. Can you confirm the OsalDrv_mmap code is similar to below in your codebase:

    static
    int
    OsalDrv_mmap (struct file * filp, struct vm_area_struct * vma)
    {
    #ifdef CONFIG_MMU
        UInt16 regionId;
        Bool   isCached = FALSE;
        ULong  physAddr;
        Int    i;
    
        /*
         * Set all regions as non-cached except for sharedRegion based on
         * cacheEnable setting
         */
    
        vma->vm_page_prot = pgprot_noncached (vma->vm_page_prot);
        physAddr = vma->vm_pgoff << PAGE_SHIFT;
    
        regionId = _SharedRegion_getIdPhys((Ptr)physAddr);
        if (regionId != SharedRegion_INVALIDREGIONID) {
            isCached = SharedRegion_isCacheEnabled(regionId);
        }
        else {
            for (i = 0; i < NUM_CACHEMMAP_ENTRIES; i++) {
                if (OsalDriver_state.cachemmap[i].physAddr == physAddr) {
                    isCached = TRUE;
                    OsalDriver_state.cachemmap[i].physAddr = 0;
    
                    break;
                }
            }
        }
    
        GT_2trace(curTrace, GT_2CLASS,
                   "OsalDrv_mmap(): setting cache %s for physical address %p",
                   isCached ? "enabled" : "disabled", physAddr);
    
        if (_OsalDrv_isNormalMemory((UInt32) physAddr,
                                     vma->vm_end - vma->vm_start)) {
            /*
             * Map as Normal Memory (as opposed to Strongly Ordered)
             */
            if (isCached == TRUE) {
                vma->vm_page_prot = __pgprot(pgprot_val(vma->vm_page_prot) |
                    L_PTE_MT_WRITEBACK);
            }
            else {
                /* Un-cached */
                vma->vm_page_prot = __pgprot(pgprot_val(vma->vm_page_prot) |
                    L_PTE_MT_BUFFERABLE );
            }
        }
        else {
            /* Do not map as Normal Memory */
            if (isCached == TRUE) {
                vma->vm_page_prot = __pgprot(pgprot_val(vma->vm_page_prot) |
                    (L_PTE_MT_WRITETHROUGH | L_PTE_MT_BUFFERABLE));
            }
        }
    #endif
    
        if (remap_pfn_range (vma,
                             vma->vm_start,
                             vma->vm_pgoff,
                             vma->vm_end - vma->vm_start,
                             vma->vm_page_prot)) {
            return -EAGAIN;
        }
        return 0;
    }
    

  • Hi Badri, your code is different to mine. I am using Syslink 2.20.00.14 by the way. What version are you using? It looks like my memory is not having the L_PTE_MT_BUFFERABLE flag applied to it unlike in your code.

    Your code has this:

        GT_2trace(curTrace, GT_2CLASS,
                   "OsalDrv_mmap(): setting cache %s for physical address %p",
                   isCached ? "enabled" : "disabled", physAddr);
        if (_OsalDrv_isNormalMemory((UInt32) physAddr,
                                     vma->vm_end - vma->vm_start)) {
            /*
             * Map as Normal Memory (as opposed to Strongly Ordered)
             */
            if (isCached == TRUE) {
                vma->vm_page_prot = __pgprot(pgprot_val(vma->vm_page_prot) |
                    L_PTE_MT_WRITEBACK);
            }
            else {
                /* Un-cached */
                vma->vm_page_prot = __pgprot(pgprot_val(vma->vm_page_prot) |
                    L_PTE_MT_BUFFERABLE );
            }
        }
        else {
            /* Do not map as Normal Memory */
            if (isCached == TRUE) {
                vma->vm_page_prot = __pgprot(pgprot_val(vma->vm_page_prot) |
                    (L_PTE_MT_WRITETHROUGH | L_PTE_MT_BUFFERABLE));
            }
        }


    But my code instead only has this line:

        GT_2trace(curTrace, GT_2CLASS,
                   "OsalDrv_mmap(): setting cache %s for physical address %p",
                   isCached ? "enabled" : "disabled", physAddr);

    Ralph

  • /*
     *  @file   OsalDriver.c
     *
     *  @brief      Linux kernel side IOCTL manager interface implementation.
     *
     *              This abstracts the IOCTL calls interface in the Kernel
     *              code. This will expose the interface to register and unregister
     *              functions with their command ids. There will be interface also
     *              for getting the function from table. This will also interface
     *              with command ids arbitrator.
     *
     *
     *  ============================================================================
     *
     *  Copyright (c) 2008-2012, Texas Instruments Incorporated
     *
     *  Redistribution and use in source and binary forms, with or without
     *  modification, are permitted provided that the following conditions
     *  are met:
     *  
     *  *  Redistributions of source code must retain the above copyright
     *     notice, this list of conditions and the following disclaimer.
     *  
     *  *  Redistributions in binary form must reproduce the above copyright
     *     notice, this list of conditions and the following disclaimer in the
     *     documentation and/or other materials provided with the distribution.
     *  
     *  *  Neither the name of Texas Instruments Incorporated nor the names of
     *     its contributors may be used to endorse or promote products derived
     *     from this software without specific prior written permission.
     *  
     *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     *  AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     *  THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     *  PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     *  CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     *  EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     *  PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     *  OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     *  WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     *  OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     *  EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     *  Contact information for paper mail:
     *  Texas Instruments
     *  Post Office Box 655303
     *  Dallas, Texas 75265
     *  Contact information: 
     *  http://www-k.ext.ti.com/sc/technical-support/product-information-centers.htm?
     *  DCMP=TIHomeTracking&HQS=Other+OT+home_d_contact
     *  ============================================================================
     *  
     */
    
    
    
    /* Standard headers */
    #include <ti/syslink/Std.h>
    
    /* Linux specific header files */
    #include <linux/kernel.h>
    #include <linux/version.h>
    #include <linux/types.h>
    #include <linux/module.h>
    #include <linux/init.h>
    #include <linux/device.h>
    #include <linux/fs.h>
    #include <linux/cdev.h>
    #include <linux/major.h>
    #include <linux/proc_fs.h>
    #include <linux/fs.h>
    #include <linux/mm.h>
    #include <asm/uaccess.h>
    
    #ifndef CONFIG_MMU
    #include <linux/backing-dev.h>
    #endif
    
    
    /* OSAL and utils headers */
    #include <ti/syslink/utils/Memory.h>
    #include <ti/syslink/utils/List.h>
    #include <ti/syslink/utils/IGateProvider.h>
    #include <ti/syslink/utils/GateMutex.h>
    #include <ti/syslink/utils/Trace.h>
    #include <ti/syslink/inc/TraceDrv.h>
    #include <ti/syslink/inc/TraceDrvDefs.h>
    #include <ti/syslink/utils/Cache.h>
    #include <ti/syslink/inc/CacheDrv.h>
    #include <ti/syslink/inc/CacheDrvDefs.h>
    #include <ti/syslink/inc/knl/OsalDriver.h>
    #include <ti/syslink/inc/OsalDrvDefs.h>
    
    #include <ti/syslink/utils/String.h>
    
    #include <ti/ipc/SharedRegion.h>
    #include <ti/syslink/inc/_SharedRegion.h>
    
    
    /* =============================================================================
     * macros & defines
     * =============================================================================
     */
    /*!
     *  @def    MAX_OSAL_DRIVERS
     *  @brief  Maximum number of os driver that can be created.
     */
    #define MAX_OSAL_DRIVERS       (20)
    
    /*!
     *  @def    OSALDRIVER_CLASSNAME
     *  @brief  Name of the driver class.
     */
    #define OSALDRIVER_CLASSNAME   "syslinkipc"
    
    /*!
     *  @brief  Driver minor number for OSAL.
     */
    #define OSAL_DRV_MINOR_NUMBER   12u
    
    #define NUM_CACHEMMAP_ENTRIES 16
    
    
    /* =============================================================================
     * Structure & Enums
     * =============================================================================
     */
    
    typedef struct OsalDrv_CachemmapParams {
        ULong physAddr;
    } OsalDrv_CachemmapParams;
    
    /* Structure for defining Driver state. */
    typedef struct OsalDriver_ModuleObject {
        IGateProvider_Handle gateHandle;
        /* Handle for protecting the obj list operation */
        UInt32            refCount;
        /* Reference count for this module */
        struct class *    _class;
        /* class struct for device create. */
        UInt32            major;
        /* Dynamically allocated major number of the device */
        OsalDriver_Handle osalDrvHandle;
        /* */
        OsalDrv_CachemmapParams cachemmap[NUM_CACHEMMAP_ENTRIES];
        /* physical addrs to be cached for mmap */
    } OsalDriver_ModuleObject;
    
    
    /** ============================================================================
     *  Forward declarations of internal functions
     *  ============================================================================
     */
    /*!
     *  @brief  Linux driver function to open the driver object.
     */
    static int OsalDrv_open (struct inode * inode, struct file * filp);
    
    /*!
     *  @brief  Linux driver function to close the driver object.
     */
    static int OsalDrv_close (struct inode * inode, struct file * filp);
    
    /* Linux driver function to map memory regions to user space. */
    static int OsalDrv_mmap (struct file * filp, struct vm_area_struct * vma);
    
    typedef struct OsalDrv_NormalMemory {
        UInt32       addr;
        UInt32       size;
    } OsalDrv_NormalMemory;
    
    static Bool _OsalDrv_isNormalMemory(UInt32 addr, UInt32 size);
    /*
     * This table defines all memory ranges that need to be mapped as Normal memory
     */
    #if defined(SYSLINK_VARIANT_TI814X)
    #define ADDR_TABLE_SIZE 6
    static OsalDrv_NormalMemory addrTable[ADDR_TABLE_SIZE] =
        {
            { /* OCMC */
                .addr     = 0x40300000,
                .size     = 0x20000
            },
            { /* DSP L2 RAM */
                .addr     = 0x40800000,
                .size     = 0x40000
            },
            { /* DSP L1P RAM */
                .addr     = 0x40E00000,
                .size     = 0x8000
            },
            { /* DSP L1D RAM */
                .addr     = 0x40F00000,
                .size     = 0x8000
            },
            { /* Ducati L2 */
                .addr     = 0x55020000,
                .size     = 0x10000
            },
            { /* DDR */
                .addr     = 0x80000000,
                .size     = 0x80000000
            },
        };
    #elif defined(SYSLINK_VARIANT_TI816X)
    #define ADDR_TABLE_SIZE 7
    static OsalDrv_NormalMemory addrTable[ADDR_TABLE_SIZE] =
        {
            { /* OCMC0 */
                .addr     = 0x40300000,
                .size     = 0x40000
            },
            { /* OCMC1 */
                .addr     = 0x40400000,
                .size     = 0x40000
            },
            { /* DSP L2 RAM */
                .addr     = 0x40800000,
                .size     = 0x40000
            },
            { /* DSP L1P RAM */
                .addr     = 0x40E00000,
                .size     = 0x8000
            },
            { /* DSP L1D RAM */
                .addr     = 0x40F00000,
                .size     = 0x8000
            },
            { /* Ducati L2 */
                .addr     = 0x55020000,
                .size     = 0x40000
            },
            { /* DDR */
                .addr     = 0x80000000,
                .size     = 0x80000000
            },
        };
    #elif defined(SYSLINK_VARIANT_TI811X)
    #define ADDR_TABLE_SIZE 6
    static OsalDrv_NormalMemory addrTable[ADDR_TABLE_SIZE] =
        {
            { /* OCMC */
                .addr     = 0x40300000,
                .size     = 0x40000
            },
            { /* DSP L2 RAM */
                .addr     = 0x40800000,
                .size     = 0x40000
            },
            { /* DSP L1P RAM */
                .addr     = 0x40E00000,
                .size     = 0x8000
            },
            { /* DSP L1D RAM */
                .addr     = 0x40F00000,
                .size     = 0x8000
            },
            { /* Ducati L2 */
                .addr     = 0x55020000,
                .size     = 0x10000
            },
            { /* DDR */
                .addr     = 0x80000000,
                .size     = 0x80000000
            },
        };
    #elif defined(SYSLINK_VARIANT_TI813X)
    #define ADDR_TABLE_SIZE 3
    static OsalDrv_NormalMemory addrTable[ADDR_TABLE_SIZE] =
        {
            { /* OCMC */
                .addr     = 0x40300000,
                .size     = 0x40000
            },
            { /* Ducati L2 */
                .addr     = 0x55020000,
                .size     = 0x10000
            },
            { /* DDR */
                .addr     = 0x80000000,
                .size     = 0x80000000
            },
        };
    #elif defined(SYSLINK_PLATFORM_OMAP3530)
    #define ADDR_TABLE_SIZE 5
    static OsalDrv_NormalMemory addrTable[ADDR_TABLE_SIZE] =
        {
            { /* OCMC */
                .addr     = 0x40200000,
                .size     = 0x10000
            },
            { /* DSP L2 RAM */
                .addr     = 0x5C7F8000,
                .size     = 0x18000
            },
            { /* DSP L1P RAM */
                .addr     = 0x5CE00000,
                .size     = 0x8000
            },
            { /* DSP L1D RAM */
                .addr     = 0x5CF04000,
                .size     = 0x14000
            },
            { /* SDRAM */
                .addr     = 0x70000000,
                .size     = 0x90000000
            },
        };
    
    #else
    #define ADDR_TABLE_SIZE 0
    static OsalDrv_NormalMemory addrTable[] =
        {
            { /* DDR */
                .addr     = 0x80000000,
                .size     = 0x80000000
            },
        };
    
    #endif
    /*!
     *  @brief  Linux driver function to ioctl of the driver object.
     */
    static long OsalDrvDrv_ioctl (struct file *  filp,
                                  unsigned int   cmd,
                                  unsigned long  args);
    
    #ifndef CONFIG_MMU
    /*!
     *  @brief  Linux driver function to read of the driver object.
     */
    static ssize_t
    OsalDrv_read(struct file *file, char __user *buf, size_t count, loff_t *ppos);
    
    /*!
     *  @brief  Linux driver function to unmapp the driver object.
     */
    static unsigned long OsalDrv_unmapped_area(struct file *filp,
                                       unsigned long orig_addr,
                                       unsigned long len,
                                       unsigned long pgoff,
                                       unsigned long flags);
    
    static struct backing_dev_info OsalDrv_backing_dev_info;
    #endif
    
    
    
    /* =============================================================================
     * Globals
     * =============================================================================
     */
    /*!
     *  @var    OsalDriver_state
     *
     *  @brief  OsalDriver state object variable
     */
    #if !defined(SYSLINK_BUILD_DEBUG)
    static
    #endif /* if !defined(SYSLINK_BUILD_DEBUG) */
    OsalDriver_ModuleObject OsalDriver_state =
    {
        .refCount = 0
    };
    
    /*!
     *  @brief  File operations table for Osal.
     */
    static struct file_operations OsalDrv_driverOps = {
        open:    OsalDrv_open,
        release: OsalDrv_close,
        mmap:    OsalDrv_mmap,
        unlocked_ioctl:   OsalDrvDrv_ioctl,
    #ifndef CONFIG_MMU
        /* dummy functions to satisfy no MMU module in kernel */
        read:              OsalDrv_read,
        get_unmapped_area: OsalDrv_unmapped_area,
    #endif
    } ;
    
    /* Extern declaration to Global trace flag. */
    extern Int curTrace;
    
    
    /* =============================================================================
     * APIs
     * =============================================================================
     */
    
    #ifndef CONFIG_MMU
    /*!
     *  @brief      dummy read function to satisfy no mmu mmap handling
     *
     *  @sa         Osal driver read function
     */
    static ssize_t
    OsalDrv_read(struct file *file, char __user *buf, size_t count, loff_t *ppos)
    {
        return 0;
    }
    
    /*!
     *  @brief      dummy unmapped_area function to satisfy no mmu mmap handling
     *
     *  @sa         Osal driver unmapped_area function
     */
    static unsigned long OsalDrv_unmapped_area(struct file *filp,
                                                      unsigned long orig_addr,
                                                      unsigned long len,
                                                      unsigned long pgoff,
                                                      unsigned long flags)
    {
            return (pgoff << PAGE_SHIFT);
    }
    #endif
    
    /*!
     *  @brief      Initialize the Driver module.
     *
     *  @sa         OsalDriver_destroy
     */
    Int32
    OsalDriver_setup (Void)
    {
        Int32          status = OSALDRIVER_SUCCESS;
        Int32          osStatus = 0 ;
        IArg           key;
        dev_t          dev;
        Error_Block    eb;
        Int            i;
    
        GT_0trace (curTrace, GT_ENTER, "OsalDriver_setup");
        Error_init (&eb);
    
        if (OsalDriver_state.refCount == 0) {
            /* Initialize the refCount */
            OsalDriver_state.refCount = 1;
    
            for (i = 0; i < NUM_CACHEMMAP_ENTRIES; i++) {
                OsalDriver_state.cachemmap[i].physAddr = 0;
            }
    
            OsalDriver_state.gateHandle = (IGateProvider_Handle)
                                   GateMutex_create ((GateMutex_Params*)NULL, &eb);
    #if !defined(SYSLINK_BUILD_OPTIMIZE)
            if (OsalDriver_state.gateHandle == NULL) {
                /*! @retval OSALDRIVER_E_FAIL Failed to create the gate */
                status = OSALDRIVER_E_FAIL;
                GT_setFailureReason(curTrace,
                                    GT_4CLASS,
                                    "OsalDriver_setup",
                                    status,
                                    "Failed to create the gate!");
            }
            else {
    #endif /*!defined(SYSLINK_BUILD_OPTIMIZE)*/
                OsalDriver_state._class = class_create (THIS_MODULE,
                                                        OSALDRIVER_CLASSNAME);
    #if !defined(SYSLINK_BUILD_OPTIMIZE)
                if (OsalDriver_state._class == NULL) {
                    GateMutex_delete ((GateMutex_Handle *)
                                          &OsalDriver_state.gateHandle);
                    /*! @retval OSALDRIVER_E_FAIL Failed to create the driver
                                                  class */
                    status = OSALDRIVER_E_FAIL;
                    GT_setFailureReason (curTrace,
                                         GT_4CLASS,
                                         "OsalDriver_setup",
                                         status,
                                         "Failed to create the driver class!");
                }
                else {
    #endif /*!defined(SYSLINK_BUILD_OPTIMIZE)*/
                    osStatus = alloc_chrdev_region (&dev,
                                                    0,
                                                    MAX_OSAL_DRIVERS,
                                                    OSALDRIVER_CLASSNAME);
                    OsalDriver_state.major = MAJOR(dev);
    #if !defined(SYSLINK_BUILD_OPTIMIZE)
                    if (osStatus != 0) {
                        class_destroy (OsalDriver_state._class);
                        GateMutex_delete ((GateMutex_Handle *)
                                          &OsalDriver_state.gateHandle);
                        /*! @retval OSALDRIVER_E_FAIL Failed to create region of
                                                      devices */
                        status = OSALDRIVER_E_FAIL;
                        GT_setFailureReason (curTrace,
                                             GT_4CLASS,
                                             "OsalDriver_setup",
                                             status,
                                             "Failed to create region of devices!");
                    }
                }
            }
    #endif /*!defined(SYSLINK_BUILD_OPTIMIZE)*/
    
            /* Register the OSAL driver */
            if (status >= 0) {
                OsalDriver_state.osalDrvHandle = OsalDriver_registerDriver ("Osal",
                                                                 &OsalDrv_driverOps,
                                                             OSAL_DRV_MINOR_NUMBER);
    #if !defined(SYSLINK_BUILD_OPTIMIZE)
                if (OsalDriver_state.osalDrvHandle == NULL) {
                    GT_setFailureReason (curTrace,
                                         GT_4CLASS,
                                         "OsalDriver_setup",
                                         OSALDRIVER_E_INVALIDARG,
                                         "OsalDriver_registerDriver failed!");
                    OsalDriver_destroy ();
                }
    #endif /* if !defined(SYSLINK_BUILD_OPTIMIZE) */
            }
        }
        else {
            key = IGateProvider_enter (OsalDriver_state.gateHandle);
            OsalDriver_state.refCount++;
            IGateProvider_leave (OsalDriver_state.gateHandle, key);
        }
    
        GT_0trace (curTrace, GT_LEAVE, "OsalDriver_setup");
    
        /*! @retval OSALDRIVER_SUCCESS operation successful */
        return status;
    }
    
    
    /*!
     *  @brief      Finalize the Driver module.
     *
     *  @sa         OsalDriver_setup
     */
    Int32
    OsalDriver_destroy (Void)
    {
        Int32       status = OSALDRIVER_SUCCESS;
        IArg        key;
    
        GT_0trace (curTrace, GT_ENTER, "OsalDriver_destroy");
    
        if (OsalDriver_state.refCount == 1) {
            /* Unregister the Osal Drviver */
            OsalDriver_unregisterDriver (
                             (OsalDriver_Handle *) &OsalDriver_state.osalDrvHandle);
    
            unregister_chrdev_region (MKDEV(OsalDriver_state.major, 0),
                                      MAX_OSAL_DRIVERS);
            class_destroy (OsalDriver_state._class);
    
            /* Delete the Gate handle */
            status = GateMutex_delete ((GateMutex_Handle *)
                                        &OsalDriver_state.gateHandle);
            GT_assert (curTrace, (status >= 0));
    
            OsalDriver_state.refCount = 0;
        }
        else {
            key = IGateProvider_enter (OsalDriver_state.gateHandle);
            OsalDriver_state.refCount--;
            IGateProvider_leave (OsalDriver_state.gateHandle, key);
        }
    
        GT_0trace (curTrace, GT_LEAVE, "OsalDriver_destroy");
    
        /*! @retval OSALDRIVER_SUCCESS Operation successful */
        return status;
    }
    
    
    /*!
     *  @brief      function to register a driver with the OS kernel
     *
     *  @param      name  Name of the driver.
     *  @param      fops  File operations table.
     *  @param      minor Minor numberof the driver.
     *
     *  @sa         OsalDriver_unregisterDriver
     */
    OsalDriver_Handle
    OsalDriver_registerDriver (String                   name,
                               struct file_operations * fops,
                               UInt32                   minor)
    {
        struct OsalDriver_Object * object = NULL;
        IArg                       key;
        Int32                      osStatus;
        Int32                      devNo;
    
        Char                       tempStr [50];
    
    
        GT_3trace (curTrace,
                   GT_ENTER,
                   "OsalDriver_registerDriver",
                   name,
                   fops,
                   minor);
    
        GT_assert (curTrace, (name != NULL));
        GT_assert (curTrace, (fops != NULL));
    
    #if !defined(SYSLINK_BUILD_OPTIMIZE)
        if (OsalDriver_state.refCount == 0) {
            /*! @retval NULL   Module is in invalid state */
            GT_setFailureReason (curTrace,
                                 GT_4CLASS,
                                 "OsalDriver_registerDriver",
                                 OSALDRIVER_E_INVALIDSTATE,
                                 "Module is in invalid state!");
        }
        else if (name == NULL) {
            /*! @retval NULL   Passed name is null */
            GT_setFailureReason (curTrace,
                                 GT_4CLASS,
                                 "OsalDriver_registerDriver",
                                 OSALDRIVER_E_INVALIDARG,
                                 "Passed name is null!");
        }
        else if (fops == NULL) {
            /*! @retval NULL   Passed fops is null */
            GT_setFailureReason (curTrace,
                                 GT_4CLASS,
                                 "OsalDriver_registerDriver",
                                 OSALDRIVER_E_INVALIDARG,
                                 "Passed fops is null!");
        }
        else {
    #endif /* if !defined(SYSLINK_BUILD_OPTIMIZE) */
            /* Allocate a handle */
            object = Memory_alloc (NULL, sizeof (OsalDriver_Object), 0, NULL);
    #if !defined(SYSLINK_BUILD_OPTIMIZE)
            if (object == NULL) {
                /*! @retval NULL   Failed to allocate memory for handle */
                GT_setFailureReason (curTrace,
                                     GT_4CLASS,
                                     "OsalDriver_registerDriver",
                                     OSALDRIVER_E_MEMORY,
                                     "Failed to allocate memory for handle!");
            }
            else {
    #endif /* if !defined(SYSLINK_BUILD_OPTIMIZE) */
                key = IGateProvider_enter (OsalDriver_state.gateHandle);
                cdev_init (&object->cdev, fops);
                object->cdev.owner = THIS_MODULE;
                object->cdev.ops   = fops;
                object->minor = minor;
                devNo = MKDEV(OsalDriver_state.major,
                              minor);
                osStatus = cdev_add (&object->cdev, devNo, 1);
    #if !defined(SYSLINK_BUILD_OPTIMIZE)
                if (osStatus) {
                    /*! @retval NULL   Failed to add the device */
                    GT_setFailureReason(curTrace,
                                        GT_4CLASS,
                                        "OsalDriver_registerDriver",
                                        OSALDRIVER_E_FAIL,
                                        "Failed to add the device!");
                }
                else {
    #endif /* if !defined(SYSLINK_BUILD_OPTIMIZE) */
                    String_cpy (tempStr, OSALDRIVER_CLASSNAME);
                    String_cat (tempStr, "_");
                    String_cat (tempStr, name);
    #if LINUX_VERSION_CODE <= KERNEL_VERSION(2,6,13)
                    class_device_create (OsalDriver_state._class,
                                   NULL,
                                   devNo,
                                   NULL,
                                   tempStr);
    #else
                    device_create (OsalDriver_state._class,
                                   NULL,
                                   devNo,
                                   NULL,
                                   tempStr);
    #endif
    #ifndef CONFIG_MMU
                    /* Initialize the backing_dev_info for Osal device */
                    memcpy(&OsalDrv_backing_dev_info,
                           &default_backing_dev_info,
                           sizeof(struct backing_dev_info));
                    OsalDrv_backing_dev_info.capabilities |= BDI_CAP_MAP_DIRECT |
                                        BDI_CAP_READ_MAP | BDI_CAP_WRITE_MAP;
    #endif
    
    #if !defined(SYSLINK_BUILD_OPTIMIZE)
                }
    #endif /* if !defined(SYSLINK_BUILD_OPTIMIZE) */
                IGateProvider_leave (OsalDriver_state.gateHandle, key);
    
    #if !defined(SYSLINK_BUILD_OPTIMIZE)
            }
        }
    #endif /*!defined(SYSLINK_BUILD_OPTIMIZE)*/
    
        GT_1trace (curTrace, GT_LEAVE,"OsalDriver_registerDriver", object);
    
        /*! @retval NULL   Operation failed */
        /*! @retval Handle Operation was successful */
        return object;
    }
    
    
    /*!
     *  @brief      function to unregister a driver
     *
     *  @param      name  Name of the driver.
     *  @param      fops  File operations table.
     *  @param      minor Minor numberof the driver.
    
     *  @sa         OsalIOCTL_Create
     */
    Int32
    OsalDriver_unregisterDriver (OsalDriver_Handle * drvHandle)
    {
        Int32                      status = OSALDRIVER_SUCCESS;
        struct OsalDriver_Object * object = NULL;
        /* IArg                       key; */
    
        GT_1trace (curTrace,
                   GT_ENTER,
                   "OsalDriver_unregisterDriver",
                   drvHandle);
    
        GT_assert (curTrace, (drvHandle != NULL));
    
    #if !defined(SYSLINK_BUILD_OPTIMIZE)
        if (OsalDriver_state.refCount == 0) {
            /*! @retval OSALDRIVER_E_INVALIDSTATE Module is in invalid state */
            status = OSALDRIVER_E_INVALIDSTATE;
            GT_setFailureReason(curTrace,
                                GT_4CLASS,
                                "OsalDriver_unregisterDriver",
                                status,
                                "Module is in invalid state!");
        }
        else if (drvHandle == NULL) {
            /*! @retval OSALDRIVER_E_INVALIDARG Passed drvHandle is null */
            status = OSALDRIVER_E_INVALIDARG;
            GT_setFailureReason(curTrace,
                                GT_4CLASS,
                                "OsalDriver_unregisterDriver",
                                status,
                                "Passed drvHandle is null!");
        }
        else if (*drvHandle == NULL) {
            /*! @retval OSALDRIVER_E_INVALIDARG *drvHandle passed is NULL */
            status = OSALDRIVER_E_INVALIDARG;
            GT_setFailureReason (curTrace,
                                 GT_4CLASS,
                                 "OsalDriver_unregisterDriver",
                                 status,
                                 "*drvHandle passed is NULL!");
        }
        else {
    #endif /* if !defined(SYSLINK_BUILD_OPTIMIZE) */
            object = *drvHandle;
            /* Gate protection creates error msg because of udev in kernel */
            /* key = IGateProvider_enter (OsalDriver_state.gateHandle); */
            device_destroy (OsalDriver_state._class,
                            MKDEV(OsalDriver_state.major, object->minor));
            cdev_del (&object->cdev);
            /* IGateProvider_leave (OsalDriver_state.gateHandle, key); */
            Memory_free (NULL, object, sizeof (OsalDriver_Object));
            *drvHandle = NULL;
    #if !defined(SYSLINK_BUILD_OPTIMIZE)
        }
    #endif /*!defined(SYSLINK_BUILD_OPTIMIZE)*/
    
        GT_1trace (curTrace, GT_LEAVE,"OsalDriver_unregisterDriver", status);
    
        return status;
    }
    
    
    /* Driver model for OSAL */
    
    /*!
     *  @brief  Linux specific function to open the driver.
     *
     *  @param  inode   Inode pointer.
     *  @param  filp    File structure pointer.
     *
     *  @sa     ProcMgrDrv_release
     */
    static
    int
    OsalDrv_open (struct inode * inode, struct file * filp)
    {
    #ifndef CONFIG_MMU
            if (filp && filp->f_mapping) {
                filp->f_mapping->backing_dev_info = &OsalDrv_backing_dev_info;
                filp->f_mode |= FMODE_WRITE;
            }
    #endif
        return 0;
    }
    
    
    /*!
     *  @brief  Linux driver function to close the driver object.
     *
     *  @param  inode   Inode pointer.
     *  @param  filp    File structure pointer.
     *
     *  @sa     ProcMgrDrv_open
     */
    static
    int
    OsalDrv_close (struct inode * inode, struct file * filp)
    
    {
        return 0;
    }
    
    
    /*!
     *  @brief  Linux driver function to map memory regions to user space.
     *
     *  @param  filp    File structure pointer.
     *  @param  vma     User virtual memory area structure pointer.
     *
     *  @sa     OsalDrv_open
     */
    static
    int
    OsalDrv_mmap (struct file * filp, struct vm_area_struct * vma)
    {
    #ifdef CONFIG_MMU
        UInt16 regionId;
        Bool   isCached = FALSE;
        ULong  physAddr;
        Int    i;
    
        /*
         * Set all regions as non-cached except for sharedRegion based on
         * cacheEnable setting
         */
    
        vma->vm_page_prot = pgprot_noncached (vma->vm_page_prot);
        physAddr = vma->vm_pgoff << PAGE_SHIFT;
    
        regionId = _SharedRegion_getIdPhys((Ptr)physAddr);
        if (regionId != SharedRegion_INVALIDREGIONID) {
            isCached = SharedRegion_isCacheEnabled(regionId);
        }
        else {
            for (i = 0; i < NUM_CACHEMMAP_ENTRIES; i++) {
                if (OsalDriver_state.cachemmap[i].physAddr == physAddr) {
                    isCached = TRUE;
                    OsalDriver_state.cachemmap[i].physAddr = 0;
    
                    break;
                }
            }
        }
    
        GT_2trace(curTrace, GT_2CLASS,
                   "OsalDrv_mmap(): setting cache %s for physical address %p",
                   isCached ? "enabled" : "disabled", physAddr);
    
        if (_OsalDrv_isNormalMemory((UInt32) physAddr,
                                     vma->vm_end - vma->vm_start)) {
            /*
             * Map as Normal Memory (as opposed to Strongly Ordered)
             */
            if (isCached == TRUE) {
                vma->vm_page_prot = __pgprot(pgprot_val(vma->vm_page_prot) |
                    L_PTE_MT_WRITEBACK);
            }
            else {
                /* Un-cached */
                vma->vm_page_prot = __pgprot(pgprot_val(vma->vm_page_prot) |
                    L_PTE_MT_BUFFERABLE );
            }
        }
        else {
            /* Do not map as Normal Memory */
            if (isCached == TRUE) {
                vma->vm_page_prot = __pgprot(pgprot_val(vma->vm_page_prot) |
                    (L_PTE_MT_WRITETHROUGH | L_PTE_MT_BUFFERABLE));
            }
        }
    #endif
    
        if (remap_pfn_range (vma,
                             vma->vm_start,
                             vma->vm_pgoff,
                             vma->vm_end - vma->vm_start,
                             vma->vm_page_prot)) {
            return -EAGAIN;
        }
        return 0;
    }
    
    /*!
     *  @brief  Linux specific function to close the driver.
     */
    static
    long OsalDrvDrv_ioctl (struct file *  filp,
                           unsigned int   cmd,
                           unsigned long  args)
    {
        int    osStatus = 0;
        int    rv;
        Int32  status = OSALDRIVER_SUCCESS;
    
        GT_3trace (curTrace, GT_ENTER, "OsalDrvDrv_ioctl",
                   filp, cmd, args);
    
        switch (cmd) {
            case CMD_TRACEDRV_SETTRACE:
            {
                TraceDrv_ioctl ((UInt32) cmd, (Ptr) args);
            }
            break;
    
            case CMD_CACHE_INV:
            case CMD_CACHE_WB:
            case CMD_CACHE_WBINV:
            case CMD_CACHE_WAIT:
            case CMD_CACHE_SETMODE:
            {
                status = CacheDrv_ioctl ((UInt32) cmd, (Ptr) args);
            }
            break;
    
            case CMD_OSALDRV_CACHEMMAP:
            {
                OsalDrv_CmdArgs *cargs = (OsalDrv_CmdArgs *)args;
                OsalDrv_CmdArgs cachemmapArgs;
                Int index;
    
                rv = copy_from_user(&cachemmapArgs, cargs,
                                    sizeof (OsalDrv_CmdArgs));
                if (rv != 0) {
                    osStatus = -EFAULT;
    
                    break;
                }
    
                index = 0;
                while (index < NUM_CACHEMMAP_ENTRIES &&
                       OsalDriver_state.cachemmap[index].physAddr != 0) {
    
                    if (OsalDriver_state.cachemmap[index].physAddr ==
                        cachemmapArgs.physAddr) {
    
                        break;
                    }
                    index++;
                }
    
                if (index == NUM_CACHEMMAP_ENTRIES) {
                    cachemmapArgs.apiStatus = OSALDRIVER_E_MEMORY;
                }
                else {
                    GT_1trace(curTrace, GT_2CLASS,
                              "OsalDrvDrv_ioctl(): CMD_OSALDRV_CACHEMMAP - "
                              "tagging physAddr %p as cacheable for mmap()\n",
                              cachemmapArgs.physAddr);
    
                    OsalDriver_state.cachemmap[index].physAddr =
                        cachemmapArgs.physAddr;
    
                    cachemmapArgs.apiStatus = OSALDRIVER_SUCCESS;
                }
    
                rv = copy_to_user(cargs, &cachemmapArgs,
                                  sizeof (OsalDrv_CmdArgs));
                if (rv != 0) {
                    osStatus = -EFAULT;
                }
            }
    
            break;
    
            default:
            {
                /* This does not impact return status of this function, so retVal
                 * comment is not used.
                 */
                status = OSALDRIVER_E_INVALIDARG;
                GT_setFailureReason (curTrace,
                                     GT_4CLASS,
                                     "OsalDrvDrv_ioctl",
                                     status,
                                     "Unsupported ioctl command specified");
            }
            break;
        }
    
        GT_1trace (curTrace, GT_LEAVE, "OsalDrvDrv_ioctl", osStatus);
    
        /*! @retval 0 Operation successfully completed. */
        return osStatus;
    }
    
    /*!
     *  @brief      Checks if memory range should be mapped as Normal memory
     */
    static Bool
    _OsalDrv_isNormalMemory(UInt32 addr, UInt32 size) {
        Bool   ret = FALSE;
        UInt32 upperBound;
        Int    i;
    
        for (i = 0; i < ADDR_TABLE_SIZE; i++) {
            upperBound = addrTable[i].addr + addrTable[i].size - 1;
            /*
             * If the range to be mapped is entirely within a range to be mapped as
             * Normal, then do it. Otherwise be conservative and mapped as strongly
             * ordered.
             */
            if ((addr >= addrTable[i].addr) &&
                (addr + size - 1 <= upperBound)) {
                ret = TRUE;
                break;
            }
        }
    
        return (ret);
    }
    

    Attached is OsalDriver.c from syslink syslink_2_21_01_05. You should be able to replace file and recompile. The uncached memory page should now be configured for BUFFERABLE.

    If you are accessing the buffer via A8 and the number of bytes accessed is more than 10K bytes /sec you should definitely enable  caching on A8 irrespective of the alignment issue. The performance with cache disabled will be 10 - 50 x worse than cache enabled.Syslink has APIs for cache coherency handling from user space. Refer ti/syslink/utils/Cache.h

  • Hi Badri,

    I have replaced this file in my older Syslink and I can now access the memory in an unaligned manner. :-)


    My logical next question is, how do I flush the A8 cache so that I can access this buffer on the DSP? Is there a standard Syslink way to do this?

    Thanks,
    Ralph

  • You need to perform cache coherency operation only if you make the SharedRegion cacheable. Simply making it MT_BUFFERABLE doesn't require any cache coherency operation. As I mentioned in my previous post  if you want to do cache operation

    "Syslink has APIs for cache coherency handling from user space. Refer ti/syslink/utils/Cache.h"

  • Okay, by the sound of it I have to mark my shared region as cacheable as it will be accessed by the A8. How do I do this?

    As mentioned previously, I'm using this code to create the buffer:

    heap = (IHeap_Handle)SharedRegion_getHeap(2);

    buf = Memory_alloc(heap, length, 128, NULL);

    Also, in Cache.h what should I set these function parameters to?

    Ptr blockPtr, UInt32 byteCnt, Bits16 type, Bool wait

    Thanks,
    Ralph

  • To make sharedRegion cacheable set

    SharedRegion.setEntryMeta( 2,
        {
          base:        sr2MemSection.base,
          len:         sr2MemSection.len,
          name:        sr2MemSection.name,
          isValid:     true,
          ownerProcId: srOwnerProcId,
          cacheEnable: true, //cacheEnable SR2
          cacheLineSize: 128,
          createHeap:  true
        }
    );

    in the cfg file for M3 and c674. And modify the firmware loader to set

        SysLink_params  = "SharedRegion.entry[2].cacheEnable=TRUE;" ;
        SysLink_setup ();

    The Syslink_params string should be set before doing syslink_setup. COnfirm by putting printks in Osal_driver that the SR2 is getting configured as cached.

    I am not sure if there is any additional step required in ezSDK. The above works if your sharedregion is statically configured (setup at firmware load time rather ).

  • Do I still need to alter

    media-controller-utils-3_00_00_05/src/firmware_loader/memsegdef_default.c

    as you suggested in another post to change the line

    (1 << LDR_CORE_ID_VM3) | (1 << LDR_CORE_ID_DM3) | (1 << LDR_CORE_ID_A8) | (1 << LDR_CORE_ID_DSP),

    to

    (1 << LDR_CORE_ID_VM3) | (1 << LDR_CORE_ID_DM3) |  (1 << LDR_CORE_ID_DSP),

    in the "Segment 3" section?

    Thanks.

  • Okay, so in my codec server "server.cfg" file, I have this:

    SharedRegion.setEntryMeta(
        SharedRegion_map["Ipc"],  /* index */
        entry2
    );

    var entry3 = new SharedRegion.Entry();

    entry3.base = SharedRegion2SharedMem.base;
    entry3.len = SharedRegion2SharedMem.len;
    entry3.ownerProcId = MultiProc.getIdMeta("HOST");
    entry3.isValid = true;
    entry3.createHeap = true;
    entry3.cacheEnable = true;
    entry3.name = "SR2";

    SharedRegion.setEntryMeta(
        SharedRegion_map["Shared Region 2"],  /* index */
        entry3
    );

    So that part has cache enabled. I've also made the change to memsegdef_default.c that I outlined in my previous post.

    Unfortunately I can't find anything like "SysLink_params" in the firmware_loader source code. Please could you describe where I can find this?

    I put printks in my Osal_driver.c and sadly the shared region is still marked as uncacheable (b3d00000 is the start of SR2 in the memory map):

    OsalDrv_mmap(): setting cache disabled for physical address b3d00000

    ***Memory marked as L_PTE_MT_BUFFERABLE***

    Thanks,
    Ralph

  • As I mentioned you will have to add the line.Below is code from dvr_rdk firmware loader.Refer syslink user guide for documentation.

    #include <ti/syslink/SysLink.h>

    int main (int argc, char ** argv)
    {
        Int     status       = 0;
        Bool    startupProc  = FALSE;
        Bool    shutdownProc = FALSE;
        Bool    dll          = FALSE;
        UInt16  procId       = MultiProc_INVALIDID;

        /* To enable caching of shared region, the below string should
         * be set.
         * TODO: This is currently hard coded to shared region 1.
         * This parameter should come as an argument to the firmware
         * load application
         */
        SysLink_params  = "SharedRegion.entry[2].cacheEnable=TRUE;" ; //ADD THIS LINE
        SysLink_setup ();

  • Hi Badri, I don't actually have anything containing "SysLink_params" in my DSP source code.

    I've marked the thread as resolved since my original problem has now been fixed and I don't require any further help with the caching issue.

    Thanks,

    Ralph

  • The line will not exist. As mentioned before you have to _add_ the line,

    Also the line should be added in the firmware loader running on A8 not on DSP.

    I am not familiar with ezSDK but I think the file to be modified incase you want to pursue this further is:

    \board-support\media-controller-utils_3_00_00_05\src\firmware_loader\firmware_loader.c

    int main (int argc, char *argv[])

    ..

      configTraceLevel (&currDebugLevel);

       //ADD CODE HERE

      SysLink_setup ();

  • Ah, I beg your pardon. I was in a rush and didn't read the post properly.