Hi
Our usage is such that :-
There is a 6 - DSP "TI C6670" communication with Vertex FPGA via "6 - SRIO" Links respectively.
Earlier we were using the TI C6670 DSP to communicate with vertex FPGA ---> SRIO Gen 1.
Now the FPGA guys have upgraded to SRIO GEN 2 "IP Interface" Vertex board.
Now problem we are facing is that :-
Using 2 DSP - FPGA SRIO links , At the first start up for both DSP and FPGA links are working fine but when ever DSP resets or reloads again , then the FPGA is not able to get SRIO LOCK " synchronize " though LINK and PORT state is OK. In this scenario using the NREAD transaction is fetching invalid data.
This behaviour happened only with one DSP, the other DSP works fine all the time.
Please guide me how to resolve the Issue.
Thanks and Regards,
Manav