This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Interfacing 3X4 matrix keypad to TI8148 gpio and PSP used is linux-04.01.00.07.



 Hi,

I have interface a 3x4 keypad matrix to TI8148 GPIO pins and PSP used is linux-04.01.00.07.

It has 3 colums and 4 rows.

Four row lines are pulled high.

I want to use the input subsystem GPIO matrix keypad driver for it. For that I have provided the platform data in board specific file and enabled the "matrix-keypad" driver support (drivers/input/keyboard/matrix_keypad.c). It is coming up with /dev/input/event0. From application when I am reading the /dev/input/event0 for key.code, it is showing three keys pressed.

output for 1 key pressed:

 : [key 8]
  : [key 9]
  : [key 10]
does I am going in right direction?

Regards,

Sudheer.