Other Parts Discussed in Thread: AM3352
Hi all,
we're currently experiencing a strange issue on an AM3352 based platform.
We're using a vanilla Linux Kernel with realtime extension: Linux-3.12.11-rt17
Additionally we're running the PM firmware from:
git://arago-project.org/git/projects/am33x-cm3.git
based on commit:
32cf44e25b5828b87af6dceebc3a49fed5d858ac
When activating CPU idle support we can see a random slowdown
of the system by factor 20-30 (we did a couple of measurements
using the tracing infrastructure).
Usually handling a timer interrupt takes round about 25us. When
the problem triggers this takes up to 650us and theres no idle time
left (usually we have 85% idle time)!!
There's no runaway task or anything like that, the system just slows
down! This definitely just happens with CPU idle and the PM firmware.
(I can provide some traces, if needed).
Any ideas what might go wrong here? Did someone else encounter
the same problem before? Are there any known issues with the PM
firmware?
Cheers,
Jan