Other Parts Discussed in Thread: TLC59108
I am using ti-ezsdk_dm814x-evm_5_05_02_00 to build the Linux system including TIGON3 driver module for Broadcom NetXtreme BCM5751 based Gigabit Ethernet Controller card as a PCIe Endpoint. However, when I load the tg3.ko module, it causes the system to crash in tg3_chip_reset() function while resetting the BCM57xx chip. May be EP reset causes the system/PCIe bus to go in undefined state. Our BCM5751 card works fine with Linux driver tg3.ko on Dell machine but why are we facing this reset issue with Mistral DM814x EVM Rev D? Is there any hardware/software configuration that we are missing.
- We are setting the max. remote read request size (MRRQS) to 128
- Placing the firmware files (tg3.bin and tg3_tso/bin) in the root file system at /lib/firmware
Your urgent insight in this matter will be highly appreciated.
Thanks.