Hi.
I found an image rescaling library in VLIB_3.2, VLIB_image_rescale.
But, in the VLIB_image_rescale description the library fuction is supported only 1/2 downscale in each direction.
Is there any library or sourcec code to rescailing of an input image not only 1/2 scale but also another scales?
For example, I want to reduce an input image to 0.9 times in each direction.
Regards,
Tahk.