I have looked at the EVM's that have RTC battery backup and all use TPS65910 PMIC. I found the RTC section in the AM335x Schematic Checklist useful.
The device I am working on will not have power ON/OFF, standby, or low power modes. The device will be powered ON whenever 5v is applied to the PMIC AC or USB inputs (there will be no battery attached to BAT1 or BAT2). We want to have a coin cell (or preferably a supercap) supplying RTC battery backup power when the 5v input is not present to maintain the Real Time Clock.
Is there a reference design to support RTC battery backup on the TPS65217C PMIC? Reading throug the various specs it appears that all that is needed is to supply an indipendent 1.8v to the VDDS_RTC AM3358 input (assuming 1uF attached to CAP_VDD_RTC and RTC_KALDO_ENn pulled low). Is this correct? With 1.8v applied to VDDS_RTC, would I expect the RTC LDO to be running and 1.1v on the CAP_VDD_RTC pin? Also, would I to be able to scope the RTC 32khz crystal for a signal to indicate the RTC is running?
Is there an accepted method to regulate the VDDS_RTC voltage at 1.8v to reduce load on the battery?
Thanks,
Brian