Other Parts Discussed in Thread: TPS65217
Dear TI,
I am working on total power consumption by BBB
now there are various voltage to the sitara processors. by the PMIC TPS65217.pdf
VDD_CORE,VDD_MPU, VDDS_RTC,VDDS_DDR,VDDS,VDDS_SRAM_CORE_BG,VDDS_SRAM_MPU_BB,VDDS_PLL_DDR,VDDS_PLL_CORE_LCD,VDDS_PLL_MPU,VDDS_OSC,VDDA1P8V_USB0/1,VDDA3P3V_USB0/1,VDDA_ADC,VDDSHV1,VDDSHV2 *,VDDSHV3 *,VDDSHV4,VDDSHV5,VDDSHV6
Questions:
- may i know in sleep mode which of the above voltages are operational?
- i wanted to disable the LDO4 power rail during runtime now data sheet of tps65217 say to write a value of '1' in D5 bit of the Enable Register(0x16h). it is correct or do i need to do write some other register as well or just this register(0x16h) is sufficient to turn off the LDO4 power rail. i know i2c is also connected to the LDO4 rail but for time being assume the tps65217 has i2c pull register using a different power rail.
Regards
Regards