Other Parts Discussed in Thread: TLVH431
Hi,
In AM572x GPEVM schematics, the shunt regulator circuit used between 3.3V (vddshv) and 1.8V (vdds18v) rails of the processor is to prevent the maximum difference between these rails from exceeding 2V during power down. I have a few queries regarding the same:
1. I understand that this protection circuit will be required in the case when the PMIC supply voltage is discharged within a short time (less than 1 ms). That is because, in that case even though the PMIC will start sequencing down, there will not be input power to supply 1.8V and 3.3V, and both will start to decay.
I wanted to understand the conditions under which this would occur. As per my understanding, if the event triggering the OFF request is VSYS_LO, then the protection circuit is required. It is not required otherwise. Can you please confirm if this is correct?
2. As per our understanding for this circuit to function as regulator, the cathode voltage/current of the shunt regulator - TLVH431 should be fed back to the reference input pin (closed loop mode). However in the EVM this feedback resistor between cathode and reference input is not mounted. Can you please confirm if this resistor is required for the circuit to function correctly? Also, if yes, then what should be the value of this resistor?
Regards,
Prachi