Dear community,
we are using the K2K evm board at our department and want to use 10 G Ethernet with that.
Currently, we are using the Open Embedded environment to build our own Processor SDK with the 4.1.8 Linux kernel.
I know there are instructions for the MCSDK under:
http://processors.wiki.ti.com/index.php/MCSDK_UG_Chapter_Exploring#10Gig_Ethernet_Driver
While in the latest MCSDK the keystone2_defconfig is already changed to support 10 G Ethernet (CONFIG_TI_KEYSTONE_XGE=y), I am missing that for the Processor SDK.
Moreover, there does not exist that kernel option!
The given fdt settings in U-Boot are only partly working, because the device tree has changed.
dmesg gives me:
netcp: module(netcp-xgbe) not used for device
Please I need your with that.
Kind regards,
Tobias Jaeuthe