Other Parts Discussed in Thread: SYSBIOS
Hello.
I'm trying to modify bootloader from sysbios industrial sdk 1.1.0.10 to run it from nand on custom module mtax-som-am335x.
I got some issues with MMU.
If I use original mmu initialization code I get error then I try to reset nand:
CortxA8: Can't Single Step Target Program: (Error -2062 @ 0x1FE) Unable to halt device. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.83.1)
CortxA8: Trouble Halting Target CPU: (Error -2062 @ 0x1FE) Unable to halt device. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.83.1)
It occures on line
(*(volatile unsigned char*)(cmdRegAddr)) = cmd;
where
cmdRegAddr is 0x5000007C and cmd is 0xFF
I modified MMU initialization like this:
/*
** Function to setup MMU. This function Maps three regions (1. DDR
** 2. OCMC and 3. Device memory) and enables MMU.
*/
void MMUConfigAndEnable(void)
{
/*
** Define DDR memory region of AM335x. DDR can be configured as Normal
** memory with R/W access in user/privileged modes. The cache attributes
** specified here are,
** Inner - Write through, No Write Allocate
** Outer - Write Back, Write Allocate
*/
REGION regionDdr = {
MMU_PGTYPE_SECTION, START_ADDR_DDR, NUM_SECTIONS_DDR,
MMU_MEMTYPE_NORMAL_NON_SHAREABLE(MMU_CACHE_WT_NOWA,
MMU_CACHE_WB_WA),
MMU_REGION_NON_SECURE, MMU_AP_PRV_RW_USR_RW,
(unsigned int*)pageTable
};
/*
** Define OCMC RAM region of AM335x. Same Attributes of DDR region given.
*/
REGION regionOcmc = {
MMU_PGTYPE_SECTION, START_ADDR_OCMC, NUM_SECTIONS_OCMC,
MMU_MEMTYPE_NORMAL_NON_SHAREABLE(MMU_CACHE_WT_NOWA,
MMU_CACHE_WB_WA),
MMU_REGION_NON_SECURE, MMU_AP_PRV_RW_USR_RW,
(unsigned int*)pageTable
};
/*
** Define Device Memory Region. The region between OCMC and DDR is
** configured as device memory, with R/W access in user/privileged modes.
** Also, the region is marked 'Execute Never'.
*/
REGION regionDev = {
MMU_PGTYPE_SECTION, START_ADDR_DEV, NUM_SECTIONS_DEV,
MMU_MEMTYPE_STRONG_ORD_SHAREABLE,
MMU_REGION_NON_SECURE,
MMU_AP_PRV_RW_USR_RW ,
(unsigned int*)pageTable
};
REGION regionDev2 = {
MMU_PGTYPE_SECTION, 0x50000000, 10,
MMU_MEMTYPE_DEVICE_SHAREABLE,//MMU_MEMTYPE_NORMAL_NON_SHAREABLE(0,
// 0),
MMU_REGION_NON_SECURE,
MMU_AP_PRV_RW_USR_RO| MMU_SECTION_EXEC_NEVER ,
(unsigned int*)pageTable
};
REGION regionDev3 = {
MMU_PGTYPE_SECTION, 0x10000000, 1,
MMU_MEMTYPE_STRONG_ORD_SHAREABLE,
MMU_REGION_NON_SECURE,
MMU_AP_PRV_RW_USR_RO | MMU_SECTION_EXEC_NEVER,
(unsigned int*)pageTable
};
/* Initialize the page table and MMU */
MMUInit((unsigned int*)pageTable);
/* Map the defined regions */
MMUMemRegionMap(®ionDdr);
MMUMemRegionMap(®ionOcmc);
MMUMemRegionMap(®ionDev);
MMUMemRegionMap(®ionDev2);
MMUMemRegionMap(®ionDev3);
/* Now Safe to enable MMU */
MMUEnable((unsigned int*)pageTable);
}
It's the same procedure except regions regionDev2 and regionDev3.
After this I was able to reset nand, but I get simular error:
CortxA8: Can't Single Step Target Program: (Error -2062 @ 0x1FE) Unable to halt device. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.83.1)
CortxA8: Trouble Halting Target CPU: (Error -2062 @ 0x1FE) Unable to halt device. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.83.1)
It occures on line
pinStatus = ((HWREG(baseAddr + GPMC_STATUS) & GPMC_STATUS_WAIT0STATUS)
>> GPMC_STATUS_WAIT0STATUS_SHIFT);
where baseAddr is 0x50000000.
Please tell me how should I initialize MMU to work with nand?