We were working on kernel 3.2.4 and now ported to 4.1.18(which we get from latest sdk) for AM3352.
We configured kernel as our hardware and other requirement, it is similar to 3.2.4. but it is not working. After booting u-boot, it hangs on "Starting Kernel.."
We also debugged at low level, previously there was machine id mismatch, which we solved also by changing it in boot loader.
we are using buildroot 2016 and uboot 2013.01.
In 3.2.4, no device tree blob for AM335x, but in 4.1.18 it is available. So we have to do some changes in booting process or any other way is possible or we are doing mistake?