Other Parts Discussed in Thread: AM5726, AM5728
I have a Am5726 evm and wish to check the boot via uart for our own custom designed board. I have changed the jumpers J3,J4 and J6 to select the UART boot mode. I have written a perl script based on the serial-boot.pl to dump the raw data and look for the ASCI-ID sequence. I also have added a loop that fetches the ASIC-ID 3 times using the boot message 0xf003003 to verify that I have the communications working ok. After sending the u-boot-spl.bin file from u-boot-2015.07+gitAUTOINC+5922e09363/spl I get no response on the serial port so the download of u-boot over y-modem (minicom) does not start. I configured u-boot using 'make am57xx_evm_defconfig' and it built ok. Is there something I am missing?