Hi,
As per datasheet of AM335X, The internal USB PHY can be configured to multiplex the UART2_TX or UART2_RX signals with USB0_DM or USB0_DP terminals.
So, if i want to use USB data pins as UART pins, then what care i should have to taken care?
Is voltage levels of UART TX & RX will be 3.3V?
Best Regards,
Vishal Dhanani