This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x Implementing MDIO Bitbang Driver For Clause 45



Hello,


I'm working on a custom board where I have an AM335x with an MDIO/MDC bus connected to a gigabit ethernet phy (Marvell 88E1510) and a 10-gigabit ethernet phy (Marvell 88X2222P). I am using a Buildroot[1] system with Linux kernel 4.6.

The problem is that the AM335x does not support Clause 45 MDIO access[2]. The gigabit device comes up fine as "eth0", however; it seems to be using the CPSW driver.

So I am trying to implement the MDIO Bitbang driver [3] but I can't seem to find much information for how to do this. Including it in the kernel or loading it as a kernel module don't seem to do anything (still only getting eth0).

I am going to look at the MDIO bitbang driver code to see how I'm supposed to use it, but does anyone have any experience/ideas about implementing this kind of driver? Do I still need the Marvell kernel drivers and the bitbang just handles the MDIO transaction or is the bitbang a replacement for the PHY drivers?

Any and all information/pointers are much appreciated.

Thanks,

Thomas

[1] https://buildroot.org/

[2] e2e.ti.com/.../544904

[3] github.com/.../mdio-bitbang.c, but also available in the kernel config under Device Drivers>Network device support>PHY Device support and infrastructure