Other Parts Discussed in Thread: 66AK2E05
Can KeyStone II processor support MT29F512G08CKEABH7 NAND Flash? This flash 512 Gbit part. What is maximum density/size NAND Flash we can interface with KeyStone II?
Thanks,
Alok
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: 66AK2E05
Can KeyStone II processor support MT29F512G08CKEABH7 NAND Flash? This flash 512 Gbit part. What is maximum density/size NAND Flash we can interface with KeyStone II?
Thanks,
Alok
Rahul,
Thanks for your prompt response.
I checked the list of compatible NAND devices and could not find anything larger than 4 GB. We need minimum of 64 GB to meet our requirements. Can you suggest any compatible NAND devices or even eMMC that may meet our requirements. NAND device stated above is ONFI 3.0 compatible so it may not be compatible with KeyStone II.
Thanks for your help.
Alok
Rahul,
I understood that any limitations would be due to the hardware acceleration for ECC in the NAND block. KeyStone-II devices support 1-bit and 4-bit for blocks up to 512 bytes in hardware. However, if controlled solely through software, I was not aware of any limitations on block size or ECC implementation. ONFI compatibility is required if the customer wants to boot from this NAND but if that is not the case, then it should be supported.
Tom
Alok,
I received additional confirmation. The NAND support limitations in KeyStone-I and KeyStone-II devices only exist if this will be a primary boot device. This is due to the requirement for ONFI 1.0 compliance and ECC support in hardware for 1 or 4 bit ECC on blocks up to 512 bytes. However, if the block logic and the ECC logic are managed in software, there is no known limitation. Also, if you desire to boot a large image from the NAND, you would need to boot into an intermediate boot loader that loads a NAND driver that can communicate with the large device.
Tom
Alok,
I believe that R/B can also be polled in some devices. Is that an option for you? I guess using a GPIO for R/B may also be possible. If you run out of CS signals, then that could get really difficult. Of course, you can implement a NAND solely on GPIO pins and control all of the pin transitions in software but that is extreme.
Tom
Alok,
You should check with Micron. The individual R/B status may still be able to be polled for each die.
Tom