Part Number: OMAP-L138
Other Parts Discussed in Thread: OMAPL138
Hi,
My customer is using OMAP - L 138 and is trying to connect to the FPGA via EMIFA.
FPGA is 16 bit word.
They have questions about that connection.
1, In the case of always 16-bit access, can connection of EMA_WE_DQM[1: 0] be unnecessary?
2, When fixing the address mapping of FPGA to even number, can connection of EMA_BA[1] be unnecessary?
Their recognition is that, since EMA_BA[1] corresponds to the LSB of the FPGA address,
if there is no need to access the odd address of the FPGA, EMA_BA[1] is no need to connect.
Please tell me if there is any information.
Best Regards,
Miyashiro