This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6678: DDR3(ECC) on C6678EVM

Part Number: TMS320C6678


Hi Champs,

According to C6678 EVM TRM below, the EVM has DDR3(ECC) on it.  But the DDR3(ECC) is not installed on the EVM.
So, could you please let me clarify why the DDR3(ECC) is not installed?

  o TMDSEVM6678L EVM TRM Version 2.01 [SPRUH58 MAR12]
    (http://wfcache.advantech.com/support/DSPM-8301E_EVM%20(6678)-3.0/TMDSEVM6678L_Technical_Reference_Manual_2V01_0320.pdf)

    - Page 48

      * DDR3 – 2.63W;
       
* 5 SDRAMs to support 64‐bit with ECC of the DSP

Best regards,
j-breeze