Other Parts Discussed in Thread: TMS320DM6467
Dear Experts,
I am unable to start the DM6467 in the JTAG debug mode for the DSP. I have been trying to set the Switch setting (SW3) according to the doc here (TMS320DM6467 Technical Reference Sec 3.4.3). I have also set EMU0 and EMU1 to HIGH. But I keep getting the following error when starting the CCS
Error connecting to the target:
Error 0x80000260/-1137
Fatal Error during: Execution, Initialization, OCS,
It appears that the target is being held in reset. This may be
due to Wait-In-Reset (WIR) configuration set by the EMU0=0
and EMU1=1 pin settings. If this is the case, DISCONNECT
all CONNECTED devices including icepick and then select
RETRY to clear the WIR configuration.
Please guide me if I have missed out on anything. Also it would be helpful if somebody who has got this working mentions the steps to achieve it.
-Regards
Vallabha