Hi
I am going to design a motherboard with AM5728 as CPU and Linux as OS. I am going to use some PCIe and PCI slots on it. I want to make sure about using PCIe switch and PCIe to PCI bridge. I am planing to use PEX8609 as PCIe switch (it was already been used with iMX6Q cpu) and TI XIO2001 as PCIe to PCI bridge.
1- Is it possible to operate both PCIESS1 and PCIESS2 both in x1 at the same time?
2- Is it possible to attach a x4 PCIe peripheral card (EP) to AM5728 via PCIe switch?
3- Is there any need for some changes in the Linux kernel or driver for the following system to be functional?
Thanks.