Hi,
I have a question about AM335x nRESETIN_OUT pin .
My customer are trying to use this nRESETIN_OUT as output for reseting external device.
But after warm reset de-assertion, nRESETIN_OUT signal level is around 0.3V and never goes High level(3.3V).
so that external device never be released from reset.
In customer's board, nRESETIN_OUT pin are pulled up(10kohm) externally to 3.3V .
In AM335x TRM(spruh73p) page.1237 "8.1.7.4.11 Warm Reset Input/Reset Output(nRESETIN_OUT)",
it said as follow:
////////////////////////////////////////////////////////////////////////////////
The nRESETIN_OUT output buffer is configured as an open-drain; consequently,
an external pull-up resistor is required.
////////////////////////////////////////////////////////////////////////////////
It said nRESETIN_OUT output buffer is open-drain, so we thought it will be High(3.3V)
by external pullup resistor after warm reset de-assertion.
What kind of factor can this problem consider?
best regards,
g.f.