Part Number: PROCESSOR-SDK-AM437X
Tool/software: Code Composer Studio
I´ve got a brand new Starter Kit for the AM437x. Connected it via the usb cable to my PC. It detected "AM437x SK EVM XDS100v2".
I´ve started CCS, compiled the GPIO_LedBlink_skAM437x_armTestProject and try to debbug it. The program hungs at location 0x80168010 after calling BIOS_start().
If I try to debug the program I wrote the effect is the same. The program hungs at location 0x80168010 after calling BIOS_start().
I´ve tried UART_BasicExample_skAM437x_armTestProject and the EMAC_BasicExample_skAM437x_armBiosExampleProject. They failed fo connnect to the target. CCS says the target is on reset.
What is corrected configuration for debugging a program on the AM437x Starter Kit?
Installed itens:
CCS 7.2
GCC ARM Compiler 4.9.3
processor_sdk_rtos_am437x 4.00.00.04
am437x PDK v1.0.7
bios 6.46.05.55
xdctools 3.32.02.25_core
regards,
Marcio.